Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

VD0 and HS_VS interrupts w/ parallel camera

Other Parts Discussed in Thread: OMAP3530

I'm using the OMAP3EVM and trying to use the parallel camera interface on the ISP tp write images directly to memory with the CCDC.  I'm using the omap3camera linux tree, so I have first set up the links sensor->CCDC and CCDC->"CCDC Output" with the media-ctl tool.  When I then select() on the /dev/videoX node corresponding to "OMAP3 ISP CCDC output", it times out, never receiving the VD0 interrupt.

I first suspected that the sensor signals were not arriving at the ISP.  But I _am_ getting HS_VS interrupts on rising VS (or HS if I reprogram it) edges, which vanish when I disconnect the respective signal from the EVM, so the HS signal must be arriving.  However, while I measure a frame rate of ~100Hz on the oscilloscope, the HS_VS interrupts for VS come about 300 times faster- more like 30kHz.  My line frequency should be about 50kHz, so if the ISP is indeed getting VS at 30kHz, it's no wonder the line count never gets up to the value in VDINT.  On the oscilloscope, the signals look good- 480 HS pulses inside of each VS pulse.
I have double-checked the following registers are set up as follows to enable the VD0 interrupt appropriately.

CCDC_SYN_MODE = 0x30600
ISP_CTRL = 0x214100
HS/VS slave mode?
ISP_IRQ0ENABLE = 0x811931f9
CCDC_VDINT = 0x140000
(I've moved VDINT0 down from 480 to 20 to try to get the interrupt)

Can someone tell me how I could possibly not be getting the VD0 interrupt?  Or how I could be getting so many erroneous HS_VS interrupts?

  • Michael,

    It looks like based on your settings that your input is 10 bit raw data with discrete syncs.  You noted above that you are getting HS_VS interrupt  and down below you mentioned that you are getting erroneous HS_VS interrupts.  Can you ellaborate on what exactly you are seeing and possibly capture HS/VS signals relative to interrupts with an oscilloscope since I did not see anything obvious looking at registers settings you provided?  Also, VD0 and VD1 interrupts occur relative to VS pulse so if you are providing a valid VS pulse then you should be getting this interrupt correctly.  Please reference section 12.5.4.3.1 (Interrupts Section) of OMAP35x TRM (SPRUF98F).

     

     

     

     

     

  • I found the problem- the wiring was wrong.  Pixel clock from the sensor was connected to GND on the micron interface, so the ISP's pixel clock was floating.  According to "OMAP35 x EVM Hardware User Guide.pdf" that came on the DVD with the board, section 3.3 "Micron Camera Module Connector", pin 25 is MN_CAM_PCLK.  However, on the circuit diagrams for the EVM, CLK is connected to pin 23, which is of course correct.

    I have not found an errata sheet for this HW user guide. I would appreciate being pointed to one so I could avoid any more such errors.

    Now I have moved on to the "CCDC won't become idle!" problem which is already being discussed in this forum: http://e2e.ti.com/support/dsp/omap_applications_processors/f/447/p/29425/207831.aspx (OMAP3530 ISP: Writing CCDC Raw Output to memory.)