This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM5728: OCM reset behavior

Part Number: AM5728

Hi E2E Community

The Sitara AM5728 profides an OCM subsystem which consists of

  • OCMC_RAM1 with 512KiB of dedicated memory space
  • OCMC_RAM2 with 1024KiB of dedicated memory space
  • OCMC_RAM3 with 1024KiB of dedicated memory space

In figure 15-105 I can see that the OCMC_RAMx instances are reset with the CORE_RST signal coming from the PRCM block.

Is the content of the On-Chip Memory reset/cleared when the CPU is reset? Or just the corresponding controller?

Thanks.for your help.

Best regards,

Roger