Tool/software: Linux
Hello,
I have connected AM437X GP EVM to my Linux PC. My Linux PC is a Ubuntu 16.04. When i connect it for USB boot.
The Linux PC reports that RNDIS init has failed. I tried it on Ubuntu 14.04 and the latest 17.04 as well as with the same results.
I wanted to check if Linux Ubuntu 14.04 or 16.04 has been used to test USB boot? I have tried USB boot on multiple ubuntu distributions
with the same results. Can anyone share their Linux setup details or host enviroment on which USB boot has been tested.
Thanks for your help.
Linux Boot Messages on host
[28103.748275] usb 2-3: new full-speed USB device number 29 using xhci_hcd
[28103.888915] usb 2-3: not running at top speed; connect to a high speed hub
[28103.890316] usb 2-3: New USB device found, idVendor=0451, idProduct=6142
[28103.890321] usb 2-3: New USB device strings: Mfr=33, Product=37, SerialNumber=0
[28103.890324] usb 2-3: Product: AM43xx1.2
[28103.890327] usb 2-3: Manufacturer: Texas Instruments
[28109.008534] rndis_host 2-3:1.0: RNDIS init failed, -110
[28109.008553] rndis_host: probe of 2-3:1.0 failed with error -110