Other Parts Discussed in Thread: OMAP3530
Hi,
I am working for TI MPEG4 video encoder and tying to make an application to access
motion vectors by modifying TI DMAI video_encode_io1.
I moved the first step forwad to access MV data as follows: I started from video_encode_io1 code under dvsdk_3_00_00_36/dmai_2_00_00_02 packages. Based on MPEG4 Simple Profile Encoder on OMAP3530 User Guide (Jan 2009), I declared IMP4VENC_DynamicParams extDynParams and set the flag of MVDataEnable.
Then, created Venc1 successfully by calling Venc1_create(hEngine, args->codecName, ¶ms, (VIDENC1_DynamicParams*)&extDynParams).
By calling control(..,XDM_SETPARAMS,..) and control(..,XDM_GETBUFINFO,..), minNumOutBufs is supposed to be 2. But I get minNumOutBufs=1 when I run the application on OMAP3530 target.
(I have attached the appMain.c I modified)
Does anyone has a suggestion why this does not work ?
Thank you !
John
==============
#include <stdio.h>
#include <xdc/std.h>
#include <ti/sdo/ce/Engine.h>
#include <ti/sdo/ce/CERuntime.h>
#include <ti/sdo/dmai/Dmai.h>
#include <ti/sdo/dmai/Ccv.h>
#include <ti/sdo/dmai/Cpu.h>
#include <ti/sdo/dmai/Time.h>
#include <ti/sdo/dmai/BufTab.h>
#include <ti/sdo/dmai/Capture.h>
#include <ti/sdo/dmai/Framecopy.h>
#include <ti/sdo/dmai/BufferGfx.h>
#include <ti/sdo/dmai/ce/Venc1.h>
#include <string.h>
#include "appMain.h"
#include "mp4venc_ti.h"
#include "imp4venc.h"
Void appMain(Args * args)
{
VIDENC1_Params params = Venc1_Params_DEFAULT;
VIDENC1_DynamicParams dynParams = Venc1_DynamicParams_DEFAULT;
BufferGfx_Attrs gfxAttrs = BufferGfx_Attrs_DEFAULT;
Buffer_Attrs bAttrs = Buffer_Attrs_DEFAULT;
Time_Attrs tAttrs = Time_Attrs_DEFAULT;
Venc1_Handle hVe1 = NULL;
FILE *outFile = NULL;
FILE *reconFile = NULL;
FILE *inFile = NULL;
Engine_Handle hEngine = NULL;
Time_Handle hTime = NULL;
Buffer_Handle hOutBuf = NULL;
Buffer_Handle hInBuf = NULL;
Buffer_Handle hReconBuf = NULL;
Int numFrame = 0;
Int inBufSize, outBufSize;
Cpu_Device device;
ColorSpace_Type colorSpace;
UInt32 time;
/* Added for MV Access */
IMP4VENC_DynamicParams extDynParams = {
Venc1_DynamicParams_DEFAULT,
0, //resync
0, //hec
0, //air
1, //mir
12, //QI
12, //QP
3, //fcode
1, //HPI
0, //ACpred
0, //LFF
0, //MVaccess
1, //UMV
0, //4MV
1, //resync data
};
CERuntime_init();
Dmai_init();
inFile = fopen(args->inFile, "rb");
outFile = fopen(args->outFile, "wb");
hEngine = Engine_open(args->engineName, NULL, NULL);
//set parameters
params.rateControlPreset = IVIDEO_LOW_DELAY;
params.maxBitRate = args->bitRate;
params.inputChromaFormat = XDM_YUV_422ILE;
params.maxWidth = args->width;
params.maxHeight = args->height;
params.dataEndianness = XDM_BYTE;
params.maxInterFrameInterval = 1;
params.inputContentType = IVIDEO_CONTENTTYPE_DEFAULT ;
params.reconChromaFormat = XDM_CHROMA_NA ;
dynParams.targetBitRate = params.maxBitRate;
dynParams.inputWidth = params.maxWidth;
dynParams.inputHeight = params.maxHeight;
extDynParams.videncDynamicParams.size = sizeof(IMP4VENC_DynamicParams);
extDynParams.MVDataEnable = 1; /**** to enable MV access ***/
extDynParams.videncDynamicParams = dynParams;
/* Create the video encoder */
//hVe1 = Venc1_create(hEngine, args->codecName, ¶ms, &dynParams);
hVe1 = Venc1_create(hEngine, args->codecName, ¶ms, (VIDENC1_DynamicParams*)&extDynParams);
inBufSize = Venc1_getInBufSize(hVe1);
outBufSize = Venc1_getOutBufSize(hVe1);
colorSpace = device == Cpu_Device_DM6467 ? ColorSpace_YUV420PSEMI :
ColorSpace_UYVY;
gfxAttrs.bAttrs.memParams.align = bAttrs.memParams.align = BUFSIZEALIGN;
if (args->cache) {
gfxAttrs.bAttrs.memParams.flags = bAttrs.memParams.flags
= Memory_CACHED;
}
gfxAttrs.dim.width = args->width;
gfxAttrs.dim.height = args->height;
gfxAttrs.dim.lineLength = BufferGfx_calcLineLength(args->width, colorSpace);
gfxAttrs.colorSpace = colorSpace;
/* Create the input buffer for raw yuv data */
hInBuf = Buffer_create(Dmai_roundUp(inBufSize, BUFSIZEALIGN),
BufferGfx_getBufferAttrs(&gfxAttrs));
/* Create the output buffer for encoded video data */
hOutBuf = Buffer_create(Dmai_roundUp(outBufSize, BUFSIZEALIGN), &bAttrs);
while (numFrame++ < args->numFrames) {
readFrameUYVY(hInBuf, inFile);
if (args->cache) {
Memory_cacheWbInv(Buffer_getUserPtr(hInBuf), Buffer_getSize(hInBuf));
Memory_cacheInv(Buffer_getUserPtr(hOutBuf), Buffer_getSize(hOutBuf));
}
BufferGfx_resetDimensions(hInBuf);
Venc1_process(hVe1, hInBuf, hOutBuf);
if (args->cache) {
Memory_cacheWb(Buffer_getUserPtr(hOutBuf), Buffer_getSize(hOutBuf));
}
/* Write the encoded frame to the file system */
if (Buffer_getNumBytesUsed(hOutBuf)) {
if (fwrite(Buffer_getUserPtr(hOutBuf),
Buffer_getNumBytesUsed(hOutBuf), 1, outFile) != 1) {
printf("Failed to write encoded video data to file\n");
goto cleanup;
}
}
}
cleanup:
/* Clean up the application */
....
}
================