This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/AM3352: How to stream the IP Camera data from network to outside world...

Part Number: AM3352

Tool/software: Linux

Hi,

We are using AM3352 for streaming the data from IP Camera. IP Camera and our development board is connected to network. Our requirement is to make our dev board as server and any one connecting to it, should be able to see the IP camera stream. This I was able to do it on stand alone PC running VLC player (In VLC -> Stream, I gave the source IP address of camera, stream as RTSP and gave some name (test4.rtsp)) and any one connecting to my PC with browser, can see the stream from IP camera.

1. What is the best way to achieve this in our development board? Using any tool like VLC/ FFMPEG etc?

2. Is there any sample (or simple) code to achieve this (basically we need to show that this proof of concept works).

Let us know if you have any thoughts/ directions.

Used, FFServer and FFMPEG, but we are getting segmentation fault.

With best regards,

Phani.