I put a switch in to pull POWER_ON (from the TPS650732) low (it is otherwise pulled up to Vsys). I would still like to tie POWER_ON to the AM3517, though, in order to give the 3517 the ability to reset the board. I see on a ref schematic that POWER_ON is going into a GPIO on the 3517. My only concern is whether or not the GPIO will be pulling that line down during startup, therefore not allowing the DC convertors to enable. Suggestions?