Part Number: DRA750
Other Parts Discussed in Thread: PMP
Tool/software: Linux
Hi,
I have a question about how to build the kernel image with the dtb file attached to the kernel image. I built the kernel image with the dtb file attached . But the built kernel image can’t boot after u-boot loading it to DDR memory..
Following is the procedure to build the kernel image with the dtb file attached.
1. Set Kernel Menuconfig:
Boot options —>
[*] Use appended device tree blob to zImage (EXPERIMENTAL)
2. device tree dtb file attached to the kernel image
$: cat arch/arm/boot/zImage arch/arm/boot/dts/xxx.dtb > arch/arm/boot/zImage_dtb
3. Build uImage
mkimage -A arm -O linux -C none -T kernel -a 0x80008000 -e 0x80008000 -n 'Linux uImage' -d zImage_dtb uImage_dtb
4. The log file Log_zImage is the error message for booting zImage_dtb.
The log file Log_uImage is the error message for booting uImage_dtb.
Could you help to check the problem? Thanks a lot.
U-Boot 2014.07 (Aug 14 2017 - 21:38:42)
CPU : DRA752-GP ES2.0
Board: DRA74x EVM REV <NULL>
I2C: ready
DRAM: 256 MiB
NAND: 0 MiB
MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1
Using default environment
serial# not set, setting...
Target spinup took 0 ms.
AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl SATA mode
flags: 64bit ncq stag pm led clo only pmp pio slum part ccc apst
scanning bus for devices...
Device 0: (0:0) Vendor: ATA Prod.: suf rod vecise.. Rev: nain
Type: Hard Disk
Capacity: not available
Found 1 device(s).
SCSI: Net: <ethaddr> not set. Validating first E-fuse MAC
cpsw
Hit any key to stop autoboot: 0
@ADAPTER@
switch to partitions #0, OK
mmc0 is current device
SD/MMC found on device 0
reading uEnv.txt
221 bytes read in 3 ms (71.3 KiB/s)
Loaded environment from uEnv.txt
Importing environment from mmc0 ...
3984181 bytes read in 210 ms (18.1 MiB/s)
109113 bytes read in 16 ms (6.5 MiB/s)
Booting from mmc0 ...
Kernel image @ 0x82000000 [ 0x000000 - 0x3b20f8 ]
## Flattened Device Tree blob at 88000000
Booting using the fdt blob at 0x88000000
Loading Device Tree to 8e6fd000, end 8e71aa38 ... OK
Starting kernel ...
U-Boot 2014.07 (Aug 14 2017 - 21:11:58)
CPU : DRA752-GP ES2.0
Board: DRA74x EVM REV <NULL>
I2C: ready
DRAM: 256 MiB
NAND: 0 MiB
MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1
Using default environment
serial# not set, setting...
Target spinup took 0 ms.
AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl SATA mode
flags: 64bit ncq stag pm led clo only pmp pio slum part ccc apst
scanning bus for devices...
Device 0: (0:0) Vendor: ATA Prod.: suf rod vecise.. Rev: nain
Type: Hard Disk
Capacity: not available
Found 1 device(s).
SCSI: Net: <ethaddr> not set. Validating first E-fuse MAC
cpsw
Hit any key to stop autoboot: 0
@ADAPTER@
switch to partitions #0, OK
mmc0 is current device
SD/MMC found on device 0
3984229 bytes read in 210 ms (18.1 MiB/s)
Booting from mmc0 ...
## Booting kernel from Legacy Image at 82000000 ...
Image Name: Linux uImage
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 3984165 Bytes = 3.8 MiB
Load Address: 80008000
Entry Point: 80008000
Verifying Checksum ... OK
U-Boot 2014.07 (Aug 14 2017 - 21:11:58)
CPU : DRA752-GP ES2.0
Board: DRA74x EVM REV <NULL>
I2C: ready
DRAM: 256 MiB
NAND: 0 MiB
MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1
Using default environment
serial# not set, setting...
Target spinup took 0 ms.
AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl SATA mode
flags: 64bit ncq stag pm led clo only pmp pio slum part ccc apst
scanning bus for devices...
Device 0: (0:0) Vendor: ATA Prod.: suf rod vecise.. Rev: nain
Type: Hard Disk
Capacity: not available
Found 1 device(s).
SCSI: Net: <ethaddr> not set. Validating first E-fuse MAC
cpsw
Hit any key to stop autoboot: 0
@ADAPTER@
switch to partitions #0, OK
mmc0 is current device
SD/MMC found on device 0
3984229 bytes read in 210 ms (18.1 MiB/s)
Booting from mmc0 ...
## Booting kernel from Legacy Image at 82000000 ...
Image Name: Linux uImage
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 3984165 Bytes = 3.8 MiB
Load Address: 80008000
Entry Point: 80008000
Verifying Checksum ... OK
1. booting zImage_dtb.
U-Boot 2014.07 (Aug 14 2017 - 21:38:42)
CPU : DRA752-GP ES2.0
Board: DRA74x EVM REV <NULL>
I2C: ready
DRAM: 256 MiB
NAND: 0 MiB
MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1
Using default environment
serial# not set, setting...
Target spinup took 0 ms.
AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl SATA mode
flags: 64bit ncq stag pm led clo only pmp pio slum part ccc apst
scanning bus for devices...
Device 0: (0:0) Vendor: ATA Prod.: suf rod vecise.. Rev: nain
Type: Hard Disk
Capacity: not available
Found 1 device(s).
SCSI: Net: <ethaddr> not set. Validating first E-fuse MAC
cpsw
Hit any key to stop autoboot: 0
@ADAPTER@
switch to partitions #0, OK
mmc0 is current device
SD/MMC found on device 0
reading uEnv.txt
221 bytes read in 3 ms (71.3 KiB/s)
Loaded environment from uEnv.txt
Importing environment from mmc0 ...
3984181 bytes read in 210 ms (18.1 MiB/s)
109113 bytes read in 16 ms (6.5 MiB/s)
Booting from mmc0 ...
Kernel image @ 0x82000000 [ 0x000000 - 0x3b20f8 ]
## Flattened Device Tree blob at 88000000
Booting using the fdt blob at 0x88000000
Loading Device Tree to 8e6fd000, end 8e71aa38 ... OK
Starting kernel ...
2. booting uImage_dtb.
U-Boot 2014.07 (Aug 14 2017 - 21:11:58)
CPU : DRA752-GP ES2.0
Board: DRA74x EVM REV <NULL>
I2C: ready
DRAM: 256 MiB
NAND: 0 MiB
MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1
Using default environment
serial# not set, setting...
Target spinup took 0 ms.
AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl SATA mode
flags: 64bit ncq stag pm led clo only pmp pio slum part ccc apst
scanning bus for devices...
Device 0: (0:0) Vendor: ATA Prod.: suf rod vecise.. Rev: nain
Type: Hard Disk
Capacity: not available
Found 1 device(s).
SCSI: Net: <ethaddr> not set. Validating first E-fuse MAC
cpsw
Hit any key to stop autoboot: 0
@ADAPTER@
switch to partitions #0, OK
mmc0 is current device
SD/MMC found on device 0
3984229 bytes read in 210 ms (18.1 MiB/s)
Booting from mmc0 ...
## Booting kernel from Legacy Image at 82000000 ...
Image Name: Linux uImage
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 3984165 Bytes = 3.8 MiB
Load Address: 80008000
Entry Point: 80008000
Verifying Checksum ... OK
BR,
ShawnX Lin