Part Number: AM3352
Tool/software: Linux
Hi, all
Recently, we use a 4G module which is based on USB connection on our custom board and there is a issue about it. when we reboot the system after it is booted up,
the system hangs at the message below.
The system is going down NOW!
Sent SIGTERM to all processes
[ 20.353973] musb-hdrc musb-hdrc.1: remove, state 1
[ 20.359161] usb usb2: USB disconnect, device number 1
which i think is mostly about the usb driver, and we are not familiar with the musb driver.So, we need your help.
BTW, our CPU is AM3352 and kernel version is 3.2.0.
Thank you!
jason.