This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3358: Boot issues

Part Number: AM3358


Hi,

We have used AM3358 ZCZ100 and we have produced dozens of them till date. However in the latest production batch (15 boards), none of the boards are booting and we are unable to get "CCCCC" on the COM port. On multiple tries, we occasionally get four "CCCC" and stops and repeats when a manual reset switch is held, but this is not consistent too.

We never had a problem before and unable to debug what's causing this strange behaviour. We use TPS65217C as the PMIC and MMC0 as the program memory. The supplies from PMIC are in the correct voltage range and even the PMIC_PGOOD signal (timing wise and voltage level) seems comparable to a working board.

We suspected bad lot of parts and replaced the AM3358 and PMIC, neither resulted in any good luck

We are not well versed in using CCS and JTAG and had used JTAG only once in the beginning of the project 2 years ago, would need help in what to look for in JTAG if that's the only option.

-Prasad.

  • Hi,

    Do you have external 4.7kOhm pullups to VDDSHV6 on pins EMU0 and EMU1?
  • Hi Bisar,

    Yes, we do have them in design and also populated on the boards.

    Also on one of the boards, I observed that placing a body capacitance (touching) on BOOT0~4 while powering the board starts that board consistently. So was suspecting if there was a glitch in power supply, however as an experiment, I tried placing 1uF cap near the pull ups and also place 10nF caps on the Boot0~4 - but didn't help.

    That particular board still starts with a finger placed on top of the Pull up resistors.

    For completeness the chosen SYSBOOT config is

    4~0:11100

    5: 1

    7~6:11

    13~8: DON'T CARE (0's)

    15~14: 01 (24MHz)

  • What are the values of the SYSBOOT resistors? What else is connected on the SYSBOOT lines?
  • Hi Biser,

    The SYSBOOT pins are connected with 100K pullup/pull down accordingly. The Interface (LIDD) which is sysboot too, is connected to a FPGA (which is not powered until ARM boots up and switches on the Power)

    One more observation.

    The BOOT pins are not reaching the high and are stuck at 1.4V in the failed board. In a good board they track the 3V3A supply and reach 2V. Fig1 is the failed board and Fig2 is Good board, Channel 1 is 3v3A and Channel 2 is BOOT0

    Figure 1

    Figure2

    We have made more than 35 boards (in multiple batches) however this is first time I see the problem. There is no change in the design and attached the schematic pages for the ARM.

    340-00309-01_IP3_SPIN3A_REV01_ARM_Section.pdf

  • Hi Biser,

    I had trouble with my login, so doing with the other login.

    The SYSBOOT pins are pulled up/down with 100K, only BOOT0~4 are pulled low through a configurable switch with a 10K Pull down. We prototyped atleast 30~40 boards in 4 batches and we never had a problem before.

    One more observation and this is the problem causing the boot issues, but unable to find the root cause of it and how to contain it. In good board the BOOT pins come up to 2V tracking the VDD_3V3 supply from PMIC (connected to VDDSHV6) as in Figure 1, however in the bad board the boot pins ramp slowly and are only 1.4V, as in Fugure 2. I tried changing the pullups to 10K, still didn't work.

    I used JTAG and CCS, configured as AM3358SK, I read the control Status register as 0x00000300, but on a good one it is 0x004003FC.

    Figure1

    Figure2

    Regards,

    Prasad.

  • Hi Biser,

    I had trouble with my login, so doing with the other login.

    The SYSBOOT pins are pulled up/down with 100K, only BOOT0~4 are pulled low through a configurable switch with a 10K Pull down. We prototyped atleast 30~40 boards in 4 batches and we never had a problem before.

    One more observation and this is the problem causing the boot issues, but unable to find the root cause of it and how to contain it. In good board the BOOT pins come up to 2V tracking the VDD_3V3 supply from PMIC (connected to VDDSHV6), however in the bad board the boot pins ramp slowly and are only 1.4V, I tried changing the pullups to 10K, still didn't work.

    I used JTAG and CCS, configured as AM3358SK, I read the control Status register as 0x00000300, but on a good one it is 0x004003F

    Prasad.

  • From what I see you have voltage leaks during power supply ramp-up. The PMIC 3.3V rail should not ramp-up like that. From your schematics I cannot see the source of VCC_3.3V_Main. You must ensure that this rail does not come up before the processor 3.3V rails.

    Off-topic, another thing I notice is that your Ethernet PHY is at 2.5V IO voltage. The Processor MII/RMII/RGMII pins are either 3.3V or 1.8V. 2.5V is not a permitted voltage.
  • Hi Biser,

    The problem was the FPGA was latching the BOOT pins and we tried a very strong pullup (100 ohms to VDD_3V3A) just as experiment and still didn't help. So I had to find a work around to make sure the latchup is prevented for the duration of the Boot pins values are latched into the control register.

    Thanks for the suggestion, it was long doubted the leakages causing the supply ramp-up issue and today I sequenced the VCC_3.3V_Main to VDD_3V3A and that cleared the boot issue and also mostly cleared the supply ramp-up.

    Now the boards are booting consistently.

    With respect to Ethernet PHY, at the time of design we found it was at the border and also we needed 100/1000 so had to choose that device. Do you have a recommended phy part for 10/100/1000? we can add this to future design changes.

    Regards,

    Prasad.

  • Glad you solved this. On your other question, TI EVMs use Qualcomm AR8031-AL1A, and more recently Microchip KSZ9031RNX.