This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/AM4379: How to debug an application program using a shared library in embedded linux system?

Part Number: AM4379


Tool/software: Linux

My application program contains a shared library,a .so file.And it runs in an embedded linux system running in ARM Cortex-A9.How can I debug it?

When I used the gdb method to debug it,I got the following message:

warning: Unable to find dynamic linker breakpoint function.
GDB will be unable to debug shared library initializers
and track explicitly loaded dynamic code.
0x498c0c80 in ?? ()

Does it mean that I can't debug the application using shared library?

Thank you very much!