This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM4378: SD card detection

Part Number: AM4378


Hi,

My customer uses AM4378. OS is Linux. And they use TI processor's SDK.

They are facing one issue  "no SD card detection".

Currently, there are hardware that does not recognize the SD card when starting AM 437x.
They want to separate it is hard issur or software issue.

Kernel settings, point to analyze with device driver, etc.
Could you teach it?

Incidentally, system configuration is the below.


Mmc0: bootSD (same as Am 437 x StarterKit)
Mmc 1: SD Slot
Mmc 2: SD Slot

The CD pin of each SD slot is connected to GPIO,

At the H / L level of the GPIO, although the card can be detected, normally the following log should be displayed,
When the phenomenon occurs, the log is not displayed.

[1.864191] mmc 2: new high speed SDHC card at address e 624
[1.870185] mmcblk 1: mmc 2: e 624 SU 08 G 7.40 Gi B

Please advise me.

I appreciate your quick reply.

Best regards,

Michi