Tool/software: Linux
Hi Sirs,
We are using DM385 custom board with IPNC 3.8.We tried to enable the usb host((ohci-hcd) and usb serial driver(option,usb_wwan,usbserial) in the kernel then we inserted the usb device to test.But It did not seem to be successful.
1.I can not see the informations of USB device in /proc/tty/usb
2.I can not see the major number and minor number in /sys/dev/char
3.But I can see the character device (188 ttyUSB) in /proc/devices
4.The messages in the kernel are as below.It seem the driver can be enabled.
-----------------------
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
usbcore: registered new interface driver smsc95xx
usbcore: registered new interface driver cdc_eem
usbcore: registered new interface driver usbserial
usbserial: USB Serial Driver core
USB Serial support registered for GSM modem (1-port)
usbcore: registered new interface driver option
option: v0.7.2:USB Driver for GSM modems
ohci_hcd: USB 1.1 'Open' Host Controller (OHCI) Driver
SCSI subsystem initialized
usbcore: registered new interface driver cdc_acm
cdc_acm: v0.26:USB Abstract Control Model driver for USB modems and ISDN adapters
musb-hdrc: version 6.0, host, debug=0
USBSS revision 4ea2080b
registerd cppi-dma Intr @ IRQ 17
Cppi41 Init Done
musb-hdrc musb-hdrc.0: dma type: dma-cppi41
MUSB controller-0 revision 4ea20800
usb2phy: computed values rxcalib(15)DACs(30 14 14)
usb2phy: override computed values rxcalib(15)DACs(30 14 14)
usb2phy_config: musb(0) rxcalib done, rxcalib read value 6f6f5d76
TxFifo Empty intr enabled
musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine, bulk split, HB-ISO Rx, HB-ISO Tx, SoftConn)
musb-hdrc: MHDRC RTL version 2.0
musb-hdrc: setup fifo_mode 4
musb-hdrc: 28/31 max ep, 16384/16384 memory
musb-hdrc musb-hdrc.0: MUSB HDRC host driver
musb-hdrc musb-hdrc.0: new USB bus registered, assigned bus number 1
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
musb-hdrc musb-hdrc.0: USB Host mode controller at ce0a0000 using DMA, IRQ 18
musb-hdrc musb-hdrc.1: dma type: dma-cppi41
MUSB controller-1 revision 4ea20800
usb2phy: computed values rxcalib(15)DACs(35 16 15)
usb2phy: override computed values rxcalib(15)DACs(35 16 15)
usb2phy_config: musb(1) rxcalib done, rxcalib read value 6f71e17e
TxFifo Empty intr enabled
musb-hdrc: ConfigData=0xde (UTMI-8, dyn FIFOs, bulk combine, bulk split, HB-ISO Rx, HB-ISO Tx, SoftConn)
musb-hdrc: MHDRC RTL version 2.0
musb-hdrc: setup fifo_mode 4
musb-hdrc: 28/31 max ep, 16384/16384 memory
musb-hdrc musb-hdrc.1: MUSB HDRC host driver
musb-hdrc musb-hdrc.1: new USB bus registered, assigned bus number 2
hub 2-0:1.0: USB hub found
hub 2-0:1.0: 1 port detected
musb-hdrc musb-hdrc.1: USB Host mode controller at ce0a4800 using DMA, IRQ 19
usb 1-1: new high speed USB device using musb-hdrc and address 2
-----------------------
How do I check this issue?Please give us the suggestion,thanks.
Best Regards,
Byron