Part Number: TMS320TCI6614
Customer use 2 TCI6614 connect with SRIO, ask whether can hot plug the SRIO between TCI6614?
Below post discussed it is not possible between C6678 and another device. but this case is between two same devices.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320TCI6614
Customer use 2 TCI6614 connect with SRIO, ask whether can hot plug the SRIO between TCI6614?
Below post discussed it is not possible between C6678 and another device. but this case is between two same devices.
What are you trying to accomplish? Perhaps you could use another peripheral such as Hyperlink.
-dave
In our application, two Boards (one 6614 in one Board)will be used together and the communication ports between two 6614 is SRIO . Both 6614 Boards should support hotplug.
There are too many lines are used in Hyperlink, so it is not the best choice as the Communication ports across the board.
And if the Hyperlink support hotplug ???
Dave,
Do you mean Hyperlink support hotplug, but SRIO doesn't support hotplug?