This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM4377: Debug UART

Expert 1070 points
Part Number: AM4377


Hello,

Please advise,


Our module designed in a such way that the Primary Serial Debug port for TI Sitara AM437x is UART0 (out of 6 available instantiations of the UART).
I believe that we have followed a TI reference design.

One of our customers asking about option to use SoC UART1 instead of UART0 for Primary Serial Debug port.

From device TRM (Literature Number: SPRUHL7G) chapter "21.2.1 UART Connectivity Attributes" I've noticed that Power Domain for UART0 is Wake-Up Domain.
While for the rest of UARTS (1-5)  the power domain is Peripheral Domain.
But it still not clear for me if it possible to use UART1 instead of UART0 for Serial Debug.

Can you please help me with this?


Many thanks in advance.