This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The datasheet for the OMAP-L137 (page 61) states that for input clock frequencies between 20 and 30 MHz, a crystal with 60 ohm max ESR is recommended and typical load capacitance values are 10-20 pF. I have been searching for a crystal with a 4-SMD (2.5mm x 2.00mm) package to replace the original crystal that is now obsolete in my design. This is the crystal that I found that comes closest to meeting the OMAP-L137 requirements:
MFG PN: NX2520SA-24.576000MHZ
MFG: NDK America, Inc.
It has a Load Capacitance of 10 pF (Requirement is 10-20pF)
However, it has an ESR of 70 ohm (Requirement per the datasheet is 60 Ohm max). Will this be a problem?
Thanks
However, it has an ESR of 70 ohm (Requirement per the datasheet is 60 Ohm max). Will this be a problem?
I'm assuming the same is true for the load capacitance?
For the OMAP-L137, the clock signals have to route through vias do to the pins being F2 (OSCIN), F1 (OSCOUT) and E2 (OSCVSS). With that being said, when choosing the series capacitor values for the crystal, do you typically add approximately 3 - 5 pF to the value to account for the parasitic capacitance?
Example: Cload = ( (C1+Cparasitic) * (C2+Cparasitic) ) / ( (C1+Cparasitic) + (C2+Cparasitic) )