Part Number: TMDSSK3358
Other Parts Discussed in Thread: TPS63010
Hi experts ,first sorry for my English I'm not native.
I use starer kit (TMDSSK3358) and have problem with USB.I saw some post about VBUS_ERROR like this one :

but I can't find proper answer about this problem. I use USB 4G-LTE module and I want connect it to my board.It use " cdc_ether " kernel driver module and recompile it and check all dependency(I used official sitara SDK). but after connect LTE module I saw this message kernel errors :
[ 568.318175] musb-hdrc musb-hdrc.1: VBUS_ERROR in a_wait_vrise (89, <AValid), retry #1, port1 00000104
[ 569.366745] usb 2-1: new high-speed USB device number 2 using musb-hdrc
[ 577.946715] usb 2-1: new high-speed USB device number 3 using musb-hdrc
[ 586.506744] usb 2-1: new high-speed USB device number 4 using musb-hdrc
[ 595.066714] usb 2-1: new high-speed USB device number 5 using musb-hdrc
[ 603.626711] usb 2-1: new high-speed USB device number 6 using musb-hdrc
[ 612.656715] usb 2-1: new high-speed USB device number 7 using musb-hdrc
[ 620.886842] usb 2-1: new high-speed USB device number 8 using musb-hdrc
[ 629.306755] usb 2-1: new high-speed USB device number 9 using musb-hdrc
This module work on another PC and boards like GATEWORKS proper and with out problem . I sure circuit is OK . Please give me exact solution. if I use USB hub with external +5V power supply maybe solve problem or not ?
Thanks
Amir