Other Parts Discussed in Thread: OMAP3530
Hi,
I have a problem of Windows Embedded Compact 7 on TMDSEVM3530 (OMAP35xEVM board).
I' ve built and downloaded run-time image (Release mode) to the board, but after downloading the image, nothing displays on the LCD.
The backlight is on, but the desktop picture of Compact 7 doesn't appear. (It seems that the system holds up)
This Problem also occurs when I boot from SD card. In the SD card, MLO, EBOOTSD.nb0 and NK.bin files have been written.
I think that there is some problems in NK.bin file, because a test described below was successful. (Booting from SD card)
MLO, EBOOTSD.nb0 <----- created in Compact 7 Project
NK.BIN <----- CE 6.0 R3 Demo file (the attachment of TMDSEVM3530)
Here is terminal logs of the tests using NK.bin of Compact 7 and CE 6.0 R3 Demo.
------------------------------[ NK.bin of Compact 7 ]-------------------------------------------------------------------------
Texas Instruments Windows CE SD X-Loader for EVM 3530
Built Aug 26 2010 at 10:37:38
Version 6.13.00
open ebootsd.nb0 file
Init HW: controller RST
read ebootsd.nb0 file
jumping to ebootsd image
Microsoft Windows CE Bootloader Common Library Version 1.4 Built Aug 26 2010 10:34:03
Texas Instruments Windows CE EBOOT for Mistral OMAP EVM, Built Aug 26 2010 at 10:37:34
EBOOT Version 1.5, BSP 6.13.00
TI OMAP3530 Version 0x4b7ae02f (ES3.1)
TPS659XX Version 0x10 (Unknown)
System ready!
Preparing for download...
INFO: Predownload....
WARN: Boot config wasn't found, using defaults
INFO: SW4 boot setting: 0x18
>>> Forcing cold boot (non-persistent registry and other data will be wiped) <<<
Hit space to enter configuration menu 5...
Hit space to enter configuration menu 4...
Hit space to enter configuration menu 3...
Hit space to enter configuration menu 2...
Hit space to enter configuration menu 1...
Init HW: controller RST
BL_IMAGE_TYPE_BIN
Download file information:
-----------------------------------------------------------
[0]: Address=0x84001000 Length=0x02ef3dfc Save=0x80001000
-----------------------------------------------------------
Download file type: 1
rom_offset=0x0.
ImageStart = 0x84001000, ImageLength = 0x2ef3dfc, LaunchAddr = 0x8400ce00
Completed file(s):
-------------------------------------------------------------------------------
[0]: Address=0x84001000 Length=0x2ef3dfc Name="" Target=RAM
ROMHDR at Address 84001044h
Launch Windows CE image by jumping to 0x8000ce00...
Windows CE Kernel for ARM (Thumb Enabled)
--- High Performance Frequecy is 32768 khz---
--------------------------------------------------------------------------------------------------------------------------------------
------------------------------[ NK.bin of CE 6.0 R3 Demo ]----------------------------------------------------------------
Texas Instruments Windows CE SD X-Loader for EVM 3530
Built Aug 26 2010 at 10:37:38
Version 6.13.00
open ebootsd.nb0 file
Init HW: controller RST
read ebootsd.nb0 file
jumping to ebootsd image
Microsoft Windows CE Bootloader Common Library Version 1.4 Built Aug 26 2010 10:34:03
Texas Instruments Windows CE EBOOT for Mistral OMAP EVM, Built Aug 26 2010 at 10:37:34
EBOOT Version 1.5, BSP 6.13.00
TI OMAP3530 Version 0x4b7ae02f (ES3.1)
TPS659XX Version 0x10 (Unknown)
System ready!
Preparing for download...
INFO: Predownload....
WARN: Boot config wasn't found, using defaults
INFO: SW4 boot setting: 0x18
>>> Forcing cold boot (non-persistent registry and other data will be wiped) <<<
Hit space to enter configuration menu 5...
Hit space to enter configuration menu 4...
Hit space to enter configuration menu 3...
Hit space to enter configuration menu 2...
Hit space to enter configuration menu 1...
Init HW: controller RST
BL_IMAGE_TYPE_BIN
Download file information:
-----------------------------------------------------------
[0]: Address=0x84001000 Length=0x023af378 Save=0x80001000
-----------------------------------------------------------
Download file type: 1
rom_offset=0x0.
ImageStart = 0x84001000, ImageLength = 0x23af378, LaunchAddr = 0x8400b1c4
Completed file(s):
-------------------------------------------------------------------------------
[0]: Address=0x84001000 Length=0x23af378 Name="" Target=RAM
ROMHDR at Address 84001044h
Launch Windows CE image by jumping to 0x8000b1c4...
Windows CE Kernel for ARM (Thumb Enabled) Built on Sep 25 2009 at 11:04:23
--- High Performance Frequecy is 32768 khz---
--------------------------------------------------------------------------------------------------------------------------------------
Also, I've built successfully in Debug Mode by modifying the memory allocation as below. ("successfully " means no errors)
[Before Modification]
MEMORY
; Name VA Length Type
ARGS 84000000 00001000 RESERVED ; 4K
#if (defined BSP_DSPLINK || defined BSP_TI_DVSDK)
IF BSP_SDRAM_BANK1_ENABLE
NK 84001000 047FF000 RAMIMAGE ; 72MB - 4K
DISPLAY 88800000 01000000 RESERVED ; 16MB
CMEM_DSP 89800000 02800000 RESERVED ; 40 MB
RAM 8C000000 08000000 RAM ; 128MB
[After Modification]
MEMORY
; Name VA Length Type
ARGS 84000000 00001000 RESERVED ; 4K
#if (defined BSP_DSPLINK || defined BSP_TI_DVSDK)
IF BSP_SDRAM_BANK1_ENABLE
NK 84001000 096FF000 RAMIMAGE ; 151MB - 4K
DISPLAY 8D700000 01000000 RESERVED ; 16MB
CMEM_DSP 8E700000 02800000 RESERVED ; 40 MB
RAM 90F00000 03100000 RAM ; 49MB
However, after download run-time image to the OMAP3530 board, there is an exception as below,
First-chance exception in NAND.DLL.
(0xC0000005: Access Violation)
This exception occurs in "C:\WINCE700\platform\ti_evm_3530\SRC\DRIVERS\BLOCK\NAND\fmd.c"
Are there any problems in NAND driver in BSP of "ti_evm_3530"?
Before building, I deleted drivers for OneNAND from the Catalog file and added those for NAND to that file instead because the board has 256MB NAND flash only.
What causes these problems and what should I do to work around them?