Part Number: AM3354
Other Parts Discussed in Thread: TPS65910
Hi,
In custom board of AM3354. When starting boot from SD card. I m getting attached Log and the device stops at that point.
Log -
Remove CPU : AM335X-GP rev 2.1
Model: TI AM335x EVM
Watchdog enabled
DRAM: 512 MiB
NAND: 256 MiB
MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1
reading uboot.env
** Unable to read "uboot.env" from mmc0:1 **
Using default environment
<ethaddr> not set. Validating first E-fuse MAC
Net: eth0: ethernet@4a100000
Warning: usb_ether MAC addresses don't match:
Address in SROM is de:ad:be:ef:00:01
Address in environment is 68:9e:19:81:96:6a
, eth1: usb_ether
Press SPACE to abort autoboot in 2 seconds
Booting from nand ...
NAND read: device 0 offset 0x80000, size 0x40000
262144 bytes read: OK
NAND read: device 0 offset 0x200000, size 0x800000
8388608 bytes read: OK
Bad Linux ARM zImage magic!
switch to partitions #0, OK
mmc0 is current device
SD/MMC found on device 0
reading boot.scr
** Unable to read file boot.scr **
reading uEnv.txt
** Unable to read file uEnv.txt **
switch to partitions #0, OK
mmc0 is current device
Scanning mmc 0:1...
switch to partitions #0, OK
mmc0 is current device
SD/MMC found on device 0
3474872 bytes read in 570 ms (5.8 MiB/s)
43047 bytes read in 43 ms (977.5 KiB/s)
Kernel image @ 0x82000000 [ 0x000000 - 0x3505b8 ]
## Flattened Device Tree blob at 88000000
Booting using the fdt blob at 0x88000000
Loading Device Tree to 8fff2000, end 8ffff826 ... OK
Starting kernel ...
[ 0.000000] Booting Linux on physical CPU 0x0
[ 0.000000] Initializing cgroup subsys cpu
[ 0.000000] Initializing cgroup subsys cpuacct
[ 0.000000] Linux version 4.4.41-gf9f6f0db2d (root@user-bltsp01373) (gcc version 5.3.1 20160113 (Linaro GCC 5.3-2016.02) ) #30 PREEMPT Fri Aug 18 03:50:29 IST 2017
[ 0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c5387d
[ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
[ 0.000000] Machine model: TI AM335x EVM
[ 0.000000] cma: Reserved 48 MiB at 0x9d000000
[ 0.000000] Memory policy: Data cache writeback
[ 0.000000] CPU: All CPU(s) started in SVC mode.
[ 0.000000] AM335X ES2.1 (sgx neon )
[ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 129920
[ 0.000000] Kernel command line: console=ttyO0,115200n8 root=PARTUUID=d8c65ab4-02 rw rootfstype=ext4 rootwait
[ 0.000000] PID hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.000000] Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)
[ 0.000000] Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)
[ 0.000000] Memory: 459980K/524288K available (6603K kernel code, 317K rwdata, 2344K rodata, 264K init, 265K bss, 15156K reserved, 49152K cma-reserved, 0K highmem)
[ 0.000000] Virtual kernel memory layout:
[ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB)
[ 0.000000] fixmap : 0xffc00000 - 0xfff00000 (3072 kB)
[ 0.000000] vmalloc : 0xe0800000 - 0xff800000 ( 496 MB)
[ 0.000000] lowmem : 0xc0000000 - 0xe0000000 ( 512 MB)
[ 0.000000] pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB)
[ 0.000000] modules : 0xbf000000 - 0xbfe00000 ( 14 MB)
[ 0.000000] .text : 0xc0008000 - 0xc08c5004 (8949 kB)
[ 0.000000] .init : 0xc08c6000 - 0xc0908000 ( 264 kB)
[ 0.000000] .data : 0xc0908000 - 0xc09574b0 ( 318 kB)
[ 0.000000] .bss : 0xc09574b0 - 0xc0999bd8 ( 266 kB)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
[ 0.000000] Preemptible hierarchical RCU implementation.
[ 0.000000] Build-time adjustment of leaf fanout to 32.
[ 0.000000] NR_IRQS:16 nr_irqs:16 16
[ 0.000000] IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts
[ 0.000000] OMAP clockevent source: timer2 at 24000000 Hz
[ 0.000031] sched_clock: 32 bits at 24MHz, resolution 41ns, wraps every 89478484971ns
[ 0.000081] clocksource: timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 79635851949 ns
[ 0.000105] OMAP clocksource: timer1 at 24000000 Hz
[ 0.000545] clocksource_probe: no matching clocksources found
[ 0.000929] Console: colour dummy device 80x30
[ 0.000987] WARNING: Your 'console=ttyO0' has been replaced by 'ttyS0'
[ 0.001004] This ensures that you still see kernel messages. Please
[ 0.001018] update your kernel commandline.
[ 0.001056] Calibrating delay loop... 298.59 BogoMIPS (lpj=1492992)
[ 0.067539] pid_max: default: 32768 minimum: 301
[ 0.067852] Mount-cache hash table entries: 1024 (order: 0, 4096 bytes)
[ 0.067881] Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes)
[ 0.069447] Initializing cgroup subsys io
[ 0.069512] Initializing cgroup subsys memory
[ 0.069592] Initializing cgroup subsys devices
[ 0.069627] Initializing cgroup subsys freezer
[ 0.069659] Initializing cgroup subsys perf_event
[ 0.069690] Initializing cgroup subsys pids
[ 0.069754] CPU: Testing write buffer coherency: ok
[ 0.070535] Setting up static identity map for 0x80008200 - 0x80008260
[ 0.075814] devtmpfs: initialized
[ 0.110191] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
[ 0.145995] omap_hwmod: debugss: _wait_target_disable failed
[ 0.218262] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
[ 0.226540] pinctrl core: initialized pinctrl subsystem
[ 0.229791] NET: Registered protocol family 16
[ 0.234972] DMA: preallocated 256 KiB pool for atomic coherent allocations
[ 0.257629] cpuidle: using governor ladder
[ 0.287608] cpuidle: using governor menu
[ 0.299069] OMAP GPIO hardware version 0.1
[ 0.320630] omap-gpmc 50000000.gpmc: could not find pctldev for node /ocp/l4_wkup@44c00000/scm@210000/pinmux@800/nandflash_pins_s0, deferring probe
[ 0.328164] hw-breakpoint: debug architecture 0x4 unsupported.
[ 0.389190] edma 49000000.edma: TI EDMA DMA engine driver
[ 0.400412] omap_i2c 44e0b000.i2c: could not find pctldev for node /ocp/l4_wkup@44c00000/scm@210000/pinmux@800/pinmux_i2c0_pins, deferring probe
[ 0.400547] omap_i2c 4819c000.i2c: could not find pctldev for node /ocp/l4_wkup@44c00000/scm@210000/pinmux@800/pinmux_i2c2_pins, deferring probe
[ 0.400905] media: Linux media interface: v0.10
[ 0.401078] Linux video capture interface: v2.00
[ 0.401205] pps_core: LinuxPPS API ver. 1 registered
[ 0.401226] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 0.401311] PTP clock support registered
[ 0.401457] EDAC MC: Ver: 3.0.0
[ 0.404215] omap-mailbox 480c8000.mailbox: omap mailbox rev 0x400
[ 0.405101] Advanced Linux Sound Architecture Driver Initialized.
[ 0.407968] clocksource: Switched to clocksource timer1
[ 0.435813] NET: Registered protocol family 2
[ 0.437557] TCP established hash table entries: 4096 (order: 2, 16384 bytes)
[ 0.437701] TCP bind hash table entries: 4096 (order: 2, 16384 bytes)
[ 0.437822] TCP: Hash tables configured (established 4096 bind 4096)
[ 0.438147] UDP hash table entries: 256 (order: 0, 4096 bytes)
[ 0.438198] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
[ 0.438569] NET: Registered protocol family 1
[ 0.439413] RPC: Registered named UNIX socket transport module.
[ 0.439445] RPC: Registered udp transport module.
[ 0.439463] RPC: Registered tcp transport module.
[ 0.439480] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.441528] hw perfevents: enabled with armv7_cortex_a8 PMU driver, 5 counters available
[ 0.446416] futex hash table entries: 256 (order: -1, 3072 bytes)
[ 0.467516] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[ 0.469818] NFS: Registering the id_resolver key type
[ 0.469947] Key type id_resolver registered
[ 0.469967] Key type id_legacy registered
[ 0.470148] ntfs: driver 2.1.32 [Flags: R/O].
[ 0.478522] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 247)
[ 0.478587] io scheduler noop registered
[ 0.478619] io scheduler deadline registered
[ 0.479040] io scheduler cfq registered (default)
[ 0.482588] pinctrl-single 44e10800.pinmux: 142 pins at pa f9e10800 size 568
[ 0.490519] backlight supply power not found, using dummy regulator
[ 0.651188] Serial: 8250/16550 driver, 10 ports, IRQ sharing disabled
[ 0.660808] 44e09000.serial: ttyS0 at MMIO 0x44e09000 (irq = 158, base_baud = 3000000) is a 8250
[ 1.289563] console [ttyS0] enabled
[ 1.295731] 48022000.serial: ttyS1 at MMIO 0x48022000 (irq = 159, base_baud = 3000000) is a 8250
[ 1.307480] [drm] Initialized drm 1.1.0 20060810
[ 1.318494] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).
[ 1.325176] [drm] No driver support for vblank timestamp query.
[ 1.379167] Console: switching to colour frame buffer device 100x30
[ 1.401709] tilcdc 4830e000.lcdc: fb0: frame buffer device
[ 1.428386] [drm] Initialized tilcdc 1.0.0 20121205 on minor 0
[ 1.451343] loop: module loaded
[ 1.463629] libphy: Fixed MDIO Bus: probed
[ 1.473478] mousedev: PS/2 mouse device common for all mice
[ 1.480616] i2c /dev entries driver
[ 1.487001] cpuidle: enable-method property 'ti,am3352' found operations
[ 1.518507] pinctrl-single 44e10800.pinmux: pin 44e1099c.0 already requested by 481a0000.spi; cannot claim for 47810000.mmc
[ 1.529878] pinctrl-single 44e10800.pinmux: pin-103 (47810000.mmc) status -22
[ 1.537149] pinctrl-single 44e10800.pinmux: could not request pin 103 (44e1099c.0) from group pinmux_wlan_pins on device pinctrl-single
[ 1.549676] omap_hsmmc 47810000.mmc: Error applying setting, reverse things back
[ 1.689929] ledtrig-cpu: registered to indicate activity on CPUs
[ 1.721289] NET: Registered protocol family 10
[ 1.739279] sit: IPv6 over IPv4 tunneling driver
[ 1.746031] NET: Registered protocol family 17
[ 1.758094] Key type dns_resolver registered
[ 1.762958] omap_voltage_late_init: Voltage driver support not added
[ 1.792816] omap-gpmc 50000000.gpmc: GPMC revision 6.0
[ 1.808073] gpmc_mem_init: disabling cs 0 mapped at 0x0-0x1000000
[ 1.817258] nand: device found, Manufacturer ID: 0x98, Chip ID: 0xda
[ 1.837993] nand: Toshiba NAND 256MiB 3,3V 8-bit
[ 1.842664] nand: 256 MiB, SLC, erase size: 128 KiB, page size: 2048, OOB size: 128
[ 1.858057] nand: using OMAP_ECC_BCH8_CODE_HW ECC scheme
[ 1.868210] 10 ofpart partitions found on MTD device 8000000.nand
[ 1.874347] Creating 10 MTD partitions on "8000000.nand":
[ 1.894756] 0x000000000000-0x000000020000 : "NAND.SPL"
[ 1.911022] 0x000000020000-0x000000040000 : "NAND.SPL.backup1"
[ 1.930811] 0x000000040000-0x000000060000 : "NAND.SPL.backup2"
[ 1.948281] 0x000000060000-0x000000080000 : "NAND.SPL.backup3"
[ 1.964979] 0x000000080000-0x0000000c0000 : "NAND.u-boot-spl-os"
[ 1.980207] 0x0000000c0000-0x0000001c0000 : "NAND.u-boot"
[ 2.001020] 0x0000001c0000-0x0000001e0000 : "NAND.u-boot-env"
[ 2.016592] 0x0000001e0000-0x000000200000 : "NAND.u-boot-env.backup1"
[ 2.030632] 0x000000200000-0x000000a00000 : "NAND.kernel"
[ 2.053991] 0x000000a00000-0x000010000000 : "NAND.file-system"
[ 4.308036] omap_i2c 44e0b000.i2c: controller timed out
[ 5.348409] tps65910 0-002d: No interrupt support, no core IRQ
[ 7.368030] omap_i2c 44e0b000.i2c: controller timed out
[ 10.428017] omap_i2c 44e0b000.i2c: controller timed out
[ 12.468009] omap_i2c 44e0b000.i2c: controller timed out
[ 12.488022] tps65910 0-002d: Error in configuring external control EN1
[ 12.494658] tps65910 0-002d: Failed to initialise ext control config
[ 14.518020] omap_i2c 44e0b000.i2c: controller timed out
[ 17.578012] omap_i2c 44e0b000.i2c: controller timed out
[ 17.598012] vrtc: failed to enable
[ 17.601737] tps65910 0-002d: failed to register tps65910-pmic regulator
[ 17.608499] tps65910-pmic: probe of tps65910-pmic failed with error -110
[ 17.616290] omap_i2c 44e0b000.i2c: bus 0 rev0.11 at 400 kHz
[ 17.624816] omap_i2c 4819c000.i2c: bus 2 rev0.11 at 400 kHz
[ 17.661372] input: volume_keys@0 as /devices/platform/volume_keys@0/input/input0
[ 17.672688] hctosys: unable to open rtc device (rtc0)
[ 17.686352] vbat: disabling
[ 17.689506] lis3_reg: disabling
[ 17.692687] wlan-en-regulator: disabling
[ 17.696857] ALSA device list:
[ 17.701101] No soundcards found.
[ 17.706872] Waiting for root device PARTUUID=d8c65ab4-02...
[ 17.706872] Waiting for root device PARTUUID=d8c65ab4-02...
[76.926502] random: nonblocking pool is initialized
We had thought PMIC had gone bad and replaced it. but still same error
Please help on resolving this issue.
Regards
Sujay A