Part Number: TMS320C6678
Hello,
I am developing a software sequence which goal is to test EDC/ECC mechanism of the DSP TMS302C6678.
The sequence is the following:
-
Enabling EDC ( in L1P, L2 and MSM) and ECC in DDR3
-
Initialization of L2, MSM and DDR3 to 0
-
Initialization of Memory protection, interrupts
-
Running EDC/ECC test
L2 EDC test consist in:
5-1/ Writing to an arbitrary L2 address (0x00868000 in my case) value 0xFFFFFFFF
N.B: 0x00868000 is an arbitrary address. The only condition is to choose an address were R/W/X are allowed.
5-2/ Suspend L2 EDC by setting bit 3 of L2EDCMD register to 1 (to suspend EDC computation)
5-3/ Write 0xFFFFFFF3 at address 0x00868000.
N.B: Value of 0xFFFFFFF3 is chosen because only two bits are different with previous value of 0xFFFFFFFF
N.B.2: Goal of this step is to simulate corruption of bits 2 and 3 at address 0x00868000. Parity RAM is not updated since EDC mechanism is suspended
5-4/ Enable L2 EDC mechanism by setting bit 0 of L2EDCMD register to 1
5-5/ Perform a read access at address 0x00868000
5-6/ Wait for L2 EDC interrupt
However, this sequence does not work (L2 EDC interrupt corresponding to corepac event 117 is never called).
I am suspecting that L2 write done during step 5-1 is not performed in 128 bits. I know that my instruction is a 32 bit write but Initialy I was thinking that the DSM memory controller will perform the access always in 128 bits. It seems that it is not the case. And if it is confirmed then corresponding parity ram is not updated as expected (because access is narrower than 128 bits, as explained in §11 of C66x corepac datasheet), only bit validity is updated.
So, I have tried to replace in my previous sequence, the step 5-1 by following one:
5-1-bis/Program IDMA to write value 0xFFFFFFFF at range [0x00868000--0x00868010] by setting IDMA register as following:
-
IDMA1_SOURCE is set to 0xFFFFFFFF
-
IDMA1_DEST is set to 0x00868000
-
IDMA1_COUNT is set to 0x00010010
With this only modification, my test becomes OK (i.e corepac event 117 is generated).
This seems to confirm my analysis of memory access not done in 128 bits.
I have performed a third test as follow:
5-1-ter/ Write 0xFFFFFFFF at address 0x00868000, 0x00868004, 0x00868008 and 0x0086800C in 4 assembly instructions
Result: Test is KO, and event 117 not generated. This seems to confirm that every DSP access is done in 32 bit.
So, my test works (using IDMA) but I have following questions:
Q1- If DSP R/W instructions are done in 32 bits, then parity RAM will never be updated and only bit validity will be set to invalid. Could you explain how a L2 memory corruption should be detected/corrected in this case?
Q2- There is a scrubbing technique described in §11.3.3 of C66x corepac datasheet. Is is the only method of detecting a L2 data corruption?
Q3- Can you explain me if there is a way to force every R/W accesses coming from DSP core to be done in 128 bits? If it is already the case, can you explain me what I am doing wrong in my test sequence?
Q4- I am trying to perform same kind of test in MSM memory but it seems complicated because as explained in §2.5.2.1 of SPRUGW7A “Setting ECM=1 enables error correction; however, any further writes to the ECM bit are ignored (that is, once enabled, error correction stays enabled until the MSMC is reset).”. Since ECC mechanism cannot be deactivated then it is impossible to test MSM EDC mechanism with my technique because it is impossible for me to “simulate” a MSM data corruption. Am I right or there is a other possibility to test it?
Q5- Same question for DDR3, is it possible to test DDR3 ECC mechanism (with the test sequence described below or by an other way)?
Thanks by advance for your answer.
Regards,