when I "rebuild all" the video_preview project, there are some error appear. But if I just compile File(press F7, not rebuild all), the compile is OK.
The errors are as following:
------------------------ video_preview.pjt - Release ------------------------
[video_preview.tcf] "C:\CCStudio_v3.3\bios_5_31_02\xdctools\tconf" -b -Dconfig.importPath=".;../common;C:/CCStudio_v3.3/bios_5_31_02/packages" video_preview.tcf
js: "C:/CCStudio_v3.3/bios_5_31_02/xdctools/include/utils.tci", line 484: exception from uncaught JavaScript throw: Error: Can't find import file: 'DM6437_common.tci' (not found along 'C:\dvsdk_1_01_00_15\examples\video_preview/;.;../common;C:/CCStudio_v3.3/bios_5_31_02/packages;C:\CCStudio_v3.3\bios_5_31_02\xdctools/include;C:\CCStudio_v3.3\bios_5_31_02\xdctools/packages')
"./video_preview.tcf", line 18
[i2c_params.c] "C:\CCStudio_v3.3\C6000\cgtools\bin\cl6x" -g -fr"C:/dvsdk_1_01_00_15/examples/video_preview/Release" -i"C:/dvsdk_1_01_00_15/examples/video_preview" -i"." -i"C:/CCStudio_v3.3/boards/evmdm6437_v1/include" -i"../../PSP_0_05_03/pspdrivers/inc" -i"../../PSP_0_05_03/pspdrivers/drivers/inc" -i"../../PSP_0_05_03/pspdrivers/system/DM6437/bios/dm6437_evm/src/video/src" -i"../../PSP_0_05_03/pspdrivers/soc/dm6437/dsp/inc" -mv6400+ -@"../video_preview/Release.lkf" "i2c_params.c"
"i2c_params.c", line 9: fatal error: could not open source file "psp_i2c.h"
1 fatal error detected in the compilation of "i2c_params.c".
Compilation terminated.
>> Compilation failure
[video_preview.c] "C:\CCStudio_v3.3\C6000\cgtools\bin\cl6x" -g -fr"C:/dvsdk_1_01_00_15/examples/video_preview/Release" -i"C:/dvsdk_1_01_00_15/examples/video_preview" -i"." -i"C:/CCStudio_v3.3/boards/evmdm6437_v1/include" -i"../../PSP_0_05_03/pspdrivers/inc" -i"../../PSP_0_05_03/pspdrivers/drivers/inc" -i"../../PSP_0_05_03/pspdrivers/system/DM6437/bios/dm6437_evm/src/video/src" -i"../../PSP_0_05_03/pspdrivers/soc/dm6437/dsp/inc" -mv6400+ -@"Release.lkf" "video_preview.c"
"video_preview.c", line 31: fatal error: could not open source file "psp_i2c.h"
1 fatal error detected in the compilation of "video_preview.c".
Compilation terminated.
>> Compilation failure
Build Complete,
3 Errors, 0 Warnings, 0 Remarks.
Please help me. Thank you very much!