Part Number: TMS320DM369
Hello,
According to the datasheet for the processor on page 45, VDD_ISIF18_33 is a power supply for switchable ISIF (3.3V/1.8V). Then it has the example:
VDD_ISIF_18_33 power supply can be at
1.8V for VPFE pin functionality or it can be at 3.3V if
other peripherals pin functionality is to be used like
SPI3 or GPIO or CLKOUT0, or USBDRVVBUS.
Does this mean that I can't use the VPFE functionality on a 3.3V device? My image sensor bridge IC has 3.3V logic, and if I didn't need a voltage translator for the TMS320DM369 ISIF interface, that would be great. Can someone please verify for me?
Thanks,
Gabe