This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/AM5728: Android build error

Part Number: AM5728


Tool/software: Linux

Hi Champs:

 I'm developing the AM57 Android.

 Issuing the "make all" & "make linux", I will have this build error.

 Any comments?

BR Rio

make[1]: Entering directory `/opt/ti-processor-sdk-android-am57xx-evm-04.00.00.04/board-support/linux-4.4.67+gitAUTOINC+6e995fe41a-g6e995fe41a'
CHK include/config/kernel.release
CHK include/generated/uapi/linux/version.h
CHK include/generated/utsrelease.h
make[2]: `include/generated/mach-types.h' is up to date.
CHK include/generated/bounds.h
CHK include/generated/timeconst.h
CHK include/generated/asm-offsets.h
CALL scripts/checksyscalls.sh
CHK include/generated/compile.h
GZIP kernel/config_data.gz
CHK kernel/config_data.h
DTC drivers/gpu/drm/tilcdc/tilcdc_slave_compat.dtb
DTB drivers/gpu/drm/tilcdc/tilcdc_slave_compat.dtb.S
AS drivers/gpu/drm/tilcdc/tilcdc_slave_compat.dtb.o
LD drivers/gpu/drm/tilcdc/built-in.o
rm drivers/gpu/drm/tilcdc/tilcdc_slave_compat.dtb drivers/gpu/drm/tilcdc/tilcdc_slave_compat.dtb.S
LD drivers/gpu/drm/built-in.o
LD drivers/gpu/built-in.o
LD drivers/built-in.o
LINK vmlinux
LD vmlinux.o
MODPOST vmlinux.o
GEN .version
CHK include/generated/compile.h
UPD include/generated/compile.h
CC init/version.o
LD init/built-in.o
KSYM .tmp_kallsyms1.o
KSYM .tmp_kallsyms2.o
LD vmlinux
SORTEX vmlinux
SYSMAP System.map
OBJCOPY arch/arm/boot/Image
Kernel: arch/arm/boot/Image is ready
Kernel: arch/arm/boot/Image is ready
LZO arch/arm/boot/compressed/piggy.lzo
/bin/sh: 1: lzop: not found
make[3]: *** [arch/arm/boot/compressed/piggy.lzo] Error 1
make[2]: *** [arch/arm/boot/compressed/vmlinux] Error 2
make[1]: *** [zImage] Error 2
make[1]: Leaving directory `/opt/ti-processor-sdk-android-am57xx-evm-04.00.00.04/board-support/linux-4.4.67+gitAUTOINC+6e995fe41a-g6e995fe41a'
make: *** [linux] Error 2