Other Parts Discussed in Thread: UNIFLASH, SYSBIOS
Tool/software: Code Composer Studio
Hi
I am developing custom board following AM437x IDK 1.4A circuit.
This custom board only have EnDat, ICSS Ethernet port and 20 pin cTI JTAG.
I use SYSBIOS ind SDK 02.01.03.02 develop EtherCAT + EnDat application, and want to flash QSPI flash via UniFlash.
Following the guide http://processors.wiki.ti.com/index.php/Sitara_Uniflash_Quick_Start_Guide
I installed Uniflash 3.4.1.00012 on Win7(32bit)
But I get confuse to these problem
1. What files I need to put into TFTP home folder ?
2. Can I flash using ICSS Ethernet port ?
3. Can I flash using JTAG via CCS6.2.0 ?
Thanks a lot
Yi-Lin