Other Parts Discussed in Thread: WL1271, , ADS7846, TSC2007, TSC2004, PCF8574, TPS65010, TPS65910, BQ24022, LP3971, LP3972, TPS65023, TLV320AIC23B, TVP5150, TVP7002, THS7303, TLV320AIC3110, DA8XX, LP3944, LP5521, LP5523, DAC124S085, TLV320AIC3104, BQ32000
Hello,
I have been searching for a solution with no resolution for the issue I am having implementing a wl1271 wlan module into my Customized DM385 board with IPNC RDK 3.5 version, kernel v2.6.37, angstom
The WL1271 is connected to the first mmc 1 sdio and I have two gpio modules used for wlan enable (gpio3_0) and wlan_irq (gpio3_1). The second mmc is used for the SD card.
I have added the code to my board definition file and built the .ko module files. It appears the modules are loaded properly but I get "ifconfig: SIOCGIFFLAGS: No such device" when trying to bring the wlan up.
I added wl1271-fw.bin and wl1271-nvs.bin to thefilsys lib/firmware/ti-connectivity . I also tried installing them in /firmware/ti-connectivity
I have searched this error for several days and can't seem to identify the problem. SHould I be using wlcore and/or wpa_supplicant? It's not clear which if any are required. Any help would be appreciated.
Here are some guides I have read:
http://processors.wiki.ti.com/index.php/WL127x_Porting_Guide
Below are system responses and my associated files.
root@dm814x-evm:/# insmod /opt/ipnc/kermod/wl1271.ko
root@dm814x-evm:/# insmod /opt/ipnc/kermod/wl1271_sdio.ko
root@dm814x-evm:/# lsmod
Module Size Used by
wl1271_sdio 2748 0
wl1271 86942 1 wl1271_sdio
syslink 772850 0
root@dm814x-evm:/# ifconfig wlan0 up
ifconfig: SIOCGIFFLAGS: No such device
root@dm814x-evm:/# modinfo /opt/ipnc/kermod/wl1271_sdio.ko
filename: /opt/ipnc/kermod/wl1271_sdio.ko
firmware: wl1271-fw.bin
author: Juuso Oikarinen <juuso.oikarinen@nokia.com>
author: Luciano Coelho <luciano.coelho@nokia.com>
license: GPL
alias: sdio:c*v0097d4076*
depends: wl1271
vermagic: 2.6.37_DM385_CBB_1.50.50 mod_unload modversions ARMv7 p2v8
root@dm814x-evm:/# modinfo /opt/ipnc/kermod/wl1271.ko
filename: /opt/ipnc/kermod/wl1271.ko
author: Juuso Oikarinen <juuso.oikarinen@nokia.com>
author: Luciano Coelho <luciano.coelho@nokia.com>
license: GPL
depends:
vermagic: 2.6.37_DM385_CBB_1.50.50 mod_unload modversions ARMv7 p2v8
root@dm814x-evm:/#
My board dm385_cbb_ubifs_defconfig file is below:
#######################################################################################################################################################
# Mark Smith to enable TI wl1271 sdio driver for wireless communication.
# Linux/arm 2.6.37 Kernel Configuration
# Tue Aug 15 09:35:19 2017
#
CONFIG_ARM=y
# CONFIG_HAVE_PWM is not set
CONFIG_SYS_SUPPORTS_APM_EMULATION=y
CONFIG_GENERIC_GPIO=y
# CONFIG_ARCH_USES_GETTIMEOFFSET is not set
CONFIG_GENERIC_CLOCKEVENTS=y
CONFIG_HAVE_PROC_CPU=y
CONFIG_GENERIC_HARDIRQS=y
CONFIG_STACKTRACE_SUPPORT=y
CONFIG_HAVE_LATENCYTOP_SUPPORT=y
CONFIG_LOCKDEP_SUPPORT=y
CONFIG_TRACE_IRQFLAGS_SUPPORT=y
CONFIG_HARDIRQS_SW_RESEND=y
CONFIG_GENERIC_IRQ_PROBE=y
CONFIG_RWSEM_GENERIC_SPINLOCK=y
CONFIG_ARCH_HAS_CPUFREQ=y
CONFIG_ARCH_HAS_CPU_IDLE_WAIT=y
CONFIG_GENERIC_HWEIGHT=y
CONFIG_GENERIC_CALIBRATE_DELAY=y
CONFIG_NEED_DMA_MAP_STATE=y
CONFIG_GENERIC_HARDIRQS_NO__DO_IRQ=y
CONFIG_ARM_L1_CACHE_SHIFT_6=y
CONFIG_VECTORS_BASE=0xffff0000
CONFIG_ARM_PATCH_PHYS_VIRT=y
CONFIG_DEFCONFIG_LIST="/lib/modules/$UNAME_RELEASE/.config"
CONFIG_CONSTRUCTORS=y
CONFIG_HAVE_IRQ_WORK=y
#
# General setup
#
CONFIG_EXPERIMENTAL=y
CONFIG_BROKEN_ON_SMP=y
CONFIG_INIT_ENV_ARG_LIMIT=32
CONFIG_CROSS_COMPILE=""
CONFIG_LOCALVERSION="_DM385_CBB_1.50.50"
CONFIG_LOCALVERSION_AUTO=y
CONFIG_HAVE_KERNEL_GZIP=y
CONFIG_HAVE_KERNEL_LZMA=y
CONFIG_HAVE_KERNEL_LZO=y
CONFIG_KERNEL_GZIP=y
# CONFIG_KERNEL_LZMA is not set
# CONFIG_KERNEL_LZO is not set
# CONFIG_SWAP is not set
CONFIG_SYSVIPC=y
CONFIG_SYSVIPC_SYSCTL=y
CONFIG_POSIX_MQUEUE=y
CONFIG_POSIX_MQUEUE_SYSCTL=y
CONFIG_BSD_PROCESS_ACCT=y
# CONFIG_BSD_PROCESS_ACCT_V3 is not set
# CONFIG_TASKSTATS is not set
# CONFIG_AUDIT is not set
# CONFIG_HAVE_GENERIC_HARDIRQS is not set
# CONFIG_SPARSE_IRQ is not set
#
# RCU Subsystem
#
CONFIG_TINY_RCU=y
# CONFIG_PREEMPT_RCU is not set
# CONFIG_TREE_RCU_TRACE is not set
CONFIG_IKCONFIG=y
CONFIG_IKCONFIG_PROC=y
CONFIG_LOG_BUF_SHIFT=17
# CONFIG_CGROUPS is not set
CONFIG_NAMESPACES=y
# CONFIG_UTS_NS is not set
# CONFIG_IPC_NS is not set
# CONFIG_USER_NS is not set
# CONFIG_PID_NS is not set
# CONFIG_NET_NS is not set
# CONFIG_SYSFS_DEPRECATED is not set
# CONFIG_RELAY is not set
CONFIG_BLK_DEV_INITRD=y
CONFIG_INITRAMFS_SOURCE=""
CONFIG_RD_GZIP=y
CONFIG_RD_BZIP2=y
CONFIG_RD_LZMA=y
CONFIG_RD_LZO=y
CONFIG_CC_OPTIMIZE_FOR_SIZE=y
CONFIG_SYSCTL=y
CONFIG_ANON_INODES=y
# CONFIG_EMBEDDED is not set
CONFIG_UID16=y
CONFIG_SYSCTL_SYSCALL=y
CONFIG_KALLSYMS=y
# CONFIG_KALLSYMS_ALL is not set
CONFIG_KALLSYMS_EXTRA_PASS=y
CONFIG_HOTPLUG=y
CONFIG_PRINTK=y
CONFIG_BUG=y
CONFIG_ELF_CORE=y
CONFIG_BASE_FULL=y
CONFIG_FUTEX=y
CONFIG_EPOLL=y
CONFIG_SIGNALFD=y
CONFIG_TIMERFD=y
CONFIG_EVENTFD=y
CONFIG_SHMEM=y
CONFIG_AIO=y
CONFIG_HAVE_PERF_EVENTS=y
CONFIG_PERF_USE_VMALLOC=y
#
# Kernel Performance Events And Counters
#
# CONFIG_PERF_EVENTS is not set
# CONFIG_PERF_COUNTERS is not set
CONFIG_VM_EVENT_COUNTERS=y
CONFIG_SLUB_DEBUG=y
CONFIG_COMPAT_BRK=y
# CONFIG_SLAB is not set
CONFIG_SLUB=y
# CONFIG_PROFILING is not set
CONFIG_HAVE_OPROFILE=y
CONFIG_KPROBES=y
CONFIG_KRETPROBES=y
CONFIG_HAVE_KPROBES=y
CONFIG_HAVE_KRETPROBES=y
CONFIG_HAVE_REGS_AND_STACK_ACCESS_API=y
CONFIG_HAVE_CLK=y
#
# GCOV-based kernel profiling
#
# CONFIG_GCOV_KERNEL is not set
CONFIG_HAVE_GENERIC_DMA_COHERENT=y
CONFIG_SLABINFO=y
CONFIG_RT_MUTEXES=y
CONFIG_BASE_SMALL=0
CONFIG_MODULES=y
# CONFIG_MODULE_FORCE_LOAD is not set
CONFIG_MODULE_UNLOAD=y
# CONFIG_MODULE_FORCE_UNLOAD is not set
CONFIG_MODVERSIONS=y
# CONFIG_MODULE_SRCVERSION_ALL is not set
CONFIG_BLOCK=y
# CONFIG_LBDAF is not set
# CONFIG_BLK_DEV_BSG is not set
# CONFIG_BLK_DEV_INTEGRITY is not set
#
# IO Schedulers
#
CONFIG_IOSCHED_NOOP=y
CONFIG_IOSCHED_DEADLINE=y
CONFIG_IOSCHED_CFQ=y
# CONFIG_DEFAULT_DEADLINE is not set
CONFIG_DEFAULT_CFQ=y
# CONFIG_DEFAULT_NOOP is not set
CONFIG_DEFAULT_IOSCHED="cfq"
#
# sbull Driver
#
CONFIG_SBULL=m
# CONFIG_INLINE_SPIN_TRYLOCK is not set
# CONFIG_INLINE_SPIN_TRYLOCK_BH is not set
# CONFIG_INLINE_SPIN_LOCK is not set
# CONFIG_INLINE_SPIN_LOCK_BH is not set
# CONFIG_INLINE_SPIN_LOCK_IRQ is not set
# CONFIG_INLINE_SPIN_LOCK_IRQSAVE is not set
CONFIG_INLINE_SPIN_UNLOCK=y
# CONFIG_INLINE_SPIN_UNLOCK_BH is not set
CONFIG_INLINE_SPIN_UNLOCK_IRQ=y
# CONFIG_INLINE_SPIN_UNLOCK_IRQRESTORE is not set
# CONFIG_INLINE_READ_TRYLOCK is not set
# CONFIG_INLINE_READ_LOCK is not set
# CONFIG_INLINE_READ_LOCK_BH is not set
# CONFIG_INLINE_READ_LOCK_IRQ is not set
# CONFIG_INLINE_READ_LOCK_IRQSAVE is not set
CONFIG_INLINE_READ_UNLOCK=y
# CONFIG_INLINE_READ_UNLOCK_BH is not set
CONFIG_INLINE_READ_UNLOCK_IRQ=y
# CONFIG_INLINE_READ_UNLOCK_IRQRESTORE is not set
# CONFIG_INLINE_WRITE_TRYLOCK is not set
# CONFIG_INLINE_WRITE_LOCK is not set
# CONFIG_INLINE_WRITE_LOCK_BH is not set
# CONFIG_INLINE_WRITE_LOCK_IRQ is not set
# CONFIG_INLINE_WRITE_LOCK_IRQSAVE is not set
CONFIG_INLINE_WRITE_UNLOCK=y
# CONFIG_INLINE_WRITE_UNLOCK_BH is not set
CONFIG_INLINE_WRITE_UNLOCK_IRQ=y
# CONFIG_INLINE_WRITE_UNLOCK_IRQRESTORE is not set
# CONFIG_MUTEX_SPIN_ON_OWNER is not set
CONFIG_FREEZER=y
#
# System Type
#
CONFIG_MMU=y
# CONFIG_ARCH_AAEC2000 is not set
# CONFIG_ARCH_INTEGRATOR is not set
# CONFIG_ARCH_REALVIEW is not set
# CONFIG_ARCH_VERSATILE is not set
# CONFIG_ARCH_VEXPRESS is not set
# CONFIG_ARCH_AT91 is not set
# CONFIG_ARCH_BCMRING is not set
# CONFIG_ARCH_CLPS711X is not set
# CONFIG_ARCH_CNS3XXX is not set
# CONFIG_ARCH_GEMINI is not set
# CONFIG_ARCH_EBSA110 is not set
# CONFIG_ARCH_EP93XX is not set
# CONFIG_ARCH_FOOTBRIDGE is not set
# CONFIG_ARCH_MXC is not set
# CONFIG_ARCH_STMP3XXX is not set
# CONFIG_ARCH_NETX is not set
# CONFIG_ARCH_H720X is not set
# CONFIG_ARCH_IOP13XX is not set
# CONFIG_ARCH_IOP32X is not set
# CONFIG_ARCH_IOP33X is not set
# CONFIG_ARCH_IXP23XX is not set
# CONFIG_ARCH_IXP2000 is not set
# CONFIG_ARCH_IXP4XX is not set
# CONFIG_ARCH_DOVE is not set
# CONFIG_ARCH_KIRKWOOD is not set
# CONFIG_ARCH_LOKI is not set
# CONFIG_ARCH_LPC32XX is not set
# CONFIG_ARCH_MV78XX0 is not set
# CONFIG_ARCH_ORION5X is not set
# CONFIG_ARCH_MMP is not set
# CONFIG_ARCH_KS8695 is not set
# CONFIG_ARCH_NS9XXX is not set
# CONFIG_ARCH_W90X900 is not set
# CONFIG_ARCH_NUC93X is not set
# CONFIG_ARCH_TEGRA is not set
# CONFIG_ARCH_PNX4008 is not set
# CONFIG_ARCH_PXA is not set
# CONFIG_ARCH_MSM is not set
# CONFIG_ARCH_SHMOBILE is not set
# CONFIG_ARCH_RPC is not set
# CONFIG_ARCH_SA1100 is not set
# CONFIG_ARCH_S3C2410 is not set
# CONFIG_ARCH_S3C64XX is not set
# CONFIG_ARCH_S5P64X0 is not set
# CONFIG_ARCH_S5P6442 is not set
# CONFIG_ARCH_S5PC100 is not set
# CONFIG_ARCH_S5PV210 is not set
# CONFIG_ARCH_S5PV310 is not set
# CONFIG_ARCH_SHARK is not set
# CONFIG_ARCH_TCC_926 is not set
# CONFIG_ARCH_LH7A40X is not set
# CONFIG_ARCH_U300 is not set
# CONFIG_ARCH_U8500 is not set
# CONFIG_ARCH_NOMADIK is not set
# CONFIG_ARCH_DAVINCI is not set
CONFIG_ARCH_OMAP=y
# CONFIG_PLAT_SPEAR is not set
#
# TI OMAP Common Features
#
# CONFIG_ARCH_OMAP1 is not set
CONFIG_ARCH_OMAP2PLUS=y
#
# OMAP Feature Selections
#
# CONFIG_OMAP_RESET_CLOCKS is not set
CONFIG_OMAP_MUX=y
# CONFIG_OMAP_MUX_DEBUG is not set
CONFIG_OMAP_MUX_WARNINGS=y
# CONFIG_OMAP_MCBSP is not set
CONFIG_OMAP_MBOX_FWK=y
CONFIG_OMAP_MBOX_KFIFO_SIZE=256
CONFIG_OMAP_IOMMU=y
# CONFIG_OMAP_IOMMU_DEBUG is not set
CONFIG_OMAP_MPU_TIMER=y
# CONFIG_OMAP_32K_TIMER is not set
CONFIG_OMAP_DM_TIMER=y
# CONFIG_OMAP_PM_NONE is not set
CONFIG_OMAP_PM_NOOP=y
#
# TI OMAP2/3/4 Specific Features
#
CONFIG_ARCH_OMAP2PLUS_TYPICAL=y
# CONFIG_ARCH_OMAP2 is not set
# CONFIG_ARCH_OMAP3 is not set
# CONFIG_ARCH_OMAP4 is not set
CONFIG_ARCH_TI81XX=y
# CONFIG_ARCH_TI816X is not set
CONFIG_ARCH_TI814X=y
#
# OMAP Board Type
#
#
# TI81XX Board Type
#
# CONFIG_MACH_TI8148IPNC is not set
CONFIG_MACH_TI8148EVM=y
# CONFIG_MACH_DM385EVM is not set
# CONFIG_MACH_TI811XEVM is not set
# CONFIG_MACH_DM385IPNC is not set
CONFIG_MACH_DM385CBB=y
# CONFIG_TI8148_EVM_OPTIMIZED is not set
#
# Processor Type
#
CONFIG_CPU_32v6K=y
CONFIG_CPU_V7=y
CONFIG_CPU_32v7=y
CONFIG_CPU_ABRT_EV7=y
CONFIG_CPU_PABRT_V7=y
CONFIG_CPU_CACHE_V7=y
CONFIG_CPU_CACHE_VIPT=y
CONFIG_CPU_COPY_V6=y
CONFIG_CPU_TLB_V7=y
CONFIG_CPU_HAS_ASID=y
CONFIG_CPU_CP15=y
CONFIG_CPU_CP15_MMU=y
#
# Processor Features
#
CONFIG_ARM_THUMB=y
# CONFIG_ARM_THUMBEE is not set
# CONFIG_CPU_ICACHE_DISABLE is not set
# CONFIG_CPU_DCACHE_DISABLE is not set
# CONFIG_CPU_BPREDICT_DISABLE is not set
CONFIG_ARM_L1_CACHE_SHIFT=6
CONFIG_ARM_DMA_MEM_BUFFERABLE=y
CONFIG_CPU_HAS_PMU=y
# CONFIG_ARM_ERRATA_430973 is not set
# CONFIG_ARM_ERRATA_458693 is not set
# CONFIG_ARM_ERRATA_460075 is not set
# CONFIG_ARM_ERRATA_743622 is not set
CONFIG_COMMON_CLKDEV=y
#
# Bus support
#
# CONFIG_PCI is not set
# CONFIG_PCI_SYSCALL is not set
CONFIG_ARCH_SUPPORTS_MSI=y
# CONFIG_PCCARD is not set
#
# Kernel Features
#
CONFIG_TICK_ONESHOT=y
CONFIG_NO_HZ=y
CONFIG_HIGH_RES_TIMERS=y
CONFIG_GENERIC_CLOCKEVENTS_BUILD=y
CONFIG_VMSPLIT_3G=y
# CONFIG_VMSPLIT_2G is not set
# CONFIG_VMSPLIT_1G is not set
CONFIG_PAGE_OFFSET=0xC0000000
CONFIG_PREEMPT_NONE=y
# CONFIG_PREEMPT_VOLUNTARY is not set
# CONFIG_PREEMPT is not set
CONFIG_HZ=100
# CONFIG_THUMB2_KERNEL is not set
CONFIG_AEABI=y
CONFIG_OABI_COMPAT=y
CONFIG_ARCH_HAS_HOLES_MEMORYMODEL=y
# CONFIG_ARCH_SPARSEMEM_DEFAULT is not set
# CONFIG_ARCH_SELECT_MEMORY_MODEL is not set
CONFIG_HIGHMEM=y
# CONFIG_HIGHPTE is not set
CONFIG_SELECT_MEMORY_MODEL=y
CONFIG_FLATMEM_MANUAL=y
CONFIG_FLATMEM=y
CONFIG_FLAT_NODE_MEM_MAP=y
CONFIG_HAVE_MEMBLOCK=y
CONFIG_PAGEFLAGS_EXTENDED=y
CONFIG_SPLIT_PTLOCK_CPUS=4
# CONFIG_PHYS_ADDR_T_64BIT is not set
CONFIG_ZONE_DMA_FLAG=0
CONFIG_BOUNCE=y
CONFIG_VIRT_TO_BUS=y
# CONFIG_KSM is not set
CONFIG_DEFAULT_MMAP_MIN_ADDR=4096
CONFIG_NEED_PER_CPU_KM=y
CONFIG_FORCE_MAX_ZONEORDER=11
# CONFIG_LEDS is not set
CONFIG_ALIGNMENT_TRAP=y
# CONFIG_UACCESS_WITH_MEMCPY is not set
# CONFIG_SECCOMP is not set
# CONFIG_CC_STACKPROTECTOR is not set
# CONFIG_DEPRECATED_PARAM_STRUCT is not set
#
# Boot options
#
CONFIG_ZBOOT_ROM_TEXT=0
CONFIG_ZBOOT_ROM_BSS=0
CONFIG_CMDLINE=""
# CONFIG_XIP_KERNEL is not set
# CONFIG_KEXEC is not set
CONFIG_AUTO_ZRELADDR=y
#
# CPU Power Management
#
# CONFIG_CPU_FREQ is not set
# CONFIG_CPU_IDLE is not set
#
# Floating point emulation
#
#
# At least one emulation must be selected
#
CONFIG_FPE_NWFPE=y
# CONFIG_FPE_NWFPE_XP is not set
# CONFIG_FPE_FASTFPE is not set
CONFIG_VFP=y
CONFIG_VFPv3=y
CONFIG_NEON=y
#
# Userspace binary formats
#
CONFIG_BINFMT_ELF=y
# CONFIG_CORE_DUMP_DEFAULT_ELF_HEADERS is not set
CONFIG_HAVE_AOUT=y
# CONFIG_BINFMT_AOUT is not set
CONFIG_BINFMT_MISC=y
#
# Power management options
#
CONFIG_PM=y
CONFIG_PM_DEBUG=y
# CONFIG_PM_ADVANCED_DEBUG is not set
CONFIG_PM_VERBOSE=y
CONFIG_CAN_PM_TRACE=y
CONFIG_PM_SLEEP=y
CONFIG_SUSPEND_NVS=y
CONFIG_SUSPEND=y
# CONFIG_PM_TEST_SUSPEND is not set
CONFIG_SUSPEND_FREEZER=y
# CONFIG_APM_EMULATION is not set
CONFIG_PM_RUNTIME=y
CONFIG_PM_OPS=y
# CONFIG_ARCH_HAS_OPP is not set
CONFIG_ARCH_SUSPEND_POSSIBLE=y
CONFIG_NET=y
#
# Networking options
#
CONFIG_PACKET=y
CONFIG_UNIX=y
CONFIG_XFRM=y
# CONFIG_XFRM_USER is not set
# CONFIG_XFRM_SUB_POLICY is not set
# CONFIG_XFRM_MIGRATE is not set
# CONFIG_XFRM_STATISTICS is not set
# CONFIG_NET_KEY is not set
CONFIG_INET=y
CONFIG_IP_MULTICAST=y
# CONFIG_IP_ADVANCED_ROUTER is not set
CONFIG_IP_FIB_HASH=y
CONFIG_IP_PNP=y
CONFIG_IP_PNP_DHCP=y
CONFIG_IP_PNP_BOOTP=y
CONFIG_IP_PNP_RARP=y
# CONFIG_NET_IPIP is not set
# CONFIG_NET_IPGRE_DEMUX is not set
# CONFIG_IP_MROUTE is not set
# CONFIG_ARPD is not set
# CONFIG_SYN_COOKIES is not set
# CONFIG_INET_AH is not set
# CONFIG_INET_ESP is not set
# CONFIG_INET_IPCOMP is not set
# CONFIG_INET_XFRM_TUNNEL is not set
CONFIG_INET_TUNNEL=m
CONFIG_INET_XFRM_MODE_TRANSPORT=y
CONFIG_INET_XFRM_MODE_TUNNEL=y
CONFIG_INET_XFRM_MODE_BEET=y
CONFIG_INET_LRO=y
CONFIG_INET_DIAG=y
CONFIG_INET_TCP_DIAG=y
# CONFIG_TCP_CONG_ADVANCED is not set
CONFIG_TCP_CONG_CUBIC=y
CONFIG_DEFAULT_TCP_CONG="cubic"
# CONFIG_TCP_MD5SIG is not set
CONFIG_IPV6=m
# CONFIG_IPV6_PRIVACY is not set
# CONFIG_IPV6_ROUTER_PREF is not set
# CONFIG_IPV6_OPTIMISTIC_DAD is not set
# CONFIG_INET6_AH is not set
# CONFIG_INET6_ESP is not set
# CONFIG_INET6_IPCOMP is not set
# CONFIG_IPV6_MIP6 is not set
# CONFIG_INET6_XFRM_TUNNEL is not set
# CONFIG_INET6_TUNNEL is not set
CONFIG_INET6_XFRM_MODE_TRANSPORT=m
CONFIG_INET6_XFRM_MODE_TUNNEL=m
CONFIG_INET6_XFRM_MODE_BEET=m
# CONFIG_INET6_XFRM_MODE_ROUTEOPTIMIZATION is not set
CONFIG_IPV6_SIT=m
# CONFIG_IPV6_SIT_6RD is not set
CONFIG_IPV6_NDISC_NODETYPE=y
# CONFIG_IPV6_TUNNEL is not set
# CONFIG_IPV6_MULTIPLE_TABLES is not set
# CONFIG_IPV6_MROUTE is not set
# CONFIG_NETLABEL is not set
# CONFIG_NETWORK_SECMARK is not set
# CONFIG_NETWORK_PHY_TIMESTAMPING is not set
# CONFIG_NETFILTER is not set
# CONFIG_IP_DCCP is not set
# CONFIG_IP_SCTP is not set
# CONFIG_RDS is not set
# CONFIG_TIPC is not set
# CONFIG_ATM is not set
# CONFIG_L2TP is not set
# CONFIG_BRIDGE is not set
# CONFIG_NET_DSA is not set
# CONFIG_VLAN_8021Q is not set
# CONFIG_DECNET is not set
# CONFIG_LLC2 is not set
# CONFIG_IPX is not set
# CONFIG_ATALK is not set
# CONFIG_X25 is not set
# CONFIG_LAPB is not set
# CONFIG_ECONET is not set
# CONFIG_WAN_ROUTER is not set
# CONFIG_PHONET is not set
# CONFIG_IEEE802154 is not set
# CONFIG_NET_SCHED is not set
# CONFIG_DCB is not set
CONFIG_DNS_RESOLVER=y
#
# Network testing
#
# CONFIG_NET_PKTGEN is not set
# CONFIG_NET_TCPPROBE is not set
# CONFIG_HAMRADIO is not set
# CONFIG_CAN is not set
# CONFIG_IRDA is not set
# CONFIG_BT is not set
# CONFIG_AF_RXRPC is not set
CONFIG_WIRELESS=y
CONFIG_WEXT_CORE=y
CONFIG_WEXT_PROC=y
CONFIG_CFG80211=y
# CONFIG_NL80211_TESTMODE is not set
# CONFIG_CFG80211_DEVELOPER_WARNINGS is not set
# CONFIG_CFG80211_REG_DEBUG is not set
CONFIG_CFG80211_DEFAULT_PS=y
# CONFIG_CFG80211_DEBUGFS is not set
# CONFIG_CFG80211_INTERNAL_REGDB is not set
CONFIG_CFG80211_WEXT=y
CONFIG_WIRELESS_EXT_SYSFS=y
# CONFIG_LIB80211 is not set
CONFIG_MAC80211=y
CONFIG_MAC80211_HAS_RC=y
CONFIG_MAC80211_RC_MINSTREL=y
CONFIG_MAC80211_RC_MINSTREL_HT=y
CONFIG_MAC80211_RC_DEFAULT_MINSTREL=y
CONFIG_MAC80211_RC_DEFAULT="minstrel_ht"
# CONFIG_MAC80211_MESH is not set
# CONFIG_MAC80211_LEDS is not set
# CONFIG_MAC80211_DEBUGFS is not set
# CONFIG_MAC80211_DEBUG_MENU is not set
#CONFIG_WIMAX =y
CONFIG_RFKILL=y
# CONFIG_NET_9P is not set
# CONFIG_CAIF is not set
# CONFIG_CEPH_LIB is not set
#
# Device Drivers
#
#
# Generic Driver Options
#
CONFIG_UEVENT_HELPER_PATH=""
CONFIG_DEVTMPFS=y
CONFIG_DEVTMPFS_MOUNT=y
CONFIG_STANDALONE=y
CONFIG_PREVENT_FIRMWARE_BUILD=y
CONFIG_FW_LOADER=y
CONFIG_FIRMWARE_IN_KERNEL=y
CONFIG_EXTRA_FIRMWARE=""
# CONFIG_DEBUG_DRIVER is not set
# CONFIG_DEBUG_DEVRES is not set
# CONFIG_SYS_HYPERVISOR is not set
# CONFIG_CONNECTOR is not set
CONFIG_MTD=y
# CONFIG_MTD_DEBUG is not set
# CONFIG_MTD_TESTS is not set
CONFIG_MTD_CONCAT=y
CONFIG_MTD_PARTITIONS=y
# CONFIG_MTD_REDBOOT_PARTS is not set
CONFIG_MTD_CMDLINE_PARTS=y
# CONFIG_MTD_AFS_PARTS is not set
# CONFIG_MTD_AR7_PARTS is not set
#
# User Modules And Translation Layers
#
CONFIG_MTD_CHAR=y
CONFIG_MTD_BLKDEVS=y
CONFIG_MTD_BLOCK=y
# CONFIG_FTL is not set
# CONFIG_NFTL is not set
# CONFIG_INFTL is not set
# CONFIG_RFD_FTL is not set
# CONFIG_SSFDC is not set
# CONFIG_SM_FTL is not set
# CONFIG_MTD_OOPS is not set
#
# RAM/ROM/Flash chip drivers
#
# CONFIG_MTD_CFI is not set
# CONFIG_MTD_JEDECPROBE is not set
CONFIG_MTD_MAP_BANK_WIDTH_1=y
CONFIG_MTD_MAP_BANK_WIDTH_2=y
CONFIG_MTD_MAP_BANK_WIDTH_4=y
# CONFIG_MTD_MAP_BANK_WIDTH_8 is not set
# CONFIG_MTD_MAP_BANK_WIDTH_16 is not set
# CONFIG_MTD_MAP_BANK_WIDTH_32 is not set
CONFIG_MTD_CFI_I1=y
CONFIG_MTD_CFI_I2=y
# CONFIG_MTD_CFI_I4 is not set
# CONFIG_MTD_CFI_I8 is not set
# CONFIG_MTD_RAM is not set
# CONFIG_MTD_ROM is not set
# CONFIG_MTD_ABSENT is not set
#
# Mapping drivers for chip access
#
# CONFIG_MTD_COMPLEX_MAPPINGS is not set
# CONFIG_MTD_PLATRAM is not set
#
# Self-contained MTD device drivers
#
# CONFIG_MTD_DATAFLASH is not set
# CONFIG_MTD_M25P80 is not set
# CONFIG_MTD_SST25L is not set
# CONFIG_MTD_SLRAM is not set
# CONFIG_MTD_PHRAM is not set
# CONFIG_MTD_MTDRAM is not set
# CONFIG_MTD_BLOCK2MTD is not set
#
# Disk-On-Chip Device Drivers
#
# CONFIG_MTD_DOC2000 is not set
# CONFIG_MTD_DOC2001 is not set
# CONFIG_MTD_DOC2001PLUS is not set
CONFIG_MTD_NAND_ECC=y
# CONFIG_MTD_NAND_ECC_SMC is not set
CONFIG_MTD_NAND=y
# CONFIG_MTD_NAND_VERIFY_WRITE is not set
# CONFIG_ECC_BCH8_OFF is not set
# CONFIG_MTD_SM_COMMON is not set
# CONFIG_MTD_NAND_MUSEUM_IDS is not set
# CONFIG_MTD_NAND_GPIO is not set
CONFIG_MTD_NAND_OMAP2=y
# CONFIG_MTD_NAND_OMAP_ECC_BCH16_CODE_HW is not set
CONFIG_MTD_NAND_OMAP_ECC_BCH8_CODE_HW=y
# CONFIG_MTD_NAND_OMAP_ECC_BCH4_CODE_HW is not set
# CONFIG_MTD_NAND_OMAP_ECC_HAMMING_CODE_HW is not set
# CONFIG_MTD_NAND_OMAP_ECC_HAMMING_CODE_SW is not set
CONFIG_MTD_NAND_IDS=y
# CONFIG_MTD_NAND_DISKONCHIP is not set
# CONFIG_MTD_NAND_NANDSIM is not set
# CONFIG_MTD_NAND_PLATFORM is not set
# CONFIG_MTD_ONENAND is not set
#
# LPDDR flash memory drivers
#
# CONFIG_MTD_LPDDR is not set
CONFIG_MTD_UBI=y
CONFIG_MTD_UBI_WL_THRESHOLD=4096
CONFIG_MTD_UBI_BEB_RESERVE=1
# CONFIG_MTD_UBI_GLUEBI is not set
# CONFIG_MTD_UBI_DEBUG is not set
# CONFIG_PARPORT is not set
CONFIG_BLK_DEV=y
# CONFIG_BLK_DEV_COW_COMMON is not set
CONFIG_BLK_DEV_LOOP=y
# CONFIG_BLK_DEV_CRYPTOLOOP is not set
#
# DRBD disabled because PROC_FS, INET or CONNECTOR not selected
#
# CONFIG_BLK_DEV_NBD is not set
CONFIG_BLK_DEV_RAM=y
CONFIG_BLK_DEV_RAM_COUNT=16
CONFIG_BLK_DEV_RAM_SIZE=32768
# CONFIG_BLK_DEV_XIP is not set
# CONFIG_CDROM_PKTCDVD is not set
# CONFIG_ATA_OVER_ETH is not set
# CONFIG_MG_DISK is not set
# CONFIG_BLK_DEV_RBD is not set
# CONFIG_MISC_DEVICES is not set
CONFIG_HAVE_IDE=y
# CONFIG_IDE is not set
#
# SCSI device support
#
CONFIG_SCSI_MOD=y
# CONFIG_RAID_ATTRS is not set
CONFIG_SCSI=y
CONFIG_SCSI_DMA=y
# CONFIG_SCSI_TGT is not set
# CONFIG_SCSI_NETLINK is not set
CONFIG_SCSI_PROC_FS=y
#
# SCSI support type (disk, tape, CD-ROM)
#
CONFIG_BLK_DEV_SD=y
# CONFIG_CHR_DEV_ST is not set
# CONFIG_CHR_DEV_OSST is not set
# CONFIG_BLK_DEV_SR is not set
CONFIG_CHR_DEV_SG=y
# CONFIG_CHR_DEV_SCH is not set
# CONFIG_SCSI_MULTI_LUN is not set
# CONFIG_SCSI_CONSTANTS is not set
# CONFIG_SCSI_LOGGING is not set
# CONFIG_SCSI_SCAN_ASYNC is not set
CONFIG_SCSI_WAIT_SCAN=m
#
# SCSI Transports
#
# CONFIG_SCSI_SPI_ATTRS is not set
# CONFIG_SCSI_FC_ATTRS is not set
# CONFIG_SCSI_ISCSI_ATTRS is not set
# CONFIG_SCSI_SAS_ATTRS is not set
# CONFIG_SCSI_SAS_LIBSAS is not set
# CONFIG_SCSI_SRP_ATTRS is not set
# CONFIG_SCSI_LOWLEVEL is not set
# CONFIG_SCSI_DH is not set
# CONFIG_SCSI_OSD_INITIATOR is not set
# CONFIG_ATA is not set
# CONFIG_MD is not set
CONFIG_NETDEVICES=y
# CONFIG_DUMMY is not set
# CONFIG_BONDING is not set
# CONFIG_MACVLAN is not set
# CONFIG_EQUALIZER is not set
# CONFIG_TUN is not set
# CONFIG_VETH is not set
CONFIG_MII=y
CONFIG_PHYLIB=y
#
# MII PHY device drivers
#
# CONFIG_MARVELL_PHY is not set
# CONFIG_DAVICOM_PHY is not set
# CONFIG_QSEMI_PHY is not set
# CONFIG_LXT_PHY is not set
# CONFIG_CICADA_PHY is not set
# CONFIG_VITESSE_PHY is not set
# CONFIG_SMSC_PHY is not set
# CONFIG_BROADCOM_PHY is not set
# CONFIG_BCM63XX_PHY is not set
# CONFIG_ICPLUS_PHY is not set
# CONFIG_REALTEK_PHY is not set
# CONFIG_NATIONAL_PHY is not set
# CONFIG_STE10XP is not set
# CONFIG_LSI_ET1011C_PHY is not set
# CONFIG_MICREL_PHY is not set
# CONFIG_FIXED_PHY is not set
# CONFIG_MDIO_BITBANG is not set
# CONFIG_NET_ETHERNET is not set
CONFIG_NETDEV_1000=y
CONFIG_TI_DAVINCI_MDIO=y
CONFIG_TI_DAVINCI_CPDMA=y
CONFIG_TI_CPSW=y
# CONFIG_TI_CPSW_DUAL_EMAC is not set
# CONFIG_STMMAC_ETH is not set
# CONFIG_NETDEV_10000 is not set
CONFIG_WLAN=y
# CONFIG_LIBERTAS_THINFIRM is not set
# CONFIG_MAC80211_HWSIM is not set
# CONFIG_ATH_COMMON is not set
# CONFIG_B43 is not set
# CONFIG_B43LEGACY is not set
# CONFIG_HOSTAP is not set
# CONFIG_IWM is not set
# CONFIG_LIBERTAS is not set
# CONFIG_P54_COMMON is not set
# CONFIG_RT2X00 is not set
# CONFIG_WL1251 is not setCustomized DM385 board with IPNC RDK 3.5 version
CONFIG_WL12XX=m
CONFIG_WL1271=m
# CONFIG_WL1271_SPI is not set
CONFIG_WL1271_SDIO=m
CONFIG_WL12XX_PLATFORM_DATA=y
#
# Enable WiMAX (Networking options) to see the WiMAX drivers
#
# CONFIG_WAN is not set
#
# CAIF transport drivers
#
# CONFIG_PPP is not set
# CONFIG_SLIP is not set
# CONFIG_NETCONSOLE is not set
# CONFIG_NETPOLL is not set
# CONFIG_NET_POLL_CONTROLLER is not set
# CONFIG_ISDN is not set
# CONFIG_PHONE is not set
#
# Input device support
#
CONFIG_INPUT=y
# CONFIG_INPUT_FF_MEMLESS is not set
# CONFIG_INPUT_POLLDEV is not set
# CONFIG_INPUT_SPARSEKMAP is not set
#
# Userland interfaces
#
CONFIG_INPUT_MOUSEDEV=y
# CONFIG_INPUT_MOUSEDEV_PSAUX is not set
CONFIG_INPUT_MOUSEDEV_SCREEN_X=1024
CONFIG_INPUT_MOUSEDEV_SCREEN_Y=768
# CONFIG_INPUT_JOYDEV is not set
CONFIG_INPUT_EVDEV=y
# CONFIG_INPUT_EVBUG is not set
#
# Input Device Drivers
#
# CONFIG_INPUT_KEYBOARD is not set
# CONFIG_INPUT_MOUSE is not set
# CONFIG_INPUT_JOYSTICK is not set
# CONFIG_INPUT_TABLET is not set
CONFIG_INPUT_TOUCHSCREEN=y
# CONFIG_TOUCHSCREEN_ADS7846 is not set
# CONFIG_TOUCHSCREEN_AD7877 is not set
# CONFIG_TOUCHSCREEN_AD7879 is not set
# CONFIG_TOUCHSCREEN_BU21013 is not set
# CONFIG_TOUCHSCREEN_CY8CTMG110 is not set
# CONFIG_TOUCHSCREEN_DYNAPRO is not set
# CONFIG_TOUCHSCREEN_HAMPSHIRE is not set
# CONFIG_TOUCHSCREEN_EETI is not set
# CONFIG_TOUCHSCREEN_FUJITSU is not set
# CONFIG_TOUCHSCREEN_GUNZE is not set
# CONFIG_TOUCHSCREEN_ELO is not set
# CONFIG_TOUCHSCREEN_WACOM_W8001 is not set
# CONFIG_TOUCHSCREEN_MCS5000 is not set
# CONFIG_TOUCHSCREEN_MTOUCH is not set
# CONFIG_TOUCHSCREEN_INEXIO is not set
# CONFIG_TOUCHSCREEN_MK712 is not set
# CONFIG_TOUCHSCREEN_PENMOUNT is not set
# CONFIG_TOUCHSCREEN_QT602240 is not set
# CONFIG_TOUCHSCREEN_TOUCHRIGHT is not set
# CONFIG_TOUCHSCREEN_TOUCHWIN is not set
# CONFIG_TOUCHSCREEN_USB_COMPOSITE is not set
# CONFIG_TOUCHSCREEN_TOUCHIT213 is not set
# CONFIG_TOUCHSCREEN_TSC2007 is not set
CONFIG_TOUCHSCREEN_TSC2004=y
# CONFIG_TOUCHSCREEN_W90X900 is not set
# CONFIG_TOUCHSCREEN_TPS6507X is not set
CONFIG_INPUT_MISC=y
# CONFIG_INPUT_AD714X is not set
# CONFIG_INPUT_ATI_REMOTE is not set
# CONFIG_INPUT_ATI_REMOTE2 is not set
# CONFIG_INPUT_KEYSPAN_REMOTE is not set
# CONFIG_INPUT_POWERMATE is not set
# CONFIG_INPUT_YEALINK is not set
# CONFIG_INPUT_CM109 is not set
# CONFIG_INPUT_UINPUT is not set
# CONFIG_INPUT_PCF8574 is not set
# CONFIG_INPUT_GPIO_ROTARY_ENCODER is not set
# CONFIG_INPUT_ADXL34X is not set
CONFIG_INPUT_BMA250=y
CONFIG_INPUT_ISL29023=y
CONFIG_INPUT_MCU_BRIDGE=y
#
# Hardware I/O ports
#
CONFIG_SERIO=y
CONFIG_SERIO_SERPORT=y
# CONFIG_SERIO_RAW is not set
# CONFIG_SERIO_ALTERA_PS2 is not set
# CONFIG_SERIO_PS2MULT is not set
# CONFIG_GAMEPORT is not set
#
# Character devices
#
CONFIG_VT=y
CONFIG_CONSOLE_TRANSLATIONS=y
CONFIG_VT_CONSOLE=y
CONFIG_HW_CONSOLE=y
# CONFIG_VT_HW_CONSOLE_BINDING is not set
CONFIG_DEVKMEM=y
CONFIG_SERIAL_NONSTANDARD=y
# CONFIG_N_HDLC is not set
# CONFIG_N_GSM is not set
# CONFIG_RISCOM8 is not set
# CONFIG_SPECIALIX is not set
# CONFIG_STALDRV is not set
#
# Serial drivers
#
CONFIG_SERIAL_8250=y
CONFIG_SERIAL_8250_CONSOLE=y
CONFIG_SERIAL_8250_NR_UARTS=64
CONFIG_SERIAL_8250_RUNTIME_UARTS=4
CONFIG_SERIAL_8250_EXTENDED=y
# CONFIG_SERIAL_8250_MANY_PORTS is not set
CONFIG_SERIAL_8250_SHARE_IRQ=y
CONFIG_SERIAL_8250_DETECT_IRQ=y
CONFIG_SERIAL_8250_RSA=y
#
# Non-8250 serial port support
#
# CONFIG_SERIAL_MAX3100 is not set
# CONFIG_SERIAL_MAX3107 is not set
CONFIG_SERIAL_CORE=y
CONFIG_SERIAL_CORE_CONSOLE=y
CONFIG_SERIAL_OMAP=y
CONFIG_SERIAL_OMAP_CONSOLE=y
# CONFIG_SERIAL_TIMBERDALE is not set
# CONFIG_SERIAL_ALTERA_JTAGUART is not set
# CONFIG_SERIAL_ALTERA_UART is not set
CONFIG_UNIX98_PTYS=y
# CONFIG_DEVPTS_MULTIPLE_INSTANCES is not set
# CONFIG_LEGACY_PTYS is not set
# CONFIG_IPMI_HANDLER is not set
# CONFIG_HW_RANDOM is not set
# CONFIG_R3964 is not set
# CONFIG_RAW_DRIVER is not set
# CONFIG_TCG_TPM is not set
# CONFIG_TI81XX_PCIE_EPDRV is not set
# CONFIG_RAMOOPS is not set
CONFIG_I2C=y
CONFIG_I2C_BOARDINFO=y
CONFIG_I2C_COMPAT=y
CONFIG_I2C_CHARDEV=y
# CONFIG_I2C_MUX is not set
CONFIG_I2C_HELPER_AUTO=y
#
# I2C Hardware Bus support
#
#
# I2C system bus drivers (mostly embedded / system-on-chip)
#
# CONFIG_I2C_DESIGNWARE is not set
# CONFIG_I2C_GPIO is not set
# CONFIG_I2C_OCORES is not set
CONFIG_I2C_OMAP=y
# CONFIG_I2C_PCA_PLATFORM is not set
# CONFIG_I2C_SIMTEC is not set
# CONFIG_I2C_XILINX is not set
#
# External I2C/SMBus adapter drivers
#
# CONFIG_I2C_PARPORT_LIGHT is not set
# CONFIG_I2C_TAOS_EVM is not set
#
# Other I2C/SMBus bus drivers
#
# CONFIG_I2C_STUB is not set
# CONFIG_I2C_DEBUG_CORE is not set
# CONFIG_I2C_DEBUG_ALGO is not set
# CONFIG_I2C_DEBUG_BUS is not set
CONFIG_SPI=y
# CONFIG_SPI_DEBUG is not set
CONFIG_SPI_MASTER=y
#
# SPI Master Controller Drivers
#
# CONFIG_SPI_BITBANG is not set
# CONFIG_SPI_GPIO is not set
CONFIG_SPI_OMAP24XX=y
# CONFIG_SPI_XILINX is not set
# CONFIG_SPI_DESIGNWARE is not set
#
# SPI Protocol Masters
#
# CONFIG_SPI_SPIDEV is not set
# CONFIG_SPI_TLE62X0 is not set
#
# PPS support
#
# CONFIG_PPS is not set
#
# PTP clock support
#
#
# Enable Device Drivers -> PPS to see the PTP clock options.
#
CONFIG_ARCH_REQUIRE_GPIOLIB=y
CONFIG_GPIOLIB=y
# CONFIG_DEBUG_GPIO is not set
CONFIG_GPIO_SYSFS=y
#
# Memory mapped GPIO expanders:
#
# CONFIG_GPIO_BASIC_MMIO is not set
# CONFIG_GPIO_IT8761E is not set
# CONFIG_GPIO_VX855 is not set
#
# I2C GPIO expanders:
#
# CONFIG_GPIO_MAX7300 is not set
# CONFIG_GPIO_MAX732X is not set
# CONFIG_GPIO_PCA953X is not set
# CONFIG_GPIO_PCF857X is not set
# CONFIG_GPIO_SX150X is not set
# CONFIG_GPIO_ADP5588 is not set
#
# PCI GPIO expanders:
#
#
# SPI GPIO expanders:
#
# CONFIG_GPIO_MAX7301 is not set
# CONFIG_GPIO_MCP23S08 is not set
# CONFIG_GPIO_MC33880 is not set
# CONFIG_GPIO_74X164 is not set
#
# AC97 GPIO expanders:
#
#
# MODULbus GPIO expanders:
#
# CONFIG_W1 is not set
# CONFIG_POWER_SUPPLY is not set
# CONFIG_HWMON is not set
# CONFIG_THERMAL is not set
CONFIG_WATCHDOG=y
# CONFIG_WATCHDOG_NOWAYOUT is not set
#
# Watchdog Device Drivers
#
# CONFIG_SOFT_WATCHDOG is not set
CONFIG_OMAP_WATCHDOG=y
# CONFIG_MAX63XX_WATCHDOG is not set
CONFIG_SSB_POSSIBLE=y
#
# Sonics Silicon Backplane
#
CONFIG_SSB=m
CONFIG_SSB_SDIOHOST_POSSIBLE=y
# CONFIG_SSB_SDIOHOST is not set
# CONFIG_SSB_DEBUG is not set
CONFIG_MFD_SUPPORT=y
# CONFIG_MFD_CORE is not set
# CONFIG_MFD_88PM860X is not set
# CONFIG_MFD_SM501 is not set
# CONFIG_MFD_ASIC3 is not set
# CONFIG_HTC_EGPIO is not set
# CONFIG_HTC_PASIC3 is not set
# CONFIG_HTC_I2CPLD is not set
# CONFIG_TPS65010 is not set
# CONFIG_TPS6507X is not set
# CONFIG_MFD_STMPE is not set
# CONFIG_MFD_TC35892 is not set
# CONFIG_MFD_TMIO is not set
# CONFIG_MFD_T7L66XB is not set
# CONFIG_MFD_TC6387XB is not set
# CONFIG_MFD_TC6393XB is not set
# CONFIG_PMIC_DA903X is not set
# CONFIG_PMIC_ADP5520 is not set
# CONFIG_MFD_MAX8925 is not set
# CONFIG_MFD_MAX8998 is not set
# CONFIG_MFD_WM8400 is not set
# CONFIG_MFD_WM831X_I2C is not set
# CONFIG_MFD_WM831X_SPI is not set
# CONFIG_MFD_WM8350_I2C is not set
# CONFIG_MFD_WM8994 is not set
# CONFIG_MFD_PCF50633 is not set
# CONFIG_MFD_MC13XXX is not set
# CONFIG_ABX500_CORE is not set
# CONFIG_EZX_PCAP is not set
# CONFIG_MFD_TPS6586X is not set
# CONFIG_MFD_TPS65910 is not set
CONFIG_REGULATOR=y
# CONFIG_REGULATOR_DEBUG is not set
# CONFIG_REGULATOR_DUMMY is not set
CONFIG_REGULATOR_FIXED_VOLTAGE=y
# CONFIG_REGULATOR_VIRTUAL_CONSUMER is not set
# CONFIG_REGULATOR_USERSPACE_CONSUMER is not set
# CONFIG_REGULATOR_BQ24022 is not set
# CONFIG_REGULATOR_MAX1586 is not set
# CONFIG_REGULATOR_MAX8649 is not set
# CONFIG_REGULATOR_MAX8660 is not set
# CONFIG_REGULATOR_MAX8952 is not set
# CONFIG_REGULATOR_LP3971 is not set
# CONFIG_REGULATOR_LP3972 is not set
# CONFIG_REGULATOR_TPS65023 is not set
# CONFIG_REGULATOR_TPS6507X is not set
# CONFIG_REGULATOR_ISL6271A is not set
# CONFIG_REGULATOR_AD5398 is not set
CONFIG_MEDIA_SUPPORT=y
#
# Multimedia core support
#
# CONFIG_MEDIA_CONTROLLER is not set
CONFIG_VIDEO_DEV=y
CONFIG_VIDEO_V4L2_COMMON=y
CONFIG_VIDEO_ALLOW_V4L1=y
CONFIG_VIDEO_V4L1_COMPAT=y
# CONFIG_DVB_CORE is not set
CONFIG_VIDEO_MEDIA=y
#
# Multimedia drivers
#
# CONFIG_IR_CORE is not set
# CONFIG_MEDIA_ATTACH is not set
CONFIG_MEDIA_TUNER=y
# CONFIG_MEDIA_TUNER_CUSTOMISE is not set
CONFIG_MEDIA_TUNER_SIMPLE=y
CONFIG_MEDIA_TUNER_TDA8290=y
CONFIG_MEDIA_TUNER_TDA827X=y
CONFIG_MEDIA_TUNER_TDA18271=y
CONFIG_MEDIA_TUNER_TDA9887=y
CONFIG_MEDIA_TUNER_TEA5761=y
CONFIG_MEDIA_TUNER_TEA5767=y
CONFIG_MEDIA_TUNER_MT20XX=y
CONFIG_MEDIA_TUNER_XC2028=y
CONFIG_MEDIA_TUNER_XC5000=y
CONFIG_MEDIA_TUNER_MC44S803=y
CONFIG_VIDEO_V4L2=y
CONFIG_VIDEO_V4L1=y
CONFIG_VIDEOBUF_GEN=y
CONFIG_VIDEOBUF_DMA_SG=y
CONFIG_VIDEOBUF_DMA_CONTIG=y
CONFIG_VIDEO_CAPTURE_DRIVERS=y
# CONFIG_VIDEO_ADV_DEBUG is not set
# CONFIG_VIDEO_FIXED_MINOR_RANGES is not set
# CONFIG_VIDEO_HELPER_CHIPS_AUTO is not set
#
# Encoders/decoders and other helper chips
#
#
# Audio decoders
#
# CONFIG_VIDEO_TVAUDIO is not set
# CONFIG_VIDEO_TDA7432 is not set
# CONFIG_VIDEO_TDA9840 is not set
# CONFIG_VIDEO_TDA9875 is not set
# CONFIG_VIDEO_TEA6415C is not set
# CONFIG_VIDEO_TEA6420 is not set
# CONFIG_VIDEO_MSP3400 is not set
# CONFIG_VIDEO_CS5345 is not set
# CONFIG_VIDEO_CS53L32A is not set
# CONFIG_VIDEO_M52790 is not set
# CONFIG_VIDEO_TLV320AIC23B is not set
# CONFIG_VIDEO_WM8775 is not set
# CONFIG_VIDEO_WM8739 is not set
# CONFIG_VIDEO_VP27SMPX is not set
#
# RDS decoders
#
# CONFIG_VIDEO_SAA6588 is not set
#
# Video decoders
#
# CONFIG_VIDEO_ADV7180 is not set
# CONFIG_VIDEO_BT819 is not set
# CONFIG_VIDEO_BT856 is not set
# CONFIG_VIDEO_BT866 is not set
# CONFIG_VIDEO_KS0127 is not set
# CONFIG_VIDEO_OV7670 is not set
# CONFIG_VIDEO_MT9T001 is not set
# CONFIG_VIDEO_MT9V011 is not set
# CONFIG_VIDEO_MT9V113 is not set
# CONFIG_VIDEO_MT9T111 is not set
# CONFIG_VIDEO_TCM825X is not set
# CONFIG_VIDEO_SAA7110 is not set
# CONFIG_VIDEO_SAA711X is not set
# CONFIG_VIDEO_SAA717X is not set
# CONFIG_VIDEO_SAA7191 is not set
# CONFIG_VIDEO_TVP514X is not set
# CONFIG_VIDEO_TVP5150 is not set
# CONFIG_VIDEO_TVP7002 is not set
# CONFIG_VIDEO_VPX3220 is not set
#
# Video and audio decoders
#
# CONFIG_VIDEO_CX25840 is not set
#
# MPEG video encoders
#
# CONFIG_VIDEO_CX2341X is not set
#
# Video encoders
#
# CONFIG_VIDEO_SAA7127 is not set
# CONFIG_VIDEO_SAA7185 is not set
# CONFIG_VIDEO_ADV7170 is not set
# CONFIG_VIDEO_ADV7175 is not set
# CONFIG_VIDEO_THS7303 is not set
# CONFIG_VIDEO_ADV7343 is not set
# CONFIG_VIDEO_AK881X is not set
#
# Video improvement chips
#
# CONFIG_VIDEO_UPD64031A is not set
# CONFIG_VIDEO_UPD64083 is not set
CONFIG_VIDEO_TI81XX_VIDOUT=m
# CONFIG_VIDEO_TI81XX_VIDIN is not set
# CONFIG_VIDEO_SR030PC30 is not set
# CONFIG_SOC_CAMERA is not set
# CONFIG_V4L_MEM2MEM_DRIVERS is not set
# CONFIG_RADIO_ADAPTERS is not set
# CONFIG_DAB is not set
CONFIG_HAVE_TI_TILER=y
# CONFIG_TI_TILER is not set
#
# Graphics support
#
# CONFIG_DRM is not set
# CONFIG_VGASTATE is not set
CONFIG_VIDEO_OUTPUT_CONTROL=y
CONFIG_FB=y
# CONFIG_FIRMWARE_EDID is not set
# CONFIG_FB_DDC is not set
# CONFIG_FB_BOOT_VESA_SUPPORT is not set
CONFIG_FB_CFB_FILLRECT=y
CONFIG_FB_CFB_COPYAREA=y
CONFIG_FB_CFB_IMAGEBLIT=y
# CONFIG_FB_CFB_REV_PIXELS_IN_BYTE is not set
# CONFIG_FB_SYS_FILLRECT is not set
# CONFIG_FB_SYS_COPYAREA is not set
# CONFIG_FB_SYS_IMAGEBLIT is not set
# CONFIG_FB_FOREIGN_ENDIAN is not set
# CONFIG_FB_SYS_FOPS is not set
# CONFIG_FB_SVGALIB is not set
# CONFIG_FB_MACMODES is not set
# CONFIG_FB_BACKLIGHT is not set
# CONFIG_FB_MODE_HELPERS is not set
# CONFIG_FB_TILEBLITTING is not set
#
# Frame buffer hardware drivers
#
# CONFIG_FB_S1D13XXX is not set
# CONFIG_FB_VIRTUAL is not set
# CONFIG_FB_METRONOME is not set
# CONFIG_FB_MB862XX is not set
# CONFIG_FB_BROADSHEET is not set
CONFIG_TI81XX_VPSS=m
CONFIG_TI81XX_VPSS_VRAM_SIZE=4
CONFIG_TI81XX_VPSS_DEBUG_SUPPORT=y
CONFIG_FB_TI81XX=m
CONFIG_FB_TI81XX_DEBUG_SUPPORT=y
CONFIG_FB_TI81XX_NUM_FBS=3
CONFIG_TI81XX_HDMI=m
# CONFIG_TI81XX_HDMI_HDCP is not set
# CONFIG_SII9022a is not set
# CONFIG_BACKLIGHT_LCD_SUPPORT is not set
#
# Display device support
#
# CONFIG_DISPLAY_SUPPORT is not set
#
# Console display driver support
#
CONFIG_DUMMY_CONSOLE=y
# CONFIG_FRAMEBUFFER_CONSOLE is not set
# CONFIG_LOGO is not set
CONFIG_SOUND=y
# CONFIG_SOUND_OSS_CORE is not set
CONFIG_SND=y
CONFIG_SND_TIMER=y
CONFIG_SND_PCM=y
CONFIG_SND_JACK=y
# CONFIG_SND_SEQUENCER is not set
# CONFIG_SND_MIXER_OSS is not set
# CONFIG_SND_PCM_OSS is not set
# CONFIG_SND_HRTIMER is not set
# CONFIG_SND_DYNAMIC_MINORS is not set
CONFIG_SND_SUPPORT_OLD_API=y
CONFIG_SND_VERBOSE_PROCFS=y
# CONFIG_SND_VERBOSE_PRINTK is not set
# CONFIG_SND_DEBUG is not set
# CONFIG_SND_RAWMIDI_SEQ is not set
# CONFIG_SND_OPL3_LIB_SEQ is not set
# CONFIG_SND_OPL4_LIB_SEQ is not set
# CONFIG_SND_SBAWE_SEQ is not set
# CONFIG_SND_EMU10K1_SEQ is not set
# CONFIG_SND_DRIVERS is not set
# CONFIG_SND_ARM is not set
# CONFIG_SND_SPI is not set
CONFIG_SND_SOC=y
CONFIG_SND_TI81XX_SOC=y
CONFIG_SND_DAVINCI_SOC_MCASP=y
CONFIG_SND_TI81XX_SOC_EVM=y
# CONFIG_SND_SOC_TI81XX_HDMI is not set
# CONFIG_SND_OMAP_SOC is not set
CONFIG_SND_SOC_I2C_AND_SPI=y
# CONFIG_SND_SOC_ALL_CODECS is not set
CONFIG_SND_SOC_TLV320AIC3110=y
# CONFIG_SOUND_PRIME is not set
# CONFIG_HID_SUPPORT is not set
CONFIG_USB_SUPPORT=y
CONFIG_USB_ARCH_HAS_HCD=y
CONFIG_USB_ARCH_HAS_OHCI=y
# CONFIG_USB_ARCH_HAS_EHCI is not set
# CONFIG_USB is not set
CONFIG_USB_MUSB_HDRC=y
#
# Platform Glue Layer
#
# CONFIG_USB_MUSB_TUSB6010_GLUE is not set
# CONFIG_USB_MUSB_OMAP2PLUS_GLUE is not set
# CONFIG_USB_MUSB_AM35X_GLUE is not set
CONFIG_USB_MUSB_TI81XX_GLUE=y
# CONFIG_USB_MUSB_DAVINCI is not set
# CONFIG_USB_MUSB_DA8XX is not set
# CONFIG_USB_MUSB_TUSB6010 is not set
# CONFIG_USB_MUSB_OMAP2PLUS is not set
# CONFIG_USB_MUSB_AM35X is not set
CONFIG_USB_MUSB_TI81XX=y
# CONFIG_USB_MUSB_BLACKFIN is not set
# CONFIG_USB_MUSB_UX500 is not set
CONFIG_USB_TI81XX_USBID_CTRL_SW=y
# CONFIG_USB_TI81XX_USBID_CTRL_HW is not set
CONFIG_USB_MUSB_PERIPHERAL=y
CONFIG_USB_GADGET_MUSB_HDRC=y
# CONFIG_MUSB_PIO_ONLY is not set
# CONFIG_USB_INVENTRA_DMA_HW is not set
# CONFIG_USB_TI_CPPI_DMA_HW is not set
CONFIG_USB_TI_CPPI41_DMA_HW=y
# CONFIG_USB_INVENTRA_DMA is not set
# CONFIG_USB_TI_CPPI_DMA is not set
CONFIG_USB_TI_CPPI41_DMA=y
# CONFIG_USB_TUSB_OMAP_DMA is not set
CONFIG_USB_MUSB_DEBUG=y
#
# NOTE: USB_STORAGE depends on SCSI but BLK_DEV_SD may
#
CONFIG_USB_GADGET=y
# CONFIG_USB_GADGET_DEBUG is not set
# CONFIG_USB_GADGET_DEBUG_FILES is not set
# CONFIG_USB_GADGET_DEBUG_FS is not set
CONFIG_USB_GADGET_VBUS_DRAW=2
CONFIG_USB_GADGET_SELECTED=y
# CONFIG_USB_GADGET_OMAP is not set
# CONFIG_USB_GADGET_R8A66597 is not set
# CONFIG_USB_GADGET_M66592 is not set
CONFIG_USB_GADGET_DUALSPEED=y
# CONFIG_USB_ZERO is not set
# CONFIG_USB_AUDIO is not set
# CONFIG_USB_ETH is not set
# CONFIG_USB_GADGETFS is not set
# CONFIG_USB_FUNCTIONFS is not set
CONFIG_USB_FILE_STORAGE=m
CONFIG_USB_FILE_STORAGE_TEST=y
# CONFIG_USB_MASS_STORAGE is not set
# CONFIG_USB_G_SERIAL is not set
# CONFIG_USB_MIDI_GADGET is not set
# CONFIG_USB_G_PRINTER is not set
# CONFIG_USB_CDC_COMPOSITE is not set
# CONFIG_USB_G_MULTI is not set
# CONFIG_USB_G_HID is not set
# CONFIG_USB_G_DBGP is not set
# CONFIG_USB_G_WEBCAM is not set
#
# OTG and related infrastructure
#
CONFIG_USB_OTG_UTILS=y
# CONFIG_USB_GPIO_VBUS is not set
# CONFIG_USB_ULPI is not set
CONFIG_NOP_USB_XCEIV=y
CONFIG_MMC=y
# CONFIG_MMC_DEBUG is not set
# CONFIG_MMC_UNSAFE_RESUME is not set
#
# MMC/SD/SDIO Card Drivers
#
CONFIG_MMC_BLOCK=y
CONFIG_MMC_BLOCK_MINORS=8
CONFIG_MMC_BLOCK_BOUNCE=y
# CONFIG_SDIO_UART is not set
# CONFIG_MMC_TEST is not set
#
# MMC/SD/SDIO Host Controller Drivers
#
# CONFIG_MMC_SDHCI is not set
# CONFIG_MMC_OMAP is not set
CONFIG_MMC_OMAP_HS=y
# CONFIG_MMC_DM385_EMMC is not set
# CONFIG_MEMSTICK is not set
CONFIG_NEW_LEDS=y
CONFIG_LEDS_CLASS=y
#
# LED drivers
#
# CONFIG_LEDS_PCA9532 is not set
CONFIG_LEDS_GPIO=y
CONFIG_LEDS_CARBB=y
CONFIG_LEDS_GPIO_PLATFORM=y
# CONFIG_LEDS_LP3944 is not set
# CONFIG_LEDS_LP5521 is not set
# CONFIG_LEDS_LP5523 is not set
# CONFIG_LEDS_PCA955X is not set
# CONFIG_LEDS_DAC124S085 is not set
# CONFIG_LEDS_REGULATOR is not set
# CONFIG_LEDS_BD2802 is not set
# CONFIG_LEDS_LT3593 is not set
CONFIG_LEDS_TRIGGERS=y
#
# LED Triggers
#
CONFIG_LEDS_TRIGGER_TIMER=y
CONFIG_LEDS_TRIGGER_HEARTBEAT=y
# CONFIG_LEDS_TRIGGER_BACKLIGHT is not set
# CONFIG_LEDS_TRIGGER_GPIO is not set
# CONFIG_LEDS_TRIGGER_DEFAULT_ON is not set
#
# iptables trigger is under Netfilter config (LED target)
#
# CONFIG_ACCESSIBILITY is not set
CONFIG_RTC_LIB=y
CONFIG_RTC_CLASS=y
CONFIG_RTC_HCTOSYS=y
CONFIG_RTC_HCTOSYS_DEVICE="rtc0"
# CONFIG_RTC_DEBUG is not set
#
# RTC interfaces
#
CONFIG_RTC_INTF_SYSFS=y
CONFIG_RTC_INTF_PROC=y
CONFIG_RTC_INTF_DEV=y
# CONFIG_RTC_INTF_DEV_UIE_EMUL is not set
# CONFIG_RTC_DRV_TEST is not set
#
# I2C RTC drivers
#
# CONFIG_RTC_DRV_DS1307 is not set
# CONFIG_RTC_DRV_DS1374 is not set
# CONFIG_RTC_DRV_DS1672 is not set
# CONFIG_RTC_DRV_DS3232 is not set
# CONFIG_RTC_DRV_MAX6900 is not set
# CONFIG_RTC_DRV_RS5C372 is not set
# CONFIG_RTC_DRV_ISL1208 is not set
# CONFIG_RTC_DRV_ISL12022 is not set
# CONFIG_RTC_DRV_X1205 is not set
# CONFIG_RTC_DRV_PCF8563 is not set
# CONFIG_RTC_DRV_PCF8583 is not set
# CONFIG_RTC_DRV_M41T80 is not set
CONFIG_RTC_DRV_BQ32K=y
# CONFIG_RTC_DRV_S35390A is not set
# CONFIG_RTC_DRV_FM3130 is not set
# CONFIG_RTC_DRV_RX8581 is not set
# CONFIG_RTC_DRV_RX8025 is not set
#
# SPI RTC drivers
#
# CONFIG_RTC_DRV_M41T94 is not set
# CONFIG_RTC_DRV_DS1305 is not set
# CONFIG_RTC_DRV_DS1390 is not set
# CONFIG_RTC_DRV_MAX6902 is not set
# CONFIG_RTC_DRV_R9701 is not set
# CONFIG_RTC_DRV_RS5C348 is not set
# CONFIG_RTC_DRV_DS3234 is not set
# CONFIG_RTC_DRV_PCF2123 is not set
#
# Platform RTC drivers
#
# CONFIG_RTC_DRV_CMOS is not set
# CONFIG_RTC_DRV_DS1286 is not set
# CONFIG_RTC_DRV_DS1511 is not set
# CONFIG_RTC_DRV_DS1553 is not set
# CONFIG_RTC_DRV_DS1742 is not set
# CONFIG_RTC_DRV_STK17TA8 is not set
# CONFIG_RTC_DRV_M48T86 is not set
# CONFIG_RTC_DRV_M48T35 is not set
# CONFIG_RTC_DRV_M48T59 is not set
# CONFIG_RTC_DRV_MSM6242 is not set
# CONFIG_RTC_DRV_BQ4802 is not set
# CONFIG_RTC_DRV_RP5C01 is not set
# CONFIG_RTC_DRV_V3020 is not set
#
# on-CPU RTC drivers
#
# CONFIG_RTC_DRV_OMAP is not set
# CONFIG_DMADEVICES is not set
# CONFIG_AUXDISPLAY is not set
CONFIG_UIO=y
# CONFIG_UIO_PDRV is not set
CONFIG_UIO_PDRV_GENIRQ=y
# CONFIG_STAGING is not set
CONFIG_Sys_Link=y
CONFIG_SYSLINK_MULTIPROC=y
CONFIG_SYSLINK_NOTIFY=y
#
# File systems
#
CONFIG_EXT2_FS=y
CONFIG_EXT2_FS_XATTR=y
CONFIG_EXT2_FS_POSIX_ACL=y
CONFIG_EXT2_FS_SECURITY=y
# CONFIG_EXT2_FS_XIP is not set
CONFIG_EXT3_FS=y
# CONFIG_EXT3_DEFAULTS_TO_ORDERED is not set
CONFIG_EXT3_FS_XATTR=y
CONFIG_EXT3_FS_POSIX_ACL=y
CONFIG_EXT3_FS_SECURITY=y
# CONFIG_EXT4_FS is not set
CONFIG_JBD=y
# CONFIG_JBD_DEBUG is not set
CONFIG_FS_MBCACHE=y
# CONFIG_REISERFS_FS is not set
# CONFIG_JFS_FS is not set
CONFIG_FS_POSIX_ACL=y
# CONFIG_XFS_FS is not set
# CONFIG_OCFS2_FS is not set
# CONFIG_BTRFS_FS is not set
# CONFIG_NILFS2_FS is not set
CONFIG_FILE_LOCKING=y
# CONFIG_FSNOTIFY is not set
# CONFIG_DNOTIFY is not set
# CONFIG_INOTIFY_USER is not set
# CONFIG_FANOTIFY is not set
# CONFIG_QUOTA is not set
# CONFIG_QUOTACTL is not set
# CONFIG_AUTOFS4_FS is not set
# CONFIG_FUSE_FS is not set
#
# Caches
#
# CONFIG_FSCACHE is not set
#
# CD-ROM/DVD Filesystems
#
# CONFIG_ISO9660_FS is not set
# CONFIG_UDF_FS is not set
#
# DOS/FAT/NT Filesystems
#
CONFIG_FAT_FS=y
CONFIG_MSDOS_FS=y
CONFIG_VFAT_FS=y
CONFIG_FAT_DEFAULT_CODEPAGE=437
CONFIG_FAT_DEFAULT_IOCHARSET="iso8859-1"
# CONFIG_NTFS_FS is not set
#
# Pseudo filesystems
#
CONFIG_PROC_FS=y
CONFIG_PROC_SYSCTL=y
CONFIG_PROC_PAGE_MONITOR=y
CONFIG_SYSFS=y
CONFIG_TMPFS=y
# CONFIG_TMPFS_POSIX_ACL is not set
# CONFIG_HUGETLB_PAGE is not set
# CONFIG_CONFIGFS_FS is not set
CONFIG_MISC_FILESYSTEMS=y
# CONFIG_ADFS_FS is not set
# CONFIG_AFFS_FS is not set
# CONFIG_ECRYPT_FS is not set
# CONFIG_HFS_FS is not set
# CONFIG_HFSPLUS_FS is not set
# CONFIG_BEFS_FS is not set
# CONFIG_BFS_FS is not set
# CONFIG_EFS_FS is not set
CONFIG_JFFS2_FS=y
CONFIG_JFFS2_FS_DEBUG=0
CONFIG_JFFS2_FS_WRITEBUFFER=y
CONFIG_JFFS2_FS_WBUF_VERIFY=y
# CONFIG_JFFS2_SUMMARY is not set
# CONFIG_JFFS2_FS_XATTR is not set
# CONFIG_JFFS2_COMPRESSION_OPTIONS is not set
CONFIG_JFFS2_ZLIB=y
# CONFIG_JFFS2_LZO is not set
CONFIG_JFFS2_RTIME=y
# CONFIG_JFFS2_RUBIN is not set
CONFIG_UBIFS_FS=y
# CONFIG_UBIFS_FS_XATTR is not set
# CONFIG_UBIFS_FS_ADVANCED_COMPR is not set
CONFIG_UBIFS_FS_LZO=y
CONFIG_UBIFS_FS_ZLIB=y
# CONFIG_UBIFS_FS_DEBUG is not set
# CONFIG_LOGFS is not set
# CONFIG_CRAMFS is not set
# CONFIG_SQUASHFS is not set
# CONFIG_VXFS_FS is not set
# CONFIG_MINIX_FS is not set
# CONFIG_OMFS_FS is not set
# CONFIG_HPFS_FS is not set
# CONFIG_QNX4FS_FS is not set
# CONFIG_ROMFS_FS is not set
# CONFIG_SYSV_FS is not set
# CONFIG_UFS_FS is not set
CONFIG_NETWORK_FILESYSTEMS=y
CONFIG_NFS_FS=y
CONFIG_NFS_V3=y
# CONFIG_NFS_V3_ACL is not set
CONFIG_NFS_V4=y
# CONFIG_NFS_V4_1 is not set
CONFIG_ROOT_NFS=y
# CONFIG_NFS_USE_LEGACY_DNS is not set
CONFIG_NFS_USE_KERNEL_DNS=y
# CONFIG_NFS_USE_NEW_IDMAPPER is not set
# CONFIG_NFSD is not set
CONFIG_LOCKD=y
CONFIG_LOCKD_V4=y
CONFIG_NFS_COMMON=y
CONFIG_SUNRPC=y
CONFIG_SUNRPC_GSS=y
CONFIG_RPCSEC_GSS_KRB5=y
# CONFIG_CEPH_FS is not set
# CONFIG_CIFS is not set
# CONFIG_NCP_FS is not set
# CONFIG_CODA_FS is not set
# CONFIG_AFS_FS is not set
#
# Partition Types
#
# CONFIG_PARTITION_ADVANCED is not set
CONFIG_MSDOS_PARTITION=y
CONFIG_NLS=y
CONFIG_NLS_DEFAULT="utf8"
CONFIG_NLS_CODEPAGE_437=y
# CONFIG_NLS_CODEPAGE_737 is not set
# CONFIG_NLS_CODEPAGE_775 is not set
# CONFIG_NLS_CODEPAGE_850 is not set
# CONFIG_NLS_CODEPAGE_852 is not set
# CONFIG_NLS_CODEPAGE_855 is not set
# CONFIG_NLS_CODEPAGE_857 is not set
# CONFIG_NLS_CODEPAGE_860 is not set
# CONFIG_NLS_CODEPAGE_861 is not set
# CONFIG_NLS_CODEPAGE_862 is not set
# CONFIG_NLS_CODEPAGE_863 is not set
# CONFIG_NLS_CODEPAGE_864 is not set
# CONFIG_NLS_CODEPAGE_865 is not set
# CONFIG_NLS_CODEPAGE_866 is not set
# CONFIG_NLS_CODEPAGE_869 is not set
# CONFIG_NLS_CODEPAGE_936 is not set
# CONFIG_NLS_CODEPAGE_950 is not set
# CONFIG_NLS_CODEPAGE_932 is not set
# CONFIG_NLS_CODEPAGE_949 is not set
# CONFIG_NLS_CODEPAGE_874 is not set
# CONFIG_NLS_ISO8859_8 is not set
# CONFIG_NLS_CODEPAGE_1250 is not set
# CONFIG_NLS_CODEPAGE_1251 is not set
CONFIG_NLS_ASCII=y
CONFIG_NLS_ISO8859_1=y
# CONFIG_NLS_ISO8859_2 is not set
# CONFIG_NLS_ISO8859_3 is not set
# CONFIG_NLS_ISO8859_4 is not set
# CONFIG_NLS_ISO8859_5 is not set
# CONFIG_NLS_ISO8859_6 is not set
# CONFIG_NLS_ISO8859_7 is not set
# CONFIG_NLS_ISO8859_9 is not set
# CONFIG_NLS_ISO8859_13 is not set
# CONFIG_NLS_ISO8859_14 is not set
# CONFIG_NLS_ISO8859_15 is not set
# CONFIG_NLS_KOI8_R is not set
# CONFIG_NLS_KOI8_U is not set
CONFIG_NLS_UTF8=y
# CONFIG_DLM is not set
#
# Kernel hacking
#
# CONFIG_PRINTK_TIME is not set
CONFIG_ENABLE_WARN_DEPRECATED=y
CONFIG_ENABLE_MUST_CHECK=y
CONFIG_FRAME_WARN=1024
CONFIG_MAGIC_SYSRQ=y
# CONFIG_STRIP_ASM_SYMS is not set
# CONFIG_UNUSED_SYMBOLS is not set
CONFIG_DEBUG_FS=y
# CONFIG_HEADERS_CHECK is not set
CONFIG_DEBUG_KERNEL=y
# CONFIG_DEBUG_SHIRQ is not set
# CONFIG_LOCKUP_DETECTOR is not set
# CONFIG_HARDLOCKUP_DETECTOR is not set
# CONFIG_DETECT_HUNG_TASK is not set
# CONFIG_SCHED_DEBUG is not set
# CONFIG_SCHEDSTATS is not set
# CONFIG_TIMER_STATS is not set
# CONFIG_DEBUG_OBJECTS is not set
# CONFIG_SLUB_DEBUG_ON is not set
# CONFIG_SLUB_STATS is not set
# CONFIG_DEBUG_KMEMLEAK is not set
# CONFIG_DEBUG_RT_MUTEXES is not set
# CONFIG_RT_MUTEX_TESTER is not set
# CONFIG_DEBUG_SPINLOCK is not set
# CONFIG_DEBUG_MUTEXES is not set
CONFIG_BKL=y
# CONFIG_DEBUG_LOCK_ALLOC is not set
# CONFIG_PROVE_LOCKING is not set
# CONFIG_SPARSE_RCU_POINTER is not set
# CONFIG_LOCK_STAT is not set
# CONFIG_DEBUG_SPINLOCK_SLEEP is not set
# CONFIG_DEBUG_LOCKING_API_SELFTESTS is not set
# CONFIG_DEBUG_KOBJECT is not set
# CONFIG_DEBUG_HIGHMEM is not set
CONFIG_DEBUG_BUGVERBOSE=y
# CONFIG_DEBUG_INFO is not set
# CONFIG_DEBUG_VM is not set
# CONFIG_DEBUG_WRITECOUNT is not set
CONFIG_DEBUG_MEMORY_INIT=y
# CONFIG_DEBUG_LIST is not set
# CONFIG_TEST_LIST_SORT is not set
# CONFIG_DEBUG_SG is not set
# CONFIG_DEBUG_NOTIFIERS is not set
# CONFIG_DEBUG_CREDENTIALS is not set
CONFIG_FRAME_POINTER=y
# CONFIG_BOOT_PRINTK_DELAY is not set
# CONFIG_RCU_TORTURE_TEST is not set
# CONFIG_KPROBES_SANITY_TEST is not set
# CONFIG_BACKTRACE_SELF_TEST is not set
# CONFIG_DEBUG_BLOCK_EXT_DEVT is not set
# CONFIG_DEBUG_FORCE_WEAK_PER_CPU is not set
# CONFIG_LKDTM is not set
# CONFIG_FAULT_INJECTION is not set
# CONFIG_LATENCYTOP is not set
# CONFIG_SYSCTL_SYSCALL_CHECK is not set
# CONFIG_PAGE_POISONING is not set
CONFIG_HAVE_FUNCTION_TRACER=y
CONFIG_HAVE_DYNAMIC_FTRACE=y
CONFIG_HAVE_FTRACE_MCOUNT_RECORD=y
CONFIG_TRACING_SUPPORT=y
# CONFIG_FTRACE is not set
# CONFIG_DYNAMIC_DEBUG is not set
# CONFIG_ATOMIC64_SELFTEST is not set
# CONFIG_SAMPLES is not set
CONFIG_HAVE_ARCH_KGDB=y
# CONFIG_KGDB is not set
# CONFIG_STRICT_DEVMEM is not set
# CONFIG_ARM_UNWIND is not set
# CONFIG_DEBUG_USER is not set
# CONFIG_DEBUG_ERRORS is not set
# CONFIG_DEBUG_STACK_USAGE is not set
CONFIG_DEBUG_LL=y
CONFIG_EARLY_PRINTK=y
# CONFIG_DEBUG_ICEDCC is not set
# CONFIG_OC_ETM is not set
#
# Security options
#
CONFIG_KEYS=y
CONFIG_KEYS_DEBUG_PROC_KEYS=y
# CONFIG_SECURITY_DMESG_RESTRICT is not set
CONFIG_SECURITY=y
# CONFIG_SECURITYFS is not set
CONFIG_SECURITY_NETWORK=y
# CONFIG_SECURITY_NETWORK_XFRM is not set
# CONFIG_SECURITY_PATH is not set
# CONFIG_SECURITY_TOMOYO is not set
# CONFIG_SECURITY_APPARMOR is not set
# CONFIG_IMA is not set
CONFIG_DEFAULT_SECURITY_DAC=y
CONFIG_DEFAULT_SECURITY=""
CONFIG_CRYPTO=y
#
# Crypto core or helper
#
CONFIG_CRYPTO_ALGAPI=y
CONFIG_CRYPTO_ALGAPI2=y
CONFIG_CRYPTO_AEAD2=y
CONFIG_CRYPTO_BLKCIPHER=y
CONFIG_CRYPTO_BLKCIPHER2=y
CONFIG_CRYPTO_HASH=y
CONFIG_CRYPTO_HASH2=y
CONFIG_CRYPTO_RNG2=y
CONFIG_CRYPTO_PCOMP2=y
CONFIG_CRYPTO_MANAGER=y
CONFIG_CRYPTO_MANAGER2=y
CONFIG_CRYPTO_MANAGER_DISABLE_TESTS=y
# CONFIG_CRYPTO_GF128MUL is not set
# CONFIG_CRYPTO_NULL is not set
CONFIG_CRYPTO_WORKQUEUE=y
# CONFIG_CRYPTO_CRYPTD is not set
# CONFIG_CRYPTO_AUTHENC is not set
# CONFIG_CRYPTO_TEST is not set
#
# Authenticated Encryption with Associated Data
#
# CONFIG_CRYPTO_CCM is not set
# CONFIG_CRYPTO_GCM is not set
# CONFIG_CRYPTO_SEQIV is not set
#
# Block modes
#
CONFIG_CRYPTO_CBC=y
# CONFIG_CRYPTO_CTR is not set
# CONFIG_CRYPTO_CTS is not set
CONFIG_CRYPTO_ECB=y
# CONFIG_CRYPTO_LRW is not set
# CONFIG_CRYPTO_PCBC is not set
# CONFIG_CRYPTO_XTS is not set
#
# Hash modes
#
# CONFIG_CRYPTO_HMAC is not set
# CONFIG_CRYPTO_XCBC is not set
# CONFIG_CRYPTO_VMAC is not set
#
# Digest
#
# CONFIG_CRYPTO_CRC32C is not set
# CONFIG_CRYPTO_GHASH is not set
# CONFIG_CRYPTO_MD4 is not set
CONFIG_CRYPTO_MD5=y
CONFIG_CRYPTO_MICHAEL_MIC=y
# CONFIG_CRYPTO_RMD128 is not set
# CONFIG_CRYPTO_RMD160 is not set
# CONFIG_CRYPTO_RMD256 is not set
# CONFIG_CRYPTO_RMD320 is not set
# CONFIG_CRYPTO_SHA1 is not set
# CONFIG_CRYPTO_SHA256 is not set
# CONFIG_CRYPTO_SHA512 is not set
# CONFIG_CRYPTO_TGR192 is not set
# CONFIG_CRYPTO_WP512 is not set
#
# Ciphers
#
CONFIG_CRYPTO_AES=y
# CONFIG_CRYPTO_ANUBIS is not set
CONFIG_CRYPTO_ARC4=y
# CONFIG_CRYPTO_BLOWFISH is not set
# CONFIG_CRYPTO_CAMELLIA is not set
# CONFIG_CRYPTO_CAST5 is not set
# CONFIG_CRYPTO_CAST6 is not set
CONFIG_CRYPTO_DES=y
# CONFIG_CRYPTO_FCRYPT is not set
# CONFIG_CRYPTO_KHAZAD is not set
# CONFIG_CRYPTO_SALSA20 is not set
# CONFIG_CRYPTO_SEED is not set
# CONFIG_CRYPTO_SERPENT is not set
# CONFIG_CRYPTO_TEA is not set
# CONFIG_CRYPTO_TWOFISH is not set
#
# Compression
#
CONFIG_CRYPTO_DEFLATE=y
# CONFIG_CRYPTO_ZLIB is not set
CONFIG_CRYPTO_LZO=y
#
# Random Number Generation
#
# CONFIG_CRYPTO_ANSI_CPRNG is not set
# CONFIG_CRYPTO_HW is not set
# CONFIG_BINARY_PRINTF is not set
#
# Library routines
#
CONFIG_BITREVERSE=y
CONFIG_GENERIC_FIND_LAST_BIT=y
# CONFIG_CRC_CCITT is not set
CONFIG_CRC16=y
# CONFIG_CRC_T10DIF is not set
# CONFIG_CRC_ITU_T is not set
CONFIG_CRC32=y
CONFIG_CRC7=y
# CONFIG_LIBCRC32C is not set
CONFIG_ZLIB_INFLATE=y
CONFIG_ZLIB_DEFLATE=y
CONFIG_LZO_COMPRESS=y
CONFIG_LZO_DECOMPRESS=y
CONFIG_DECOMPRESS_GZIP=y
CONFIG_DECOMPRESS_BZIP2=y
CONFIG_DECOMPRESS_LZMA=y
CONFIG_DECOMPRESS_LZO=y
CONFIG_HAS_IOMEM=y
CONFIG_HAS_IOPORT=y
CONFIG_HAS_DMA=y
CONFIG_NLATTR=y
#######################################################################################################################################################
I added the wl12xx files as specified in my board-dm385cbb.c is below:
/*
* Code for DM385 EVM.
*
* Copyright (C) 2010 Texas Instruments, Inc. - http://www.ti.com/
*
* This program is free software; you can redistribute it and/or
* modify it under the terms of the GNU General Public License as
* published by the Free Software Foundation version 2.
*
* This program is distributed "as is" WITHOUT ANY WARRANTY of any
* kind, whether express or implied; without even the implied warranty
* of MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
* GNU General Public License for more details.
*/
#include <linux/kernel.h>
#include <linux/init.h>
#include <linux/device.h>
#include <linux/spi/spi.h>
#include <linux/spi/flash.h>
#include <linux/platform_device.h>
#include <linux/mtd/mtd.h>
#include <linux/mtd/nand.h>
#include <linux/mtd/partitions.h>
#include <linux/gpio.h>
#include <linux/i2c.h>
#include <linux/i2c/at24.h>
#include <linux/i2c/qt602240_ts.h>
#include <linux/regulator/machine.h>
#include <linux/mfd/tps65910.h>
#include <linux/clk.h>
#include <linux/err.h>
#include <linux/leds.h>
#include <linux/wl12xx.h> //MSS added 20170816
#include <mach/hardware.h>
#include <asm/mach-types.h>
#include <asm/mach/arch.h>
#include <asm/mach/map.h>
#include <plat/mcspi.h>
#include <plat/irqs.h>
#include <plat/board.h>
#include <plat/common.h>
#include <plat/asp.h>
#include <plat/usb.h>
#include <plat/mmc.h>
#include <plat/gpmc.h>
#include <plat/nand.h>
#include <plat/hdmi_lib.h>
#include <mach/board-ti814x.h>
#ifdef CONFIG_HAVE_PWM
#include <plat/pwm.h>
#endif
#include "board-flash.h"
#include "clock.h"
#include "mux.h"
#include "hsmmc.h"
#include "control.h"
#ifdef CONFIG_INPUT_BMA250
#include <linux/i2c/bma250.h>
#endif
#ifdef CONFIG_TOUCHSCREEN_TSC2004
#include <linux/i2c/tsc2004.h>
#endif
#ifdef CONFIG_SND_SOC_TLV320AIC3X
#include <sound/tlv320aic3x.h>
#endif
#ifdef CONFIG_INPUT_ISL29023
#include <linux/isl29023.h>
#endif
#ifdef CONFIG_UIO_PDRV_GENIRQ
#include <linux/uio_driver.h>
#endif
#define GPIO_TO_PIN(bank, gpio) (32 * (bank) + (gpio))
#ifdef CONFIG_TOUCHSCREEN_TSC2004
#define GPIO_TSC2004_IRQ GPIO_TO_PIN(3, 14)
#define GPIO_TSC2004_RST GPIO_TO_PIN(3, 13)
#endif
#ifdef CONFIG_INPUT_ISL29023
#define GPIO_ISL29023_IRQ GPIO_TO_PIN(3, 3)
#endif
#ifdef CONFIG_LEDS_CARBB
#define GPIO_REC_STATUS_LED_RED GPIO_TO_PIN(3, 11)
#define GPIO_REC_STATUS_LED_GREEN GPIO_TO_PIN(3, 10)
#define GPIO_SYS_STATUS_LED_RED GPIO_TO_PIN(3, 9)
#define GPIO_SYS_STATUS_LED_GREEN GPIO_TO_PIN(3, 7)
#endif
#ifdef CONFIG_OMAP_MUX
static struct omap_board_mux board_mux[] __initdata = {
{ .reg_offset = OMAP_MUX_TERMINATOR },
};
#else
#define board_mux NULL
#endif
//********************************************************************************************
static struct omap2_hsmmc_info mmc[] = {
#ifdef CONFIG_WL12XX_PLATFORM_DATA
{
//MSS cinfigured
/* WLAN_EN is GP3[0] */
#define GPIO_WLAN_EN ((3 * 32) + 0)
/* WLAN_IRQ is GP3[1] */
#define GPIO_WLAN_IRQ ((3 * 32) + 1)
.mmc = 1,
.caps = MMC_CAP_4_BIT_DATA | MMC_CAP_POWER_OFF_CARD,
.gpio_cd = -EINVAL,
.gpio_wp = -EINVAL,
.ocr_mask = MMC_VDD_33_34, //MMC_VDD_165_195, //MMC_VDD_32_33 | MMC_VDD_33_34, /* fixed to 3.3 V */
.nonremovable = true,
},
#endif
// .mmc = 1,
// .caps = MMC_CAP_4_BIT_DATA,// | MMC_CAP_NEEDS_POLL,
// .gpio_cd = -EINVAL, /* Dedicated pins for CD and WP */
// .gpio_wp = -EINVAL,
// .ocr_mask = MMC_VDD_33_34,
#if defined(CONFIG_MMC_DM385_EMMC)
{
.mmc = 2,
.caps = MMC_CAP_8_BIT_DATA | MMC_CAP_NEEDS_POLL | MMC_CAP_NONREMOVABLE | MMC_CAP_MMC_HIGHSPEED,
.gpio_cd = -EINVAL, /* Dedicated pins for CD and WP */
.gpio_wp = -EINVAL,
.nonremovable = true,
.ocr_mask = MMC_VDD_33_34,
},
#endif
{} /* Terminator */
};
#ifdef CONFIG_TOUCHSCREEN_TSC2004
static int tsc2004_init_gpio(void)
{
int ret = 0;
ret = gpio_request(GPIO_TSC2004_RST, "tsc2004-rst");
if (ret < 0) {
printk("failed to request GPIO#%d: %d\n", GPIO_TSC2004_RST, ret);
return ret;
}
if (gpio_direction_output(GPIO_TSC2004_RST, 0)) {
printk("GPIO#%d cannot be configured as output\n", GPIO_TSC2004_RST);
return -ENXIO;
}
gpio_set_value(GPIO_TSC2004_RST, 0);
msleep(1);
gpio_set_value(GPIO_TSC2004_RST, 1);
ret = gpio_request(GPIO_TSC2004_IRQ, "tsc2004-irq");
if (ret < 0) {
printk(KERN_WARNING "failed to request GPIO#%d: %d\n",
GPIO_TSC2004_IRQ, ret);
return ret;
}
if (gpio_direction_input(GPIO_TSC2004_IRQ)) {
printk(KERN_WARNING "GPIO#%d cannot be configured as "
"input\n", GPIO_TSC2004_IRQ);
return -ENXIO;
}
gpio_set_debounce(GPIO_TSC2004_IRQ, 0xa);
return ret;
}
static void tsc2004_exit_gpio(void)
{
gpio_free(GPIO_TSC2004_RST);
gpio_free(GPIO_TSC2004_IRQ);
}
static int tsc2004_get_irq_level(void)
{
return gpio_get_value(GPIO_TSC2004_IRQ) ? 0 : 1;
}
struct tsc2004_platform_data dm385cbb_tsc2004data = {
.model = 2004,
.x_plate_ohms = 180,
.get_pendown_state = tsc2004_get_irq_level,
.init_platform_hw = tsc2004_init_gpio,
.exit_platform_hw = tsc2004_exit_gpio,
};
#endif // CONFIG_TOUCHSCREEN_TSC2004
#ifdef CONFIG_INPUT_BMA250
#if 0
static int bma250_gpio_setup(struct device *dev)
{
return 1;
}
static void bma250_gpio_teardown(struct device *dev)
{
return;
}
static struct bma250_platform_data __refdata bma250_platform_data = {
.setup = bma250_gpio_setup,
.teardown = bma250_gpio_teardown,
};
#endif
#endif // CONFIG_INPUT_BMA250
#ifdef CONFIG_SND_SOC_TLV320AIC3X
static struct aic3x_pdata dm385cbb_aic3x_data = {
.gpio_reset = GPIO_TO_PIN(0,9),
};
#endif
#ifdef CONFIG_INPUT_ISL29023
struct isl29023_platform_data isl29023_pdata = {
.rext = 100
};
#endif
static struct i2c_board_info __initdata dm385cbb_i2c0_boardinfo[] = {
#ifdef CONFIG_INPUT_BMA250
{
I2C_BOARD_INFO("bma250", 0x19),
//.platform_data = &bma250_platform_data,
},
#endif
#ifdef CONFIG_TOUCHSCREEN_TSC2004
{ // ADXL345BCCZ
I2C_BOARD_INFO("tsc2004", 0x4A),
.type = "tsc2004",
.platform_data = &dm385cbb_tsc2004data,
},
#endif
#ifdef CONFIG_INPUT_ISL29023
{
I2C_BOARD_INFO("isl29023", 0x88 >> 1),
.platform_data = &isl29023_pdata,
},
#endif
#ifdef CONFIG_SND_SOC_TLV320AIC3X
{
I2C_BOARD_INFO("tlv320aic3104", 0x18),
.platform_data = &dm385cbb_aic3x_data,
},
#endif
};
#if 1
static struct i2c_board_info __initdata dm385cbb_i2c1_boardinfo[] = {
};
#endif
static struct i2c_board_info __initdata dm385cbb_i2c2_boardinfo[] = {
// CON1001 / MIPI_CONN-1
// CON701 / PARALLERL_CONN-1
};
static struct i2c_board_info __initdata dm385cbb_i2c3_boardinfo[] = {
#ifdef CONFIG_RTC_DRV_BQ32K
{
I2C_BOARD_INFO("bq32000", 0xD0 >> 1),
},
#endif
// MCU
#ifdef CONFIG_INPUT_MCU_BRIDGE
{
I2C_BOARD_INFO("mcu_bridge", 0x55),
}
#endif
};
static void __init ti814x_evm_i2c_init(void)
{
#ifdef CONFIG_TOUCHSCREEN_TSC2004
dm385cbb_i2c0_boardinfo[1].irq = gpio_to_irq(GPIO_TSC2004_IRQ);
#endif
#ifdef CONFIG_INPUT_ISL29023
dm385cbb_i2c0_boardinfo[2].irq = gpio_to_irq(GPIO_ISL29023_IRQ);
#endif
omap_register_i2c_bus(1, 400, dm385cbb_i2c0_boardinfo,
ARRAY_SIZE(dm385cbb_i2c0_boardinfo));
//MSS - Enable I2C1 (I2C2 in software) may want to leave at 100khz try up to 400 khz
//omap_register_i2c_bus(2, 100, NULL, 0);
#if 1
omap_register_i2c_bus(2, 100, dm385cbb_i2c1_boardinfo,
ARRAY_SIZE(dm385cbb_i2c1_boardinfo));
#endif
omap_register_i2c_bus(3, 400, dm385cbb_i2c2_boardinfo,
ARRAY_SIZE(dm385cbb_i2c2_boardinfo));
omap_register_i2c_bus(4, 100, dm385cbb_i2c3_boardinfo,
ARRAY_SIZE(dm385cbb_i2c3_boardinfo));
}
static u8 dm385_iis_serializer_direction[] = {
TX_MODE, RX_MODE, INACTIVE_MODE, INACTIVE_MODE,
INACTIVE_MODE, INACTIVE_MODE, INACTIVE_MODE, INACTIVE_MODE,
INACTIVE_MODE, INACTIVE_MODE, INACTIVE_MODE, INACTIVE_MODE,
INACTIVE_MODE, INACTIVE_MODE, INACTIVE_MODE, INACTIVE_MODE,
};
static struct snd_platform_data dm385_evm_snd_data = {
.tx_dma_offset = 0x46400000,
.rx_dma_offset = 0x46400000,
.op_mode = DAVINCI_MCASP_IIS_MODE,
.num_serializer = ARRAY_SIZE(dm385_iis_serializer_direction),
.tdm_slots = 2,
.serial_dir = dm385_iis_serializer_direction,
.asp_chan_q = EVENTQ_2,
.version = MCASP_VERSION_2,
.txnumevt = 1,
.rxnumevt = 1,
};
/* NAND flash information */
static struct mtd_partition ti814x_nand_partitions[] = {
/* All the partition sizes are listed in terms of NAND block size */
{
.name = "U-Boot-min",
.offset = 0, /* Offset = 0x0 */
#ifdef CONFIG_MTD_NAND_OMAP_ECC_BCH16_CODE_HW
.size = 1 * SZ_256K,
#else
.size = SZ_128K,
#endif
},
{
.name = "U-Boot",
.offset = MTDPART_OFS_APPEND, /* Offset = 0x0 + 128K */
#ifdef CONFIG_MTD_NAND_OMAP_ECC_BCH16_CODE_HW
.size = 9 * SZ_256K,
#else
.size = 18 * SZ_128K,
#endif
},
{
.name = "U-Boot Env",
.offset = MTDPART_OFS_APPEND, /* Offset = 0x260000 */
#ifdef CONFIG_MTD_NAND_OMAP_ECC_BCH16_CODE_HW
.size = 1 * SZ_256K,
#else
.size = 1 * SZ_128K,
#endif
},
{
.name = "Kernel",
.offset = MTDPART_OFS_APPEND, /* Offset = 0x280000 */
#ifdef CONFIG_MTD_NAND_OMAP_ECC_BCH16_CODE_HW
.size = 17 * SZ_256K,
#else
.size = 34 * SZ_128K,
#endif
},
{
.name = "File System",
.offset = MTDPART_OFS_APPEND, /* Offset = 0x6C0000 */
#ifdef CONFIG_MTD_NAND_OMAP_ECC_BCH16_CODE_HW
.size = 420 * SZ_256K,
#else
.size = 840 * SZ_128K,
#endif
},
{
.name = "Data",
.offset = MTDPART_OFS_APPEND, /* Offset = 0x55C0000 */
#ifdef CONFIG_MTD_NAND_OMAP_ECC_BCH16_CODE_HW
.size = 48 * SZ_256K,
#else
.size = 96 * SZ_128K,
#endif
},
{
.name = "File System2",
.offset = MTDPART_OFS_APPEND, /* Offset = 0x61C0000 */
#ifdef CONFIG_MTD_NAND_OMAP_ECC_BCH16_CODE_HW
.size = 420 * SZ_256K,
#else
.size = 840 * SZ_128K,
#endif
},
{
.name = "Reserved",
.offset = MTDPART_OFS_APPEND, /* Offset = 0xB0C0000 */
.size = MTDPART_SIZ_FULL,
},
};
/* SPI fLash information */
struct mtd_partition dm385_spi_partitions[] = {
/* All the partition sizes are listed in terms of erase size */
{
.name = "U-Boot-min",
.offset = 0, /* Offset = 0x0 */
.size = 32 * SZ_4K,
.mask_flags = MTD_WRITEABLE, /* force read-only */
},
{
.name = "U-Boot",
.offset = MTDPART_OFS_APPEND, /* 0x0 + (32*4K) */
.size = 64 * SZ_4K,
.mask_flags = MTD_WRITEABLE, /* force read-only */
},
{
.name = "U-Boot Env",
.offset = MTDPART_OFS_APPEND, /* 0x40000 + (32*4K) */
.size = 2 * SZ_4K,
},
{
.name = "Kernel",
.offset = MTDPART_OFS_APPEND, /* 0x42000 + (32*4K) */
.size = 640 * SZ_4K,
},
{
.name = "File System",
.offset = MTDPART_OFS_APPEND, /* 0x2C2000 + (32*4K) */
.size = MTDPART_SIZ_FULL, /* size ~= 1.1 MiB */
}
};
const struct flash_platform_data dm385_spi_flash = {
.type = "w25x32",
.name = "spi_flash",
.parts = dm385_spi_partitions,
.nr_parts = ARRAY_SIZE(dm385_spi_partitions),
};
struct spi_board_info __initdata dm385_spi_slave_info[] = {
{
.modalias = "m25p80",
.platform_data = &dm385_spi_flash,
.irq = -1,
.max_speed_hz = 75000000,
.bus_num = 1,
.chip_select = 0,
},
};
void __init dm385_spi_init(void)
{
spi_register_board_info(dm385_spi_slave_info,
ARRAY_SIZE(dm385_spi_slave_info));
}
static struct omap_musb_board_data musb_board_data = {
.interface_type = MUSB_INTERFACE_ULPI,
#ifdef CONFIG_USB_MUSB_OTG
.mode = MUSB_OTG,
#elif defined(CONFIG_USB_MUSB_HDRC_HCD)
.mode = MUSB_HOST,
#elif defined(CONFIG_USB_GADGET_MUSB_HDRC)
.mode = MUSB_PERIPHERAL,
#endif
.power = 500,
.instances = 1,
};
#ifdef CONFIG_HAVE_PWM
struct omap2_pwm_platform_config dm385_cbb_pwm_cfg[] ={
{
.timer_id = 6,
.polarity = 1,
},
{
.timer_id = 7,
.polarity = 1,
}
};
#endif
static void __init dm385_evm_init_irq(void)
{
omap2_init_common_infrastructure();
omap2_init_common_devices(NULL, NULL);
omap_init_irq();
gpmc_init();
}
#ifdef CONFIG_SND_SOC_TI81XX_HDMI
static struct snd_hdmi_platform_data dm385_snd_hdmi_pdata = {
.dma_addr = TI81xx_HDMI_WP + HDMI_WP_AUDIO_DATA,
.channel = 53,
.data_type = 4,
.acnt = 4,
.fifo_level = 0x20,
};
static struct platform_device dm385_hdmi_audio_device = {
.name = "hdmi-dai",
.id = -1,
.dev = {
.platform_data = &dm385_snd_hdmi_pdata,
}
};
static struct platform_device dm385_hdmi_codec_device = {
.name = "hdmi-dummy-codec",
.id = -1,
};
/*
* HDMI Audio Auto CTS MCLK configuration.
* sysclk20, sysclk21, sysclk21 and CLKS(external)
* setting sysclk20 as the parent of hdmi_i2s_ck
* ToDo:
*/
void __init ti813x_hdmi_clk_init(void)
{
int ret = 0;
struct clk *parent, *child;
/* modify the clk name to choose diff clk*/
parent = clk_get(NULL, "sysclk20_ck");
if (IS_ERR(parent))
pr_err("Unable to get [sysclk20_ck] clk\n");
child = clk_get(NULL, "hdmi_i2s_ck");
if (IS_ERR(child))
pr_err("Unable to get [hdmi_i2s_ck] clk\n");
ret = clk_set_parent(child, parent);
if (ret < 0)
pr_err("Unable to set parent clk [hdmi_i2s_ck]\n");
clk_put(child);
clk_put(parent);
pr_debug("{{HDMI Audio MCLK setup completed}}\n");
}
#endif
#ifdef CONFIG_UIO_PDRV_GENIRQ // by denny
static struct resource mmc_irq_resources[] = {
};
static struct uio_info mmc_irq_platform_data = {
.name = "MMC_IRQ",
.version = "0",
.irq = GPIO_TO_PIN(1, 6), // gpio_to_irq(GPIO_TO_PIN(1, 6));
.irq_flags = IRQF_TRIGGER_RISING | IRQF_TRIGGER_FALLING|IRQF_DISABLED,
};
static struct platform_device mmc_irq_device = {
.name = "uio_pdrv_genirq",
.id = 0,
.dev = {
.platform_data = &mmc_irq_platform_data,
},
.resource = mmc_irq_resources,
.num_resources = ARRAY_SIZE(mmc_irq_resources),
};
static void __init dm385_mmc_irq_init(void)
{
mmc_irq_platform_data.irq = gpio_to_irq(GPIO_TO_PIN(1, 6));
platform_device_register(&mmc_irq_device);
}
#endif
#ifdef CONFIG_SND_SOC_TLV320AIC3110
static struct platform_device dm385_aic3110_audio_device = {
.name = "tlv320aic3110-codec",
.id = -1,
};
#endif
#ifdef CONFIG_LEDS_CARBB
static struct gpio_led carbb_gpio_led_pins[] =
{
{
.name = "rec_status_led_r",
.default_trigger = "timer",
.gpio = GPIO_REC_STATUS_LED_RED,
.default_state = LEDS_GPIO_DEFSTATE_OFF,
},
{
.name = "rec_status_led_g",
.default_trigger = "timer",
.gpio = GPIO_REC_STATUS_LED_GREEN,
.default_state = LEDS_GPIO_DEFSTATE_ON,
},
{
.name = "sys_status_led_r",
.default_trigger = "timer",
.gpio = GPIO_SYS_STATUS_LED_RED,
.default_state = LEDS_GPIO_DEFSTATE_OFF,
},
{
.name = "sys_status_led_g",
.default_trigger = "timer",
.gpio = GPIO_SYS_STATUS_LED_GREEN,
.default_state = LEDS_GPIO_DEFSTATE_ON,
},
};
static struct gpio_led_platform_data carbb_leds_pdata =
{
.num_leds = ARRAY_SIZE(carbb_gpio_led_pins),
.leds = carbb_gpio_led_pins,
};
static struct platform_device carbb_leds =
{
.name = "leds-gpio",
.id = -1,
.dev.platform_data = &carbb_leds_pdata,
};
#endif
static struct platform_device *dm385_devices[] __initdata = {
#ifdef CONFIG_SND_SOC_TI81XX_HDMI
&dm385_hdmi_audio_device,
&dm385_hdmi_codec_device,
#endif
#ifdef CONFIG_SND_SOC_TLV320AIC3110
&dm385_aic3110_audio_device,
#endif
#ifdef CONFIG_LEDS_CARBB
&carbb_leds,
#endif
};
// WLAN wl1271 initialization files***************************************************************************
static struct wl12xx_platform_data wlan_data __initdata = {
.irq = OMAP_GPIO_IRQ(GPIO_WLAN_IRQ),
/* COM6 (127x) uses FREF */
.board_ref_clock = WL12XX_REFCLOCK_38_XTAL,
/* COM7 (128x) uses TCXO */
.board_tcxo_clock = WL12XX_TCXOCLOCK_26,
};
//--
static int wl12xx_set_power(struct device *dev, int slot, int power_on,
int vdd)
{
printk(KERN_INFO "dm385_evm_init::twl12xx_set_power\r\n");
static bool power_state;
pr_debug("Powering %s wl12xx", power_on ? "on" : "off");
if (power_on == power_state)
return 0;
power_state = power_on;
if (power_on) {
printk(KERN_INFO "dm385_evm_init::wlan powering on\r\n");
/* Power up sequence required for wl127x devices */
gpio_set_value(GPIO_WLAN_EN, 1);
usleep_range(15000, 15000);
gpio_set_value(GPIO_WLAN_EN, 0);
usleep_range(1000, 1000);
gpio_set_value(GPIO_WLAN_EN, 1);
msleep(70);
} else {
gpio_set_value(GPIO_WLAN_EN, 0);
}
return 0;
}
//------
static void __init ti814x_wl12xx_wlan_init(void)
{
struct device *dev;
struct omap_mmc_platform_data *pdata;
int ret;
/* Set up mmc0 muxes */
omap_mux_init_signal("mmc0_clk", TI814X_INPUT_EN | TI814X_PULL_UP);
omap_mux_init_signal("mmc0_cmd", TI814X_INPUT_EN | TI814X_PULL_UP);
omap_mux_init_signal("mmc0_dat0", TI814X_INPUT_EN | TI814X_PULL_UP);
omap_mux_init_signal("mmc0_dat1", TI814X_INPUT_EN | TI814X_PULL_UP);
omap_mux_init_signal("mmc0_dat2", TI814X_INPUT_EN | TI814X_PULL_UP);
omap_mux_init_signal("mmc0_dat3", TI814X_INPUT_EN | TI814X_PULL_UP);
/* Set up the WLAN_EN and WLAN_IRQ muxes */
//gpio1_15_mux1 is good for application daughter board
printk(KERN_INFO "dm385_evm_init::ti814x_wl12xx_init()-muxing wlan pins\r\n");
//MSS temporry wait for debugging
omap_mux_init_signal("gpio3_0", TI814X_PULL_DIS); //MSS - wlan enable
omap_mux_init_signal("gpio3_1", TI814X_INPUT_EN | TI814X_PULL_DIS); //MSS - wlan IRQ
// printk(KERN_INFO "dm385_evm_init::ti814x_wl12xx_init()-Finished muxing wlan pins\r\n");
/* Pass the wl12xx platform data information to the wl12xx driver */
if (wl12xx_set_platform_data(&wlan_data)) {
pr_err("Error setting wl12xx data\n");
return;
}
else
{
pr_err("Successfully set wl12xx data\n");
}
/*
* The WLAN_EN gpio has to be toggled without using a fixed regulator,
* as the omap_hsmmc does not enable/disable regulators on the TI814X.
*/
ret = gpio_request_one(GPIO_WLAN_EN, GPIOF_OUT_INIT_LOW, "wlan_en");
if (ret) {
pr_err("Error requesting wlan enable gpio: %d\n", ret);
return;
}
else
{
pr_err("Successfully requested wlan enable gpio: %d\n", ret);
}
dev = mmc[0].dev;
if (!dev) {
pr_err("wl12xx mmc device initialization failed\n");
return;
}
else
{
pr_err("wl12xx mmc device initialization succeeded\n");
}
pdata = dev->platform_data;
if (!pdata) {
pr_err("Platform data of wl12xx device not set\n");
return;
}
else
{
pr_err("Platform data of wl12xx device is set successfully\n");
}
pdata->slots[0].set_power = wl12xx_set_power;
}
//-----
static void __init ti814x_wl12xx_init(void)
{
ti814x_wl12xx_wlan_init();
}
//--
// End of WLAN wl1271 initialization files***************************************************************************
//MSS platform initialization
static void __init dm385_evm_init(void)
{
int bw; /* bus-width */
ti814x_mux_init(board_mux);
omap_serial_init();
ti814x_evm_i2c_init();
ti81xx_register_mcasp(0, &dm385_evm_snd_data);
omap2_hsmmc_init(mmc);
/* nand initialisation */
if (0 /*cpu_is_ti814x()*/) {
u32 *control_status = TI81XX_CTRL_REGADDR(0x40);
if (*control_status & (1<<12)) {
printk(KERN_INFO "dm385_evm_init::814x: 8-bit NAND\r\n");
bw = 0; /*8-bit nand if BTMODE BW pin on board is ON*/
}
else {
printk(KERN_INFO "dm385_evm_init::814x: 16-bit NAND\r\n");
bw = 1; /*16-bit nand if BTMODE BW pin on board is OFF*/
}
board_nand_init(ti814x_nand_partitions, ARRAY_SIZE(ti814x_nand_partitions), 0, bw);
}
else {
printk(KERN_INFO "dm385_evm_init::dm38x: 16-bit NAND\r\n");
board_nand_init(ti814x_nand_partitions, ARRAY_SIZE(ti814x_nand_partitions), 0, NAND_OMAP_BUS_16);
}
/* initialize usb */
usb_musb_init(&musb_board_data);
#ifdef CONFIG_SND_SOC_TI81XX_HDMI
/* hdmi mclk setup */
ti813x_hdmi_clk_init();
#endif
platform_add_devices(dm385_devices, ARRAY_SIZE(dm385_devices));
regulator_use_dummy_regulator();
#ifdef CONFIG_HAVE_PWM
omap_register_pwm_config(dm385_cbb_pwm_cfg, ARRAY_SIZE(dm385_cbb_pwm_cfg));
#endif
#ifdef CONFIG_UIO_PDRV_GENIRQ // by denny
dm385_mmc_irq_init();
#endif
//MSS - Initialize the wlan12xx
printk(KERN_INFO "dm385_evm_init::ti814x_wl12xx_init()\r\n");
ti814x_wl12xx_init();
//MSS temporry wait for debugging
msleep(5000);
}
static void __init dm385_evm_map_io(void)
{
omap2_set_globals_ti816x();
ti81xx_map_common_io();
}
MACHINE_START(DM385CBB, "dm385cbb")
/* Maintainer: Texas Instruments */
.boot_params = 0x80000100,
.map_io = dm385_evm_map_io,
.reserve = ti81xx_reserve,
.init_irq = dm385_evm_init_irq,
.init_machine = dm385_evm_init,
.timer = &omap_timer,
MACHINE_END