Need to run a SPI port in Master Mode and use dMAX also. Documentation only talks about using dMAX for SPI slave mode.
If I set up a SPI slave transfer in dMAX for a SPI in master mode and manually start the first transfer, will the SPI generate the proper input events to cause the slave transfer complete correctly?
Thanks in advance