Part Number: BEAGLEBK
Tool/software: Linux
Hi,
I am trying to write an image (bone-debian-8.6-iot-armhf-2016-12-09-4gb) on a Beaglebone Black (Rev C) via SD Card following the instruction of the beaglebone black getting started guide. I have two SD Cards and by mistake I mounted the empty one on the Beaglebone causing a segmentation fault. Now when trying again with the correct one (the SD Card that has the image) nothing happens and I am not able to communicate anymore with the beaglebone. Just two leds turn on (USR0 and USR1), then nothing else happens. It seems like the eMMC is empty and there is no way to interact with the board.
I would like to know if there is any way to solve this issue. Any suggestion would be helpful. Thanks.