This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM4379: DDR address line noise

Guru 10570 points

Part Number: AM4379
Other Parts Discussed in Thread: TMDXSK437X

Hello,

I have seen the noise on DDR_A0 (N1) line in TMDXSK437X.
Since its noise also can be seen in our target board, we think AM437x output the noise.

a) AM437x DDR controller potentially output noise on A0 line. Is it known issue ?

b) We encounterd read/write error on our target board. To avoid it we are considering to change the termination resistor value from 50ohm to 100ohm.
Do you think its workaround have any possible to encounter any another problem?
Because datasheet specifies Zo as typ 50ohm max 75ohm.

c) Can you recommend the DDR3L design without termination regulator? It's another our workaround to avoid read/write error.


Best regards, RY

DDR_A0 (N1) line noise n TMDXSK437X

AM437x datasheet specifies Zo as typ 50ohm max 75ohm

  • Hi,

    a) No, this is not a known issue. This may be caused by you using an improper probe to measure the signal. Low capacitance FET probes should be used for measuring DDR signals.
    b) Termination resistor should be 50Ohm.
    c) There is no such reference design for AM437x.

    Please check that your memory is configured according to this document: www.ti.com/.../sprac70.pdf
  • Biser,

    Thanks for your comment!
    I will check that there is no issue on AM437x in other board.
    So will return when I finished.

    Best regards, RY
  • - TMDXSK437X board does not use Parallel termination on the Addr/Ctrl lines. It uses a balanced T-topology for the DDR interface for the Addr/Ctrl lines. Therefore, it is unclear to me if you are referring to termination resistor on the TI board or your board

    - Does your implementation use parallel termination (VTT) termination on the Addr/Ctrl lines? If so, this would be a different implementation than the TI SK board as mentioned above

    - With regards to the noise you measured, it is unclear where you are measuring - close to the DRAM or the processor? The measurement looks like on the TI board. How does this measurement match with your board. I'm unable to see the correlation of this noise on your board vs. TI board

    - The noise you are measuring is <200mV which is well within the VIH(min) of the Addr/Ctrl lines for the DRAM. Is this the same level of noise you measure on your board? If it is <200mV, this should not be the source of read/write errors

    - How did you arrive the noise on the Addr/Ctrl lines is the source of the read/write error? Did you verify if all the DDR settings and configuration is fine?

    - without assessing the real issue, changing the termination resistor to 100 ohm might not solve the issue

    Regards, Siva

  • Hi, Siva.
    Thanks for your response.


    sivak said:
    - TMDXSK437X board does not use Parallel termination on the Addr/Ctrl lines. It uses a balanced T-topology for the DDR interface for the Addr/Ctrl lines. Therefore, it is unclear to me if you are referring to termination resistor on the TI board or your board

    Thanks. We are referring the customer's target board.


    sivak said:
    - Does your implementation use parallel termination (VTT) termination on the Addr/Ctrl lines? If so, this would be a different implementation than the TI SK board as mentioned above

    Yes.
    So I have a question.
    You do NOT recommend to use parallel termination (VTT) with AM437x and DDR3L?


    sivak said:
    - With regards to the noise you measured, it is unclear where you are measuring - close to the DRAM or the processor? The measurement looks like on the TI board. How does this measurement match with your board. I'm unable to see the correlation of this noise on your board vs. TI board

    We can see the noise both on the target board and SK.
    Measure point is R107 on SK which is close to the Processor.


    sivak said:
    - The noise you are measuring is <200mV which is well within the VIH(min) of the Addr/Ctrl lines for the DRAM. Is this the same level of noise you measure on your board? If it is <200mV, this should not be the source of read/write errors

    I agree with you.
    Thanks for your comment.
    I will check it to the customer.


    sivak said:
    - How did you arrive the noise on the Addr/Ctrl lines is the source of the read/write error? Did you verify if all the DDR settings and configuration is fine?

    We can see the error as following:

    When write to address 0x80000000, Value changes on address 0x80000004.
    When write to address 0x80000004, Value changes on address 0x80000008.
    When write to address 0x80000008, Value changes on address 0x8000000C.
    When write to address 0x8000000C, no changes.

    We have already verified the DDR regs. on AM437x.
    Since SK can work with same configuration as target board, we think our DDR setting is fine.


    sivak said:
    - without assessing the real issue, changing the termination resistor to 100 ohm might not solve the issue

    We use 50ohm as parallel termination resister.
    It is specified as Zo on datasheet. Is that any problems?

    SPRS851D (P180) Table 5-53. PCB Stackup Specifications


    Best regards,
    Ryutaro Yoshida

  • Yoshida-san

    #1 OK. Thanks for clarifying. So, the customer board uses VTT termination. Correct? I'm not sure then why you are comparing with TI SK board. Can you please clarify why you are comparing with SK board?

    #2 I'm not recommending to remove the VTT termination. I want to clarify that TI SK board uses a different topology. TI GP EVM uses VTT termination, if you are looking for a TI board with VTT termination. All the supported memory configuration and topologies are listed in our AM437x data sheet. Please refer to the Section 5.13.8.2 which has details on the DDR3 implementation

    #3 Just to re-iterate again, the noise you are measuring <200mV should be much lower than the VIH(min) of the DRAM part. Therefore, I suspect if the noise on the address line you measured is the real issue here

    #4 Could you help specifically more on the fail signature - does the value written to 0x80000000 appear on 0x80000004 or the change on 0x80000004 is random? I strongly suggest you review your DDR configuration. Please use this tool to arrive at the right settings -  www.ti.com/lit/an/sprac70/sprac70.pdf. Please share the results of the tool and your configuration so we can take a look and comment more

    #5 I don't see an issue in using 50 ohm as the parallel termination resistor if your Z0 is 50 ohm

    As I mentioned earlier, please make sure you do the following:

    - Make sure your layout is implemented as per the requirements in the data sheet

    - Verify the EMIF configuration and settings. You can use the EMIF tool that I pointed above for this

    After you have both the above, let us review again. Please let me know if you have any other questions

    Regards, Siva

  • Siva,

    Thank you so much for your advise.
    We can NOT attach the customer's details because it have to utilize as NDA information.
    So TI Japan local staff will send them.

    Best regards, RY