Other Parts Discussed in Thread: AM5728, DS90C387
Tool/software: Linux
I'm using the AM5728 coupled with the DS90C387 in a single-to-dual LVDS setup, however we cannot get anything to show up on the display (not even a scrambled image). Our display clock frequency is 74MHz, we have properly configured the RGB clock frequency to 148MHz (DS90C387 splits this clock). It appears that the hsync, vsync, and DE has a period 1/2 as long as its supposed to be - wondering how to adjust the timing parameters of these signals?