This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

About REZ function of DM365.

Genius 3400 points

Hi all:

      At recently, I had meet a very strage problem.

      On DM365, program based on IPNC, I get YUV422 data(pix:2432x2050 ) from ISIF,  use RSZ to convert to YUV422. and then contrast the data in hex like this:.

 After RSZ,  Compared to original data,  I found two lines in front have missed, it start from the third line. and the last two line repeated two times.

I have no idea about the setting of RSZ.

Anybody can help me?

Thanks a lot.