This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/AM5718: AM5718 Boot Time

Part Number: AM5718
Other Parts Discussed in Thread: DRA722, PMP, TMP102, TLC59108

Tool/software: Linux

Hi,

We have developed a custom board with AM5718 Processor, and boot time is around 20 seconds. Is it possible to reduce the boot time to less than 10 seconds. Please check my boot log also,

U-Boot SPL 2015.07-00080-g4523775-dirty (Feb 24 2017 - 15:00:29)
DRA722 ES1.0

U-Boot SPL 2015.07-00080-g4523775-dirty (Feb 24 2017 - 15:00:29)
DRA722 ES1.0
reading args
spl_load_image_fat_os: error reading image args, err - -1
reading u-boot.img
reading u-boot.img
ti_i2c_eeprom_init failed 1                                                     
                                                                                
                                                                                
U-Boot 2015.07-00080-g4523775-dirty (Feb 24 2017 - 15:00:29 +0530)              
                                                                                
CPU  : DRA722 ES1.0                                                             
Board: AM571x II2C:   ready                                                     
DRAM:  1 GiB                                                                    
MMC:   OMAP SD/MMC: 0, OMAP SD/MMC: 1                                           
reading uboot.env                                                               
SCSI:  SATA link 0 timeout.                                                     
AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl SATA mode                       
flags: 64bit ncq stag pm led clo only pmp pio slum part ccc apst                
scanning bus for devices...                                                     
Found 0 device(s).                                                              
Net:                                                                            
 **********Auto Negotiation Available******cpsw                                 
Hit any key to stop autoboot:  0                                                
Card did not respond to voltage select!                                         
Card did not respond to voltage select!                                         
switch to partitions #0, OK                                                     
mmc1(part 0) is current device                                                  
SD/MMC found on device 1                                                        
reading uEnv.txt                                                                
574 bytes read in 5 ms (111.3 KiB/s)                                            
Loaded environment from uEnv.txt                                                
Importing environment from mmc1 ...                                             
3576616 bytes read in 213 ms (16 MiB/s)                                         
89657 bytes read in 31 ms (2.8 MiB/s)                                           
Booting from mmc1 ...                                                           
Card did not respond to voltage select!                                         
** Bad device mmc 0 **                                                          
Kernel image @ 0x82000000 [ 0x000000 - 0x369328 ]                               
## Flattened Device Tree blob at 88000000                                       
   Booting using the fdt blob at 0x88000000                                     
   Loading Device Tree to 8ffe7000, end 8ffffe38 ... OK                         
                                                                                
Starting Medha kernel ...

[    0.000000] Booting Linux on physical CPU 0x0
[    0.000000] Initializing cgroup subsys cpuset
[    0.000000] Initializing cgroup subsys cpu
[    0.000000] Initializing cgroup subsys cpuacct
[    0.000000] Linux version 4.1.13-g8dc6617 (medha@medha) (gcc version 4.9.3 20150413 (prerelease) (Linaro GCC 4.9-2015.05) ) #83 SMP PREEMPT7
[    0.000000] CPU: ARMv7 Processor [412fc0f2] revision 2 (ARMv7), cr=30c5387d
[    0.000000] CPU: PIPT / VIPT nonaliasing data cache, PIPT instruction cache
[    0.000000] Machine model: TI AM571x IDK
[    0.000000] Reserved memory: created CMA memory pool at 0x0000000095800000, size 56 MiB
[    0.000000] Reserved memory: initialized node ipu2_cma@95800000, compatible id shared-dma-pool
[    0.000000] Reserved memory: created CMA memory pool at 0x0000000099000000, size 64 MiB
[    0.000000] Reserved memory: initialized node dsp1_cma@99000000, compatible id shared-dma-pool
[    0.000000] Reserved memory: created CMA memory pool at 0x000000009d000000, size 32 MiB
[    0.000000] Reserved memory: initialized node ipu1_cma@9d000000, compatible id shared-dma-pool
[    0.000000] cma: Reserved 24 MiB at 0x00000000be400000
[    0.000000] Forcing write-allocate cache policy for SMP
[    0.000000] Memory policy: Data cache writealloc
[    0.000000] DRA722 ES1.0
[    0.000000] PERCPU: Embedded 11 pages/cpu @eee4d000 s16128 r8192 d20736 u45056
[    0.000000] Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 210514
[    0.000000] Kernel command line: console=ttyO0,115200n8 root=PARTUUID=18e1dc9e-02 rw rootfstype=ext4 rootwait
[    0.000000] PID hash table entries: 4096 (order: 2, 16384 bytes)
[    0.000000] Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)
[    0.000000] Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)
[    0.000000] Memory: 649612K/848896K available (6743K kernel code, 301K rwdata, 2312K rodata, 340K init, 258K bss, 19060K reserved, 180224K )
[    0.000000] Virtual kernel memory layout:
[    0.000000]     vector  : 0xffff0000 - 0xffff1000   (   4 kB)
[    0.000000]     fixmap  : 0xffc00000 - 0xfff00000   (3072 kB)
[    0.000000]     vmalloc : 0xf0000000 - 0xff000000   ( 240 MB)
[    0.000000]     lowmem  : 0xc0000000 - 0xef800000   ( 760 MB)
[    0.000000]     pkmap   : 0xbfe00000 - 0xc0000000   (   2 MB)
[    0.000000]     modules : 0xbf000000 - 0xbfe00000   (  14 MB)
[    0.000000]       .text : 0xc0008000 - 0xc08e0074   (9057 kB)
[    0.000000]       .init : 0xc08e1000 - 0xc0936000   ( 340 kB)
[    0.000000]       .data : 0xc0936000 - 0xc0981428   ( 302 kB)
[    0.000000]        .bss : 0xc0984000 - 0xc09c48cc   ( 259 kB)
[    0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
[    0.000000] Preemptible hierarchical RCU implementation.
[    0.000000]  Additional per-CPU info printed with stalls.
[    0.000000]  RCU restricting CPUs from NR_CPUS=4 to nr_cpu_ids=1.
[    0.000000] RCU: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=1
[    0.000000] NR_IRQS:16 nr_irqs:16 16
[    0.000000] OMAP clockevent source: timer1 at 32768 Hz
[    0.000000] clocksource 32k_counter: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 58327039986419 ns
[    0.000000] sched_clock: 32 bits at 32kHz, resolution 30517ns, wraps every 65535999984741ns
[    0.000030] OMAP clocksource: 32k_counter at 32768 Hz
[    0.000427] Architected cp15 timer(s) running at 6.14MHz (virt).
[    0.000427] clocksource arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x16af5adb9, max_idle_ns: 440795202250 ns
[    0.000462] sched_clock: 56 bits at 6MHz, resolution 162ns, wraps every 4398046511023ns
[    0.000472] Switching to timer-based delay loop, resolution 162ns
[    0.000976] Console: colour dummy device 80x30
[    0.000991] WARNING: Your 'console=ttyO0' has been replaced by 'ttyS0'
[    0.000997] This ensures that you still see kernel messages. Please
[    0.001002] update your kernel commandline.
[    0.001013] Calibrating delay loop (skipped), value calculated using timer frequency.. 12.29 BogoMIPS (lpj=61475)
[    0.001025] pid_max: default: 32768 minimum: 301
[    0.001107] Security Framework initialized
[    0.001142] Mount-cache hash table entries: 2048 (order: 1, 8192 bytes)
[    0.001152] Mountpoint-cache hash table entries: 2048 (order: 1, 8192 bytes)
[    0.001678] Initializing cgroup subsys blkio
[    0.001693] Initializing cgroup subsys memory
[    0.001718] Initializing cgroup subsys devices
[    0.001730] Initializing cgroup subsys freezer
[    0.001742] Initializing cgroup subsys perf_event
[    0.001763] CPU: Testing write buffer coherency: ok
[    0.002023] /cpus/cpu@0 missing clock-frequency property
[    0.002035] CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
[    0.002070] Setting up static identity map for 0x80008380 - 0x800083d8
[    0.040755] Brought up 1 CPUs
[    0.040767] SMP: Total of 1 processors activated (12.29 BogoMIPS).
[    0.040773] CPU: All CPU(s) started in SVC mode.
[    0.041125] devtmpfs: initialized
[    0.064782] VFP support v0.3: implementor 41 architecture 4 part 30 variant f rev 0
[    0.065589] omap_hwmod: l3_main_2 using broken dt data from ocp
[    0.078493] omap_hwmod: tptc0 using broken dt data from edma-controller
[    0.078959] omap_hwmod: tptc1 using broken dt data from edma-controller
[    0.245540] clocksource jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
[    0.249355] pinctrl core: initialized pinctrl subsystem
[    0.250161] NET: Registered protocol family 16
[    0.251140] DMA: preallocated 256 KiB pool for atomic coherent allocations
[    0.259079] OMAP GPIO hardware version 0.1
[    0.261210] omap_gpio 48059000.gpio: could not find pctldev for node /ocp/l4@4a000000/scm@2000/pinmux@1400/gpio4_pins_default, deferring pre
[    0.283761] No ATAGs?
[    0.283786] hw-breakpoint: found 5 (+1 reserved) breakpoint and 4 watchpoint registers.
[    0.283796] hw-breakpoint: maximum watchpoint size is 8 bytes.
[    0.286216] omap4_sram_init:Unable to allocate sram needed to handle errata I688
[    0.286226] omap4_sram_init:Unable to get sram pool needed to handle errata I688
[    0.286795] OMAP DMA hardware revision 0.0
[    0.327912] edma-dma-engine edma-dma-engine.0: TI EDMA DMA engine driver
[    0.330541] omap-dma-engine 4a056000.dma-controller: OMAP DMA engine driver
[    0.335355] omap-iommu 40d01000.mmu: 40d01000.mmu registered
[    0.335538] omap-iommu 40d02000.mmu: 40d02000.mmu registered
[    0.335693] omap-iommu 58882000.mmu: 58882000.mmu registered
[    0.335852] omap-iommu 55082000.mmu: 55082000.mmu registered
[    0.336124] vgaarb: loaded
[    0.336493] SCSI subsystem initialized
[    0.338405] palmas 0-0058: IRQ missing: skipping irq request
[    0.351057] palmas 0-0058: Muxing GPIO 51, PWM 0, LED 2
[    0.391515] omap_i2c 48070000.i2c: bus 0 rev0.12 at 400 kHz
[    0.391692] media: Linux media interface: v0.10
[    0.391751] Linux video capture interface: v2.00
[    0.391793] pps_core: LinuxPPS API ver. 1 registered
[    0.391800] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[    0.391825] PTP clock support registered
[    0.392457] omap-mailbox 4883c000.mailbox: omap mailbox rev 0x400
[    0.392751] omap-mailbox 4883e000.mailbox: omap mailbox rev 0x400
[    0.393029] omap-mailbox 48840000.mailbox: omap mailbox rev 0x400
[    0.393098] omap-mailbox: probe of 48842000.mailbox failed with error -22
[    0.393326] Advanced Linux Sound Architecture Driver Initialized.
[    0.393990] Switched to clocksource arch_sys_counter
[    0.403351] missing cooling_device property
[    0.403361] failed to build thermal zone board_thermal: -2
[    0.403466] NET: Registered protocol family 2
[    0.404054] TCP established hash table entries: 8192 (order: 3, 32768 bytes)
[    0.404118] TCP bind hash table entries: 8192 (order: 4, 65536 bytes)
[    0.404242] TCP: Hash tables configured (established 8192 bind 8192)
[    0.404295] UDP hash table entries: 512 (order: 2, 16384 bytes)
[    0.404326] UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)
[    0.404524] NET: Registered protocol family 1
[    0.404771] RPC: Registered named UNIX socket transport module.
[    0.404781] RPC: Registered udp transport module.
[    0.404787] RPC: Registered tcp transport module.
[    0.404792] RPC: Registered tcp NFSv4.1 backchannel transport module.
[    0.405773] CPU PMU: Failed to parse /pmu/interrupt-affinity[0]
[    0.405803] hw perfevents: enabled with armv7_cortex_a15 PMU driver, 7 counters available
[    0.407709] futex hash table entries: 256 (order: 2, 16384 bytes)
[    0.407788] audit: initializing netlink subsys (disabled)
[    0.407822] audit: type=2000 audit(0.390:1): initialized
[    0.414808] VFS: Disk quotas dquot_6.6.0
[    0.414968] VFS: Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
[    0.417001] NFS: Registering the id_resolver key type
[    0.417030] Key type id_resolver registered
[    0.417038] Key type id_legacy registered
[    0.417097] jffs2: version 2.2. (NAND) (SUMMARY)  �© 2001-2006 Red Hat, Inc.
[    0.419461] NET: Registered protocol family 38
[    0.419539] bounce: pool size: 64 pages
[    0.419551] io scheduler noop registered
[    0.419561] io scheduler deadline registered
[    0.419598] io scheduler cfq registered (default)
[    0.423038] pinctrl-single 4a003400.pinmux: 281 pins at pa fc003400 size 1124
[    0.423151] pinctrl-single 4a002e8c.pinmux: 1 pins at pa fc002e8c size 4
[    0.437809] dra7-pcie 51000000.pcie: PCI host bridge to bus 0000:00
[    0.437823] pci_bus 0000:00: root bus resource [io  0x1000-0xffff]
[    0.437834] pci_bus 0000:00: root bus resource [mem 0x20013000-0x2fffffff]
[    0.437844] pci_bus 0000:00: root bus resource [bus 00-ff]
[    0.437963] pci 0000:00:00.0: IOMMU is currently not supported for PCI
[    0.438224] PCI: bus0: Fast back to back transfers disabled
[    0.438615] pci 0000:01:00.0: IOMMU is currently not supported for PCI
[    0.438981] PCI: bus1: Fast back to back transfers disabled
[    0.439113] pci 0000:00:00.0: BAR 8: assigned [mem 0x20400000-0x20ffffff]
[    0.439126] pci 0000:00:00.0: BAR 0: assigned [mem 0x20100000-0x201fffff]
[    0.439139] pci 0000:00:00.0: BAR 1: assigned [mem 0x20020000-0x2002ffff]
[    0.439151] pci 0000:00:00.0: BAR 7: assigned [io  0x1000-0x1fff]
[    0.439164] pci 0000:01:00.0: BAR 0: assigned [mem 0x20800000-0x20ffffff]
[    0.439183] pci 0000:01:00.0: BAR 3: assigned [mem 0x20400000-0x20403fff]
[    0.439201] pci 0000:01:00.0: BAR 2: assigned [io  0x1000-0x101f]
[    0.439219] pci 0000:00:00.0: PCI bridge to [bus 01]
[    0.439229] pci 0000:00:00.0:   bridge window [io  0x1000-0x1fff]
[    0.439240] pci 0000:00:00.0:   bridge window [mem 0x20400000-0x20ffffff]
[    0.441034] ldo5: supplied by evm_3v3_sd
[    0.441564] OMAP DSS rev 6.1
[    0.441828] omapdss_dss 58000000.dss: bound 58001000.dispc (ops dispc_component_ops)
[    0.446436] Serial: 8250/16550 driver, 10 ports, IRQ sharing enabled
[    0.449365] 4806a000.serial: ttyS0 at MMIO 0x4806a000 (irq = 267, base_baud = 3000000) is a 8250
[    1.440924] console [ttyS0] enabled
[    1.445113] 48068000.serial: ttyS5 at MMIO 0x48068000 (irq = 268, base_baud = 3000000) is a 8250
[    1.454613] 48420000.serial: ttyS6 at MMIO 0x48420000 (irq = 269, base_baud = 3000000) is a 8250
[    1.464095] 48422000.serial: ttyS7 at MMIO 0x48422000 (irq = 270, base_baud = 3000000) is a 8250
[    1.473948] [drm] Initialized drm 1.1.0 20060810
[    1.486897] brd: module loaded
[    1.493929] loop: module loaded
[    1.498532] ahci 4a140000.sata: SSS flag set, parallel bus scan disabled
[    1.505342] ahci 4a140000.sata: AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl platform mode
[    1.513909] ahci 4a140000.sata: flags: 64bit ncq sntf stag pm led clo only pmp pio slum part ccc apst
[    1.524151] scsi host0: ahci
[    1.527320] ata1: SATA max UDMA/133 mmio [mem 0x4a140000-0x4a1410ff] port 0x100 irq 307
[    1.535758] mtdoops: mtd device (mtddev=name/number) must be supplied
[    1.543649] libphy: Fixed MDIO Bus: probed
[    1.548353] e1000: Intel(R) PRO/1000 Network Driver - version 7.3.21-k8-NAPI
[    1.555449] e1000: Copyright (c) 1999-2006 Intel Corporation.
[    1.561284] e1000e: Intel(R) PRO/1000 Network Driver - 2.3.2-k
[    1.567175] e1000e: Copyright(c) 1999 - 2014 Intel Corporation.
[    1.573185] igb: Intel(R) Gigabit Ethernet Network Driver - version 5.2.15-k
[    1.580279] igb: Copyright (c) 2007-2014 Intel Corporation.
[    1.585949] igb 0000:01:00.0: enabling device (0140 -> 0142)
[    1.603252] CTRL_CORE_MAC_ID_SW_3  5cf821
[    1.607294] CTRL_CORE_MAC_ID_SW_2  3f83ab
[    1.630989] pps pps0: new PPS source ptp0
[    1.635043] igb 0000:01:00.0: added PHC on eth0
[    1.639594] igb 0000:01:00.0: Intel(R) Gigabit Ethernet Network Connection
[    1.646514] igb 0000:01:00.0: eth0: (PCIe:2.5Gb/s:Width x1) 5c:f8:21:3f:83:ab
[    1.653682] igb 0000:01:00.0: eth0: PBA No: FFFFFF-0FF
[    1.658856] igb 0000:01:00.0: Using legacy interrupts. 1 rx queue(s), 1 tx queue(s)
[    1.714018] davinci_mdio 48485000.mdio: davinci mdio revision 1.6
[    1.720144] davinci_mdio 48485000.mdio: detected phy mask fffffdff
[    1.728628] libphy: 48485000.mdio: probed
[    1.732660] davinci_mdio 48485000.mdio: phy[9]: device 48485000.mdio:09, driver unknown
[    1.741248] CTRL_CORE_MAC_ID_SW_1  5cf821
[    1.745322] CTRL_CORE_MAC_ID_SW_0  3f83aa
[    1.749347] mac addr[i] 5c
[    1.752062] mac addr[i] f8
[    1.754829] mac addr[i] 21
[    1.757544] mac addr[i] 3f
[    1.760258] mac addr[i] 83
[    1.762971] mac addr[i] aa
[    1.765727] cpsw 48484000.ethernet: Missing slave[1] phy_id property
[    1.772108] CTRL_CORE_MAC_ID_SW_1  5cf821
[    1.776182] CTRL_CORE_MAC_ID_SW_0  3f83aa
[    1.780206] mac addr[i] 5c
[    1.782921] mac addr[i] f8
[    1.785653] mac addr[i] 21
[    1.788367] mac addr[i] 3f
[    1.791084] mac addr[i] 83
[    1.793797] mac addr[i] aa
[    1.796545] cpsw 48484000.ethernet: Detected MACID = 5c:f8:21:3f:83:aa
[    1.804603] mousedev: PS/2 mouse device common for all mice
[    1.810683] RTC date time get
[    1.813973] rtc-ds1307 0-0068: rtc core: registered ds1307 as rtc0
[    1.820427] rtc-ds1307 0-0068: 56 bytes nvram
[    1.824880] i2c /dev entries driver
[    1.830020] tmp102 0-0049: initialized
[    1.835215] omap_hsmmc 4809c000.mmc: Got CD GPIO
[    1.874665] omap_hsmmc 480b4000.mmc: no pinctrl state for sdr25 mode
[    1.882105] omap_hsmmc 480b4000.mmc: no pinctrl state for sdr12 mode
[    1.890538] omap_hsmmc 480b4000.mmc: no pinctrl state for ddr_1_8v mode
[    1.897263] ata1: SATA link down (SStatus 0 SControl 300)
[    1.902733] omap_hsmmc 480b4000.mmc: no pinctrl state for hs mode
[    1.908953] omap_hsmmc 480b4000.mmc: no pinctrl state for hs200_1_8v mode
[    1.954275] ledtrig-cpu: registered to indicate activity on CPUs
[    1.961741] omap-aes 4b500000.aes: OMAP AES hw accel rev: 3.3
[    1.970408] omap-aes 4b700000.aes: OMAP AES hw accel rev: 3.3
[    1.976776] omap-des 480a5000.des: OMAP DES hw accel rev: 2.2
[    1.983690] omap-sham 4b101000.sham: hw accel on OMAP rev 4.3
[    1.996324] davinci-mcasp 48468000.mcasp: ERRATA i868 workaround is enabled
[    2.004640] oprofile: using timer interrupt.
[    2.009166] Initializing XFRM netlink socket
[    2.013475] NET: Registered protocol family 17
[    2.018137] NET: Registered protocol family 15
[    2.022692] Key type dns_resolver registered
[    2.027165] omap_voltage_late_init: Voltage driver support not added
[    2.033824] Power Management for TI OMAP4+ devices.
[    2.039011] ThumbEE CPU extension supported.
[    2.043367] Registering SWP/SWPB emulation handler
[    2.049692] dmm 4e000000.dmm: workaround for errata i878 in use
[    2.055729] mmc1: MAN_BKOPS_EN bit is not set
[    2.060900] mmc1: new MMC card at address 0001
[    2.065929] dmm 4e000000.dmm: initialized all PAT entries
[    2.071788] mmcblk0: mmc1:0001 MMC04G 3.60 GiB
[    2.077494] mmcblk0boot0: mmc1:0001 MMC04G partition 1 16.0 MiB
[    2.083554] mmcblk0boot1: mmc1:0001 MMC04G partition 2 16.0 MiB
[    2.089607] tlc59108 0-0040: Successfully initialized tlc59108
[    2.098550]  mmcblk0: p1 p2
[    2.116357] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).
[    2.123001] [drm] No driver support for vblank timestamp query.
[    2.132193] [drm] Enabling DMM ywrap scrolling
[    2.177657] Console: switching to colour frame buffer device 100x37
[    2.187405] omapdrm omapdrm.0: fb0: omapdrm frame buffer device
[    2.193349] omapdrm omapdrm.0: registered panic notifier
[    2.224180] omapwb-m2m: Device registered as video10
[    2.229170] [drm] Initialized omapdrm 1.0.0 20110917 on minor 0
[    2.235355] RTC date time get
[    2.238515] rtc-ds1307 0-0068: setting system clock to 2017-07-18 16:59:01 UTC (1500397141)
[    2.247377] fdt: not creating '/sys/firmware/fdt': CRC check failed
[    2.265254] ldo4: disabling
[    2.268537] ldo2: disabling
[    2.271639] aic_dvdd_fixed: disabling
[    2.275339] vdd_3v3: disabling
[    2.278610] ALSA device list:
[    2.281587]   No soundcards found.
[    2.743714] EXT4-fs (mmcblk0p2): recovery complete
[    2.751052] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
[    2.759221] VFS: Mounted root (ext4 filesystem) on device 179:2.
[    2.773881] devtmpfs: mounted
[    2.777084] Freeing unused kernel memory: 340K (c08e1000 - c0936000)
INIT: version 2.88 booting
Starting udev
[    5.944918] udevd[104]: starting version 182
[    7.070958] omap_rng 48090000.rng: OMAP Random Number Generator ver. 20
[    7.157192] CAN device driver interface
[    7.389427] c_can_platform 4ae3c000.can: c_can_platform device registered (regs=fce3c000, irq=316)
[    7.556976] omap_wdt: OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec
[    7.606358] c_can_platform 48480000.can: c_can_platform device registered (regs=fa480000, irq=317)
[    7.742048] vpe 489d0000.vpe: loading firmware vpdma-1b8.bin
[    8.234286] vpe 489d0000.vpe: Device registered as /dev/video0
[    8.423766] ldo4: supplied by evm_3v3_sd
[    8.888263] ldo1: supplied by evm_3v3_sd
[    8.892440] vdd_3v3: supplied by ldo1
[    8.896490] aic_dvdd_fixed: supplied by vdd_3v3
[    8.929771] Enter davinci_mcasp_set_sysclk()
[    8.934782] dir == SND_SOC_CLOCK_OUT
[    8.938417] Enter davinci_mcasp_set_dai_fmt()
[    8.942819] case SND_SOC_DAIFMT_CBM_CFM
[    8.947242] asoc-simple-card sound@0: tlv320aic3x-hifi <-> 48468000.mcasp mapping ok
[   11.882905] FAT-fs (mmcblk0p1): Volume was not properly unmounted. Some data may be corrupt. Please run fsck.
[   12.877408] usbcore: registered new interface driver usbfs
[   12.883449] usbcore: registered new interface driver hub
[   12.889394] usbcore: registered new device driver usb
[   13.310003] xhci-hcd xhci-hcd.0.auto: xHCI Host Controller
[   13.315606] xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 1
[   13.323659] xhci-hcd xhci-hcd.0.auto: hcc params 0x0220f04c hci version 0x100 quirks 0x00210010
[   13.332490] xhci-hcd xhci-hcd.0.auto: irq 423, io mem 0x48890000
[   13.339557] hub 1-0:1.0: USB hub found
[   13.343355] hub 1-0:1.0: 1 port detected
[   13.347711] xhci-hcd xhci-hcd.0.auto: xHCI Host Controller
[   13.353230] xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 2
[   13.361034] usb usb2: We don't know the algorithms for LPM for this host, disabling LPM.
[   13.370078] hub 2-0:1.0: USB hub found
[   13.373872] hub 2-0:1.0: 1 port detected
[   13.379029] xhci-hcd xhci-hcd.1.auto: xHCI Host Controller
[   13.384603] xhci-hcd xhci-hcd.1.auto: new USB bus registered, assigned bus number 3
[   13.392573] xhci-hcd xhci-hcd.1.auto: hcc params 0x0220f04c hci version 0x100 quirks 0x00210010
[   13.401399] xhci-hcd xhci-hcd.1.auto: irq 424, io mem 0x488d0000
[   13.408399] hub 3-0:1.0: USB hub found
[   13.412213] hub 3-0:1.0: 1 port detected
[   13.416553] xhci-hcd xhci-hcd.1.auto: xHCI Host Controller
[   13.422071] xhci-hcd xhci-hcd.1.auto: new USB bus registered, assigned bus number 4
[   13.429882] usb usb4: We don't know the algorithms for LPM for this host, disabling LPM.
[   13.438900] hub 4-0:1.0: USB hub found
[   13.442695] hub 4-0:1.0: 1 port detected
[   13.604910] CMEMK module: reference Linux version 4.1.13
[   13.613314] cmemk initialized
[   13.664036] usb 1-1: new high-speed USB device number 2 using xhci-hcd
[   13.694053] usb 2-1: new SuperSpeed USB device number 2 using xhci-hcd
[   13.731656] hub 2-1:1.0: USB hub found
[   13.739471] hub 2-1:1.0: 4 ports detected
[   13.809241] hub 1-1:1.0: USB hub found
[   13.813160] hub 1-1:1.0: 4 ports detected
[   13.918288] cryptodev: driver 1.6 loaded.
[   13.948947] gdbserverproxy: disagrees about version of symbol module_layout
[   13.984813] EXT4-fs (mmcblk0p2): re-mounted. Opts: (null)
bootlogd: cannot allocate pseudo tty: No such file or directory
Starting random number generator daemon.
[   14.155155] random: nonblocking pool is initialized
ALSA: Restoring mixer settings...
INIT: Entering runlevel: 5me get
Initializing the graphics driver ...

[   15.243703] net eth1: initializing cpsw version 1.15 (0)
[   15.326759] net eth1: phy found : id is : 0x20005c90
[   15.331849] libphy: PHY  not found
[   15.335285] net eth1: phy  not found on slave 1
Starting telnet daemon.
Starting syslogd/klogd: done
Starting Telephony daemon
Enabling thermal zones...
Export TSLIB Variables
Operation Finished
 
Starting TFT GUI application
[   18.565659] NET: Registered protocol family 10
[   18.566408] IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready
[   18.569488] IPv6: ADDRCONF(NETDEV_UP): eth1: link is not ready
root@am57xx-evm:~#

Best Regards,

Ganesh