Part Number: BEAGLEBK
Tool/software: Linux
Hi,
How can I write the image am335x-evm-linux-04.00.00.04 (or previous versions) on the Beaglebone Black using a SD card. The usual process that works for other images (i.e. debian) and that can be found in any getting started guide does not work for the image I want to flash. It looks like the board is not able to write the SD Card image on the eMMC. How can I proceed?
Additionally, is it normal that when writing the image into the SD Card, two partitions are created ? : the BOOT partition (~70MB) and a "removable disk" (~3.8GB). This partition is not the same kept when writing (for example) a debian image into the SD card.
Any suggestion would be really helpful. Thanks.
Simon