Other Parts Discussed in Thread: UNIFLASH,
Tool/software: Linux
Hi,
We are working on EMMC(MMC1) boot on a custom board and could not make it. We used uniflash to flash the image to EMMC(MMC1) successfully. But after reboot, I tested EMMC clk/cmd pin by scope. There is no output at all.
1. For EMMC, does the GPMC_WP0 pin is required to set to low. Does the ROM(PBL) will check this Pin (Used as SD/MMC card insert detection).
2. We are aware of the pin for EMMC(MMC1) for boot is special according to Tables 5-32 or 5-33 in the TRM. Does TI have any reference design?
3. We did not connect the data pin correctly, I am looking for a work around for this. Does AM4378 has any interface and internal flash, I could use to flash MLO to boot from.
Thanks
Wayne