This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA2EVM5777: Tidl usecase can not display on LCD

Part Number: TDA2EVM5777

I have change the TIDL usecase,  and I want to make the output display on LCD. But  errors have occurred, and the log information is here:

Hi Anand, I am the workmate of Kaixiang Ye, I am trying finishing the work. When running on TDA2xx, some errors have occurred, and the log information is here:


[IPU1-0] Core Menu
[IPU1-0] ====================
[IPU1-0]
[IPU1-0] 1: DSP
[IPU1-0] 2: EVE
[IPU1-0]
[IPU1-0] Enter Choice:
[IPU1-0]
[IPU1-0] 257.539834 s:
[IPU1-0]
[IPU1-0] ====================
[IPU1-0] Use case Mode
[IPU1-0] ====================
[IPU1-0]
[IPU1-0] 1: Dump Output Frames to file
[IPU1-0] 2: Free Run (Output Frames are not dumped)
[IPU1-0]
[IPU1-0] Enter Choice:
[IPU1-0]
[IPU1-0] 261.435521 s: +++++++++++++++++pObj->chainsCfg->displayType = 7, pObj->displayWidth = 1920, pObj->displayHeight = 1200+++++++++++++++
[IPU1-0] 261.446532 s: CAPTURE: Create in progress !!!
[IPU1-0] 261.446806 s: CAPTURE: VIP1 Slice0 PortA capture mode is [ 8-bit] !!!
[IPU1-0] 261.494723 s: CAPTURE: Create Done !!!
[IPU1-0] 261.495089 s: IPC_OUT_0 : Create in progress !!!
[IPU1-0] 261.495394 s: IPC_OUT_0 : Create Done !!!
[HOST ] 261.495577 s: IPC_IN_0 : Create in progress !!!
[HOST ] 261.495882 s: IPC_IN_0 : Create Done !!!
[HOST ] 261.496095 s: ALGORITHM: Create in progress (algId = 11) !!!
[HOST ] 261.502684 s: UTILS: DMA: Allocated CH (TCC) = 0 (0)
[HOST ] 261.502714 s: UTILS: DMA: 0 of 1: Allocated PaRAM = 0 (0x43305600)
[HOST ] 261.502714 s: ALGORITHM: Create Done (algId = 11) !!!
[HOST ] 261.502806 s: IPC_OUT_1 : Create in progress !!!
[HOST ] 261.502836 s: IPC_OUT_1 : Create Done !!!
[EVE2 ] 261.503111 s: IPC_IN_0 : Create in progress !!!
[EVE2 ] 261.504026 s: IPC_IN_0 : Create Done !!!
[EVE2 ] 261.504605 s: ALGORITHM: Create in progress (algId = 14) !!!
[IPU1-0] 262.779997 s: IPC_IN_1 : Create in progress !!!
[IPU1-0] 262.781217 s: IPC_IN_1 : Create Done !!!
[HOST ] 262.781400 s: IPC_OUT_0 : Create in progress !!!
[HOST ] 262.781431 s: IPC_OUT_0 : Create Done !!!
[EVE1 ] 262.781736 s: IPC_IN_0 : Create in progress !!!
[EVE1 ] 262.782620 s: IPC_IN_0 : Create Done !!!
[EVE1 ] 262.783200 s: ALGORITHM: Create in progress (algId = 14) !!!
[EVE2 ] 262.778503 s: ALGORITHM: Create Done (algId = 14) !!!
[EVE2 ] 262.779113 s: IPC_OUT_0 : Create in progress !!!
[EVE2 ] 262.779601 s: IPC_OUT_0 : Create Done !!!
[IPU1-0] 264.056091 s: IPC_IN_0 : Create in progress !!!
[IPU1-0] 264.057311 s: IPC_IN_0 : Create Done !!!
[IPU1-0] 264.057890 s: *************************Merge*************************
[IPU1-0] 264.057982 s: *************************Display_VideoPrm.inQueParams.prevLinkId= 37 ,Display_VideoPrm.inQueParams.prevLinkQueId= 0 , Display_VideoPrm.displayId= 0 ,Display_VideoPrm.displayScanFormat= 1 ,Display_VideoPrm.rtParams.tarWidth= 1920 ,Display_VideoPrm.rtParams.tarHeight= 1200 ,Display_VideoPrm.rtParams.posX= 0 ,Display_VideoPrm.rtParams.posY= 0 ,*************************
[IPU1-0] 264.058378 s: DISPLAY: Create in progress !!!
[IPU1-0] 264.058744 s: dispcore/src/vpscore_dss.c @ Line 1369:
[IPU1-0] 264.058836 s: Upscaling of greater than 8x is not supported
[IPU1-0] 264.058927 s: dispdrv/src/vpsdrv_displayCore.c @ Line 295:
[IPU1-0] 264.058988 s: Set DSS parameter failed
[IPU1-0] 264.059049 s: Assertion @ Line: 346 in links_ipu/display/displayLink_drv.c: status==SYSTEM_LINK_STATUS_SOK : failed !!!
[EVE1 ] 264.054260 s: ALGORITHM: Create Done (algId = 14) !!!
[EVE1 ] 264.055206 s: IPC_OUT_0 : Create in progress !!!
[EVE1 ] 264.055694 s: IPC_OUT_0 : Create Done !!!


The log shows that the error occurred during the creation of DISPLAY. Is any body who konws how to sovle this problem?
Thanks!

I only change the Eve case.


UseCase: chains_tidlEve

Capture -> Alg_tidlpreproc (A15)
Alg_tidlpreproc (A15) -> Alg_tidl_1 (EVE1)
Alg_tidlpreproc (A15) -> Alg_tidl_2 (EVE2)
Alg_tidl_1 (EVE1) -> Merge (IPU1_0)
Alg_tidl_2 (EVE2) -> Merge (IPU1_0)
Merge (IPU1_0) -> Display_Video
GrpxSrc -> Display_Grpx