Part Number: EVMK2G
Hi, I'm trying to run the quickstart demo on the EVMK2G eval board. I get the message "SOC RESET FAILURE" instead of an IP address.The message and serial number of the board are shown in the attached pictures. Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: EVMK2G
Hi, I'm trying to run the quickstart demo on the EVMK2G eval board. I get the message "SOC RESET FAILURE" instead of an IP address.The message and serial number of the board are shown in the attached pictures. Thanks!
Right after power on. I don't see a boot complete message, but it might be moving by too fast. Here is a video of the sequence:
Ok, I see. Can you share the BCM log, you should be able to get it from the usb serial port (next to the sdcard slot), it should be /dev/ttyUSB1.
Best Regards,
Yordan
We appreciate the efforts you have taken to provide us with the details. this does appear to power sequencing issue on your EVM. If you connect a UART miniUSB cable and switch the SW12 to OFF position, you should see 2 serial connections from the EVM to the PC. On which is the SOC UART and the other one will be a BMC UART. configure both serial connections to 115.2 kbps.
The BMC UART has a command prompt like this,
BMC>
press enter if you are not seeing anything. Now reboot the board to provide the power sequence log as seen by the board monitor controller(BMC).
You can reset the board by reconnecting the power cable or by typing the following command on the BMC command prompt.
reboot por
I am also reporting this to the EVM team so that they can provide their inputs.
Regards,
Rahul
I also noticed some odd behavior of the reset state led. Note how it turns on dimly and then gradually increases in brightness.