Part Number: AM5728
Tool/software: Linux
Hi, Expert
My customer reported that they found the ducatih264enc Gstreamer plugin memory leak base on the PDK 03.03.00.04 on AM5728 EVM, could please have a check?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: AM5728
Tool/software: Linux
Hi, Expert
My customer reported that they found the ducatih264enc Gstreamer plugin memory leak base on the PDK 03.03.00.04 on AM5728 EVM, could please have a check?
Hi,Expert
when i use with application is memory leak.
v4l2 for cap data, v4l2 -> appsrc -> ducatih264enc(ti for encode ) -> filesink {this way is memory leak}
v4l2-> appsrc -> filesink {this way not find memory leak}
/* * * compile command arm-linux-gnueabihf-gcc app-camera.c -o app `pkg-config --cflags --libs gstreamer-1.0 gstreamer-base-1.0 gstreamer-app-1.0` * */ #include <linux/videodev2.h> #include <sys/ioctl.h> #include <sys/mman.h> #include <unistd.h> #include <stdio.h> #include <stdint.h> #include <errno.h> #include <fcntl.h> #include <stdlib.h> #include <string.h> #include <gst/gst.h> #include <gst/app/gstappsrc.h> #define waylandsink #define v4l2src typedef struct _App App; struct _App { GstElement *pipeline; GstElement *appsrc; GstElement *encode; GstElement *parse; GstElement *sink; GstElement *decode; GstBus *bus; GstMessage *msg; GMainLoop *loop; guint bus_watch_id; }; App s_app; int ret, idx, fd; #define NBUF 3 #define FRAME_SIZE 152064 //352*288*1.5 int width = 352, height = 288; void *buffer_addr[NBUF]; int size[NBUF]; static void feed_data (GstElement * appsrc, guint size, App * app) { printf("feed-data....\n"); struct v4l2_buffer buf; /* Dequeue one buffer */ memset(&buf, 0, sizeof(buf)); buf.type = V4L2_BUF_TYPE_VIDEO_CAPTURE; buf.memory = V4L2_MEMORY_MMAP; if(-1 == xioctl(fd, VIDIOC_DQBUF, &buf)) { perror("Queue Buffer"); return FALSE; } idx = buf.index; GstBuffer *buffer; GstFlowReturn ret; buffer = gst_buffer_new_allocate(NULL,FRAME_SIZE,NULL); GstMapInfo info; gst_buffer_map(buffer,&info,GST_MAP_WRITE); unsigned char * buff = info.data; memcpy(buff,buffer_addr[idx],FRAME_SIZE); gst_buffer_unmap(buffer,&info); g_signal_emit_by_name(app->appsrc,"push-buffer",buffer,&ret); printf("ret:%d\n",ret); if (ret != GST_FLOW_OK) { /* some error, stop sending data */ printf("push error...\n"); return FALSE; } gst_buffer_unref(buffer); memset(&buf, 0, sizeof(buf)); buf.type = V4L2_BUF_TYPE_VIDEO_CAPTURE; buf.memory = V4L2_MEMORY_MMAP; buf.index = idx; if(-1 == xioctl(fd, VIDIOC_QBUF, &buf)) { perror("Queue Buffer"); return FALSE; } return TRUE; } int xioctl(int fd, int request, void *arg) { int r; do r = ioctl (fd, request, arg); while (-1 == r && EINTR == errno); return r; } int init_device(int fd) { unsigned int i; struct v4l2_capability caps; struct v4l2_format fmt; struct v4l2_requestbuffers req; struct v4l2_buffer buf; /* Check for capture device */ memset(&caps, 0, sizeof(caps)); if (-1 == xioctl(fd, VIDIOC_QUERYCAP, &caps)) { perror("Setting Pixel Format"); return 1; } printf("Driver: %s\ncaps: %8x", caps.driver, caps.capabilities); if (~caps.capabilities & V4L2_CAP_VIDEO_CAPTURE) { printf("Not a capture device"); return 1; } /* Set capture format to UYVY */ memset(&fmt, 0, sizeof(fmt)); fmt.type = V4L2_BUF_TYPE_VIDEO_CAPTURE; fmt.fmt.pix.width = width; fmt.fmt.pix.height = height; fmt.fmt.pix.pixelformat = V4L2_PIX_FMT_NV12; // fmt.fmt.pix.pixelformat = V4L2_PIX_FMT_UYVY; fmt.fmt.pix.field = V4L2_FIELD_NONE; if (-1 == xioctl(fd, VIDIOC_S_FMT, &fmt)) { perror("Setting Pixel Format"); return 1; } printf("Selected Camera Mode:\n" " Width: %d\n" " Height: %d\n" " Field: %d", fmt.fmt.pix.width, fmt.fmt.pix.height, fmt.fmt.pix.field); printf(" PixFmt = %c%c%c%c\n", fmt.fmt.pix.pixelformat & 0xFF, (fmt.fmt.pix.pixelformat >> 8) & 0xFF, (fmt.fmt.pix.pixelformat >> 16) & 0xFF, (fmt.fmt.pix.pixelformat >> 24) &0xFF); /* Currently driver supports only mmap buffers * Request memory mapped buffers */ memset(&req, 0, sizeof(req)); req.count = NBUF; req.type = V4L2_BUF_TYPE_VIDEO_CAPTURE; req.memory = V4L2_MEMORY_MMAP; if (-1 == xioctl(fd, VIDIOC_REQBUFS, &req)) { perror("Requesting Buffer"); return 1; } printf("Total buffer num %d\n", req.count); for (i = 0; i < req.count; i++) { memset(&buf, 0, sizeof(buf)); buf.type = V4L2_BUF_TYPE_VIDEO_CAPTURE; buf.memory = V4L2_MEMORY_MMAP; buf.index = i; if (-1 == xioctl(fd, VIDIOC_QUERYBUF, &buf)) { perror("Querying Buffer"); return 1; } /* Memory map all the buffers and save the addresses */ buffer_addr[i] = mmap(NULL, buf.length, PROT_READ | PROT_WRITE, MAP_SHARED, fd, buf.m.offset); //buffer_addr[i]=(void*)malloc(FRAME_SIZE); size[i] = buf.length; printf("Address %p, size %d, image size: %d \n", buffer_addr[i], buf.length, buf.bytesused); /* Queue the buffer for capture */ memset(&buf, 0, sizeof(buf)); buf.type = V4L2_BUF_TYPE_VIDEO_CAPTURE; buf.memory = V4L2_MEMORY_MMAP; buf.index = i; if (-1 == xioctl(fd, VIDIOC_QBUF, &buf)) { perror("Queue Buffer"); return 1; } printf("12345\r\n"); } if (-1 == xioctl(fd, VIDIOC_STREAMON, &buf.type)) { perror("Start Capture"); return 1; } return 0; } void release_device(int fd) { int type = V4L2_BUF_TYPE_VIDEO_CAPTURE; xioctl(fd, VIDIOC_STREAMOFF, &type); close(fd); } gboolean bus_call(GstBus *bus, GstMessage *msg, gpointer data) { GMainLoop *loop = (GMainLoop *) data; switch (GST_MESSAGE_TYPE (msg)) { case GST_MESSAGE_EOS: fprintf(stderr, "End of stream\n"); g_main_loop_quit(loop); break; case GST_MESSAGE_ERROR: { gchar *debug; GError *error; gst_message_parse_error(msg, &error, &debug); g_free(debug); g_printerr("Error: %s\n", error->message); g_error_free(error); g_main_loop_quit(loop); break; } default: break; } return TRUE; } int main(int argc, char **argv) { App *app = &s_app; printf("==========\n"); char devnode[100] = "/dev/video1"; fd = open(devnode, O_RDWR); if (fd == -1) { perror("Opening video device"); return 1; } ret = init_device(fd); if (0 != ret) { printf("Exiting"); return ret; } gst_init(NULL,NULL); app->pipeline = gst_pipeline_new("encodepipeline"); g_assert(app->pipeline); app->appsrc = gst_element_factory_make("appsrc","srcElement"); g_assert(app->appsrc); app->encode = gst_element_factory_make("ducatih264enc","encodeElement"); g_assert(app->encode); app->parse = gst_element_factory_make("h264parse","parseElement"); g_assert(app->parse); app->decode = gst_element_factory_make("ducatih264dec","decodeElement"); g_assert(app->decode); app->sink = gst_element_factory_make("filesink","sinkElement"); g_assert(app->sink); printf("element creat success\n"); GstCaps *capsappsrc2H264enc; capsappsrc2H264enc = gst_caps_new_simple("video/x-raw", "format",G_TYPE_STRING, "NV12", "width", G_TYPE_INT, 352, "height",G_TYPE_INT, 288, "framerate", GST_TYPE_FRACTION, 30, 1, NULL); // g_object_set(G_OBJECT (app->sink), "sync", FALSE, // NULL); gst_app_src_set_caps(GST_APP_SRC(app->appsrc), capsappsrc2H264enc); g_object_set(app->sink,"location","/mnt/camera.yuv",NULL); app->loop = g_main_loop_new(NULL,FALSE); app->bus = gst_pipeline_get_bus(GST_PIPELINE(app->pipeline)); app->bus_watch_id = gst_bus_add_watch(app->bus,bus_call,app->loop); gst_object_unref(app->bus); gst_bin_add_many(GST_BIN(app->pipeline), app->appsrc,app->sink,NULL); gboolean bLinkOk; bLinkOk= gst_element_link(app->appsrc,app->sink); if(!bLinkOk){ g_warning("Failed to link many 1\n"); return -5; } g_signal_connect(app->appsrc, "need-data", G_CALLBACK(feed_data), app); gst_element_set_state (app->pipeline, GST_STATE_PLAYING); printf("run....1\n"); g_main_loop_run(app->loop); printf("run....2\n"); app->msg = gst_bus_timed_pop_filtered (app->bus, GST_CLOCK_TIME_NONE, GST_MESSAGE_ERROR | GST_MESSAGE_EOS); if (app->msg != NULL) gst_message_unref (app->msg); gst_object_unref (app->bus); gst_element_set_state (app->pipeline, GST_STATE_NULL); gst_object_unref (app->pipeline); gst_object_unref(app->appsrc); gst_object_unref(app->sink); printf("close...\n"); return 0; }whit is videnc2test?
when i use it I need a large enough file for encode? loop encode it?
Hi,
Is this issue not reproduced with ducatimpeg4enc?
Please share me what memory statistics you are collecting to narrow down ducatih264enc as the root cause of the issue.
I haven't used ducatimpeg4enc, about ducatih264enc you can Look at this page e2e.ti.com/.../2287603
I only use top command for watch memory leak .
Hi Abayyy,
The encoder memory leak issue has been fixed and the patch is available here -

You can use arago build to rebuild the plugin -

Hi,manisha,
thanks,but I don't know how to only build the ducatih264enc plugin with ti-processor-sdk-linux-am57xx-evm-03.03.00.04 SDK? Can you help me?
Hello,
abayyy said:thanks,but I don't know how to only build the ducatih264enc plugin with ti-processor-sdk-linux-am57xx-evm-03.03.00.04 SDK?
The issue was not observed only for ducatih264enc.
This is the user guide for PSDK version 03.03.00.04
processors.wiki.ti.com/index.php
Please follow the steps in the guide.
This is the last step for building ducati plugin:
MACHINE=am57xx-evm bitbake gstreamer1.0-plugins-ducati
You could apply the patch manually in the gstducatividenc.c file.
Please check chapter Forced Re-compilation in the guide.
The new libgstducati.so file should be cp to rootfs/usr/lib/gstreamer-1.0.
Hope this helps.
BR
Margarita
Hi Margarita,
Which version of PDK that your patch of duchati plugin work on? I think the .so file does not depend on the PDK version.
Thanks for your great support!
Thank you very much for your help to solve the memory leak problem
https://e2e.ti.com/support/embedded/linux/f/354/p/620539/2291680#2291680
Hi Margarita,
Customer do not find the memory leak issue in the H264enc plugin by the .so file you provided, thanks for your support!
Could you please also check the ducatih264dec plugin, customer reported that there is also memory leak issue in this plugin, thanks!
Hi Margarita:
Customer's test scenario is as follows:
gst-launch-1.0 -v -e v4l2src device=/dev/video1 io-mode=2 ! 'video/x-raw, format=(string)NV12, width=(int)800, height=(int)600, framerate=(fraction)30/1,bitrate=(int)30' ! ducatih264enc ! h264parse ! ducatih264dec ! waylandsink sync=false
So you can reproduce this issue? And could you please provide the updated plugin after the memory leak issue is fixed? Thanks
Hi Jian,
I reproduced the issue with your pipeline. I analyzed the ducatidecoder source code, I found one small memory leak every frame but after fixing this leak also still observe Mem% in top command increasing .
I have attached the modified libgstducati.so for your testing. Can you please confirm the behaviour?
One more observation is if kmsink in the pipeline is replaced with fakesink then no memoryleak is obsrved.
Issue is seen with kmssink or waylandsink.
Ram
Hi Ram,
Thanks a lot for your support and hard work!
So you have fixed the memory leak issue in the ducatidecoder plugin and also analyzing the code in kmssink or waylandsink?
I will work with customer to test based on your guidance, thanks!
Manisha,
Thanks for your support! I will work with customer to verify after the China National Holiday!