Part Number: AM3357
Dear sirs,
For design verification as to the timing of DDR2 interface, I need information about DDR2-EMIF of AM335x.
Are there the specification information?
("se" represents single ended signal, and "diff" represents diffirential signal)
1) Input of seDQsignal and diffDQS
I'm planning to measure the timing as to the seDQ signal at AM3357, to verify that the seDQ meets the requirement of input stage of AM3357.
1-1) seDQ input setup/hold time from diffDQS.
1-2) seDQ input setup/hold time from diffCK (if required).
1-3) diffDQS input setup/hold time from diffCK (if required).
2) AM3357 Output specifications
To set the margin due to disparison of AM3357 for timing at DDR2-SDRAM.
2-1) diffDQS output access time from diffCK.
2-2) seDQ output access time from diffDQS.
2-3) seAddress/Command output access time from diffCK.
Best regards,
Hiroshi Takakura