This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PC can not recongnize the Rndis.

Other Parts Discussed in Thread: AM3715, OMAP3530

dear all,

recently , I get  two EVM. one is AM3715(MISTRAL),and OMAP3530(SEED in shenzhen/China).I was told the AM3715 and oamp3530 is pin-to-pin.

I download the xldruart.nb0 with pserial.exe and then download .raw to flash (on the EVM AM3715 ),then ,download nk.bin with Rndis,there are all no problems.

but with the Omap3530 EVM, I download the xldruart.nb0 and .RAW to flash,then, I want to download nk.bin via Rndis.BUT the message vis UART is : 

Rndis::initialization:with addr=480AB000

Rndis::Address static map to addr=480AB000

Rndis::initialization!

+UABFN::Device ID=0x4b7ae02f

+UABFN::Device ID=0x4b7ae02f

Rndis::PDDInit Sucess!

Rndis::Get MAC address200,902F,B5D

Rndis::initialization Fail!

ERROR:Boot device driver Init call failed

and the PC just recommand: can not recongnize  USB item....But ,with the EVM 3715,it did work well.could you give me some suggestion what should i do??We are going to do a project with the IC OMAP3530 or AM3715  and do need your support....

thanks very much...

 

  • I'm not sure what SEED platform is and how different it is from the Mistral EVM (for OMAP3530).

    Do you have a OMAP3530 Mistral EVM and if so can you try it on that board. The official BSP is verified on the OMAP3530 Mistral EVM (Rev G).