Part Number: TMS320C6748
I have received new C6748 LCDK kit. I followed the instructions as in the Quick Start Guide. The serial port driver is installed (COM5) on Windows 7 PC; I have also set up Terraterm to the correct baud rate of 115200 and 8,N,1 None serial settings. The same matching settings are done for COM5 port on PC.
Also, the DIP settings are correct, 2,3,4 are ON, rest are OFF. However, I do not see any response (no characters) on the terraterm console. I have tried power cycle and Reset on the board, but nothing works.
Please advise what is wrong with the C6748 LCDK kit?
Thanks
Iqbal