Part Number: TMDSIDK437X
Other Parts Discussed in Thread: TPS62362
Tool/software: Linux
Hi,
a customer is starting a project based on Linux on AM437x SoC. They have problems when starting Linux on TMDSIDK437X.
They loaded according to the instructions of http://processors.wiki.ti.com/index.php/Processor_SDK_Linux_create_SD_card_script the „pre-built images“ onto the SD-Card which came with the TMDSIDK437X. When starting TMDSIDK437X then UART provides the below (those are not there when removing the SD card). It only occurs with Rev 1.4 A, not with Rev 1.3 A. Same SD-Card and same data was used for both.
U-Boot SPL 2017.01-g9fd60700db (Jun 28 2017 - 18:14:21)
Trying to boot from MMC1
SPL: Please implement spl_start_uboot() for your board
SPL: Direct Linux boot not active!
reading u-boot.img
reading u-boot.img
reading u-boot.img
reading u-boot.img
U-Boot 2017.01-g9fd60700db (Jun 28 2017 - 18:14:21 -0400)
CPU : AM437X-GP rev 1.2
Model: TI AM437x Industrial Development Kit
DRAM: 1 GiB
PMIC: TPS62362
NAND: 0 MiB
MMC: OMAP SD/MMC: 0
MMC: no card present
** Bad device mmc 0 **
Using default environment
Net: <ethaddr> not set. Validating first E-fuse MAC
cpsw, usb_ether
Hit any key to stop autoboot: 0
MMC: no card present
MMC: no card present
MMC: no card present
MMC: no card present
starting USB...
USB0: Register 2000440 NbrPorts 2
Starting the controller
USB XHCI 1.00
scanning bus 0 for devices... 1 USB Device(s) found
scanning usb for storage devices... 0 Storage Device(s) found
USB device 0: unknown device
Booting from nand ...
no devices available
no devices available
=>
Can you help?
You need more information?
Thanks
Fred