I got a lot of strange message while booting Omap. I flashed the board with the Omap kernel and rootfs.jffs2 from images directory according the scripts. What do I have to do to get an recent version of TI software running on that board?
Examples:
twl_reg twl_reg.18: can't register VUSB1V8, -16
twl_reg: probe of twl_reg.18 failed with error -16
NET: Registered protocol family 15
Power Management for TI OMAP3.
Division by zero in kernel.
[<c0039524>] (unwind_backtrace+0x0/0xdc) from [<c017ff3c>] (Ldiv0+0x8/0x10)
Division by zero in kernel.
[<c0039524>] (unwind_backtrace+0x0/0xdc) from [<c017ff3c>] (Ldiv0+0x8/0x10)
SmartReflex driver initialized
VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 1
twl_rtc twl_rtc: setting system clock to 2000-01-01 00:00:00 UTC (946684800)
tvp514x 3-005d: chip id mismatch msb:0xfb lsb:0xfb
tvp514x 3-005d: Unable to detect decoder
tvp514x 3-005d: chip id mismatch msb:0xfb lsb:0xfb
tvp514x 3-005d: Unable to detect decoder
tvp514x 3-005d: chip id mismatch msb:0xfb lsb:0xfb
tvp514x 3-005d: Unable to detect decoder
tvp514x 3-005d: chip id mismatch msb:0xfb lsb:0xfb
tvp514x 3-005d: Unable to detect decoder
omapdss DPI error: display already enabled
omap_vout omap_vout: 'lcd' Display already enabled
omapdss DPI error: display already enabled
omap_vout omap_vout: 'lcd' Display already enabled
Empty flash at 0x0212809c ends at 0x02128800
JFFS2 error: (1) jffs2_build_inode_pass1: child dir "opkg" (ino #3920) of dir ino #3898 appears to be a hard link
JFFS2 error: (1) jffs2_build_inode_pass1: child dir "SI7018" (ino #1443) of dir ino #1398 appears to be a hard link
VFS: Mounted root (jffs2 filesystem) on device 31:4.
Freeing init memory: 172K
INIT: version 2.86 booting
Please wait: booting...
Starting udev
udev: starting version 141
udevd[529]: inotify_add_watch(3, (null), 10) failed: Bad address
udevd[529]: inotify_add_watch(3, (null), 10) failed: Bad address
Remounting root file system...
WARNING: Couldn't open directory /lib/modules/2.6.32: No such file or directory
FATAL: Could not open /lib/modules/2.6.32/modules.dep.temp for writing: No such file or directory
modprobe: FATAL: Could not load /lib/modules/2.6.32/modules.dep: No such file or directory
modprobe: FATAL: Could not load /lib/modules/2.6.32/modules.dep: No such file or directory
root: mount: mounting rootfs on / failed: No such file or directory
root: mount: mounting usbfs on /proc/bus/usb failed: No such file or directory
Setting up IP spoofing protection: rp_filter.
Configuring network interfaces... done.
Wed Dec 2 19:41:00 UTC 2009
INIT: Entering runlevel: 5
Starting telnet daemon.
modprobe: FATAL: Could not load /lib/modules/2.6.32/modules.dep: No such file or directory
Starting syslogd/klogd: done
Starting thttpd.
Starting OMAP Demo application.
_____ _____ _ _
| _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_
| | _| .'| . | . | | __| _| . | | | -_| _| _|
|__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_|
|___| |___|
Arago Project http://arago-project.org omap3evm ttyS0
Arago 2009.11 omap3evm ttyS0
omap3evm login: vi /opt/etc/autoexecJFFS2 notice: (1158) check_node_data: wrong data CRC in data node at 0x02127f20: read 0xe6e968e3, calculated 0x2942e90e.