Part Number: AM3358
Tool/software: Linux
Hello comunity,
I have a custom board with a AM3358 similar to the beaglebone black.The only mayor difference is a Micron MT41K256M16TW-107 IT:P instead to the kingston D2516EC4BXGGB on my BBB.
I followed the bringup-tips and can the the steady output of 'C's with UART0. After inserting a sd-card with an image "3.8.13-bone70" the uboot stops at DRAM
U-Boot 2015.01-00001-gb2412df (Jan 29 2015 - 15:01:06), Build: jenkins-github_Bootloader-Builder-105 Watchdog enabled I2C: ready DRAM: 512 MiB
Do I have to edit the uboot because of a different RAM like on this page "//processors.wiki.ti.com/index.php/Sitara_Linux_Training:_Tuning_the_DDR3_Timings_on_BeagleBoneBlack"? I was thinking that the Micron RAM is compatible?!
Thank you very much for your help.
kind regards
Eric Schmieder