Part Number: AM3354
Tool/software: Linux
Hi,
when booting kernel 4.9.28 (4.9.28+gitAUTOINC+eed43d1050-geed43d1050) the above mentioned error occurs multiple times and in consequence USB devices do not work at all. With kernel 4.1.18, the same device tree files and nearly the same kernel configuration USB worked well. The boot messages with 4.9.28-kernel and the corresponding configuration files (dts, kernel config) are as follows:
Any ideas to resolve this issue?
Kind regards
Arndt