This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3352: DDR3 configuration

Part Number: AM3352

Hi All,

We have a customized board with AM3352 , DDR3L Chip (MT41K512M16HA-125IT) and NAND Flash (MT29F4G08ABADAWP-IT:D). We have planned to operate the AM3352 with 1Ghz  and DDR3L at 800 MHz operating speed . The DDR3 Length Matching are

DDR3_CK

1.46173228

DDR3_CK#

1.46173228

DDR3_DQ

1.42279528

DDR3_DQ

1.42311024

I Have attached the Customized GEL file along with the DDR3 Register calculation sheet, DDR3 Phy Calculation scheet.

AM3352&DDR3L.rar

Questions:

1. Can some one verify the DDR3 Phy Calculation and DDR3 Register calculation. Because we cant able to access the DDR3L through the GEL File ?

2. Whether the changes made in the GEL is sufficient to check the processor and DDR3L. Because we cant able to access the DDR3L through the GEL File ?

3. What changes has to done in U-Boot Source for DDR3 and NAND Flash access.

Kindly provide suggestion to solve the above issue. As it is becoming a critical issue. Thanks in advance.

Regards,

Avinash N