We are having problems getting the video buffer kernel bootargs to work on the new MV5 / DVSDK 2.00.00.22 LSP2.0 kernel release. Bootarg parameters that worked fine on the MV4 release no longer work.
We seem to have the same exact problem that was brought up on a previous post two months ago which was never resolved or for which the resolution was never posted in this forum.
http://e2e.ti.com/forums/p/6564/25252.aspx#25252 : DM6446 - Proper bootargs for video
We have duplicated this on two different DM6446 EVMs. with both virgin SVDSK binaries from the DVSDK 2.0.0.22 code repository page and rebuilt kernels. We have also poured over thecommand syntax shown in SPRUG92 (LSP 2.00 Davinci VPBE Frame Buffer Driver) and also the SPRUE66F (DM6446 Getting started guide) documents. I understand that the bootarg parameters have changed slightly, but in this case I am not sure that it is the "syntax" that is causing the problems.
For those with similar questions, look at this post that provided the documents to start with:
http://e2e.ti.com/forums/p/6767/26214.aspx#26214 : Is there a document for davincifb in mv5.0
We are attempting to "bringup" a target DM6446 platform, but until we can get this controlled on a EVM, we are stuck.
I have tried several different bootargs in an attempt to narrow down what is going on. I will post the results of a series these controlled "tests" below, but the symptoms are:
- Only a 720x480 screen size seems to be suported, bootargs setting up a 720x576 screen do not work anymore, no matter what the syntax is.
- The OSD frame buffer is not working on every bootarg tried, even one taken verbatim from a example on page 15 of the SPRUG92 document.
These are most likely completely unrelated issues, but in either case, they are problematic for us.
What are we missing?
- Gary