This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM355 - Nand configuration for serial flasher



Hi,

We developed a board based on the DM355.

We are using a NAND from Micron, the MT29F8G08AAA (1Gb) and are having issues erasing / writing / reading via UART with the TI tools (DM35x_FlashAndBootUtils_1_50).

We tried to modify the following files in order to make it work to but without success until now :

/DM35x/common/src/device_nand.c
/DM35x/common/include/device_nand.h

/common/drivers/src/nand.c
/common/drivers/include/nand.h
/common/ubl/src/ubl.c
/common/ubl/include/ubl.h
/common/ubl/src/nandboot.c
/common/ubl/include/nandboot.h

The above files never described a NAND larger than 512 Mb, so we are wondering if the chosen NAND could be troublesome. Also do we need to change the APPStartAddr & UBLStartAddr or is it always the same no matter the NAND size ?

Any help with this matter would be greatly appreciated !

Thanks a lot in advance

Kind regards,

Richard

  • Richard,

    Can you please provide the error logs? What changes were introduced in the files listed?

    UBLStartAddr need to be changed if the start address of the UBL changes (same applies for APPStartAddr ). It has nothing to do with NAND size.

    Thanks,
    Gaurav

  • Hi Gaurav,

    Thank you for your answer.

    The errors and the debug messages are put in the file " error.txt "

    For the modifications and the changes,  look rather files "device_nand.c ", " device_nand.h", " nand.c " and nand.h ". The changes are there very visibles.

    We also have difficulty in finding the following informations for our NAND:

                                                                                                                  - NAND_MAX_PAGE_SIZE

                                                                                                                  - NAND_MAX_BYTES_PER_OP         

                                                                                                                  - NAND_MIN_SPAREBYTES_PER_OP

    Are they parameters fixed by the EMIF interface?

    In the end, we want to flash NAND the reference of which is given to the previous post.

    Thank you still for your help.

    Kind regards,

    Richard & Sakho

     

     

     

  • Richard & Sakho,

    Thanks for sending the error log.

    NAND_MAX_PAGE_SIZE, NAND_MAX_BYTES_PER_OP  and NAND_MIN_SPAREBYTES_PER_OP are generic information used by the code and should be fine w.r.t the NAND in question.

    Can you please specify which silicon Revision are you using?

    The NAND in question has to be supported by the RBL (ROM bootloader) for boot to happen. That depends on the silicon version.

    Also the device ID for this NAND (0xD3) is present in DEVICE_NAND_CHIP_infoTable table (device_nand.c). However the page size is defined as 2048 + 64. The actual page size seems to be 4096 + 128 (from NAND datasheet). However given that the NAND is ONFI, the UBL should be able to talk to the NAND. You might have to introduce debug statements to see where is the problem.

    Thanks,
    Gaurav

  • Dear Gaurav,

     

    Thank you for the reply.

    The exact part number is :

    MT29F8G08AAAWP-ET:A

    Can you please confirm that this NAND is OK ?

    Thanks a lot

    Regard

    Richard

  • Richard,

    I meant the silicon revision/part no for DM355. I apologize for the confusion.

    Thanks,
    Gaurav

  • Gaurav,

    Thank you for your answer.

    The reference completes of the DM355 which I use is the following one:  TMS320DM355ZCE 216 $4A-9BA7R7W EI

    It is all that we have on this chip, and I hope that can help.

    Otherwise I manage to read all the parameters of the NAND. The writing and the erasing are well made. And thus, the UBL indeed spells at the good address.

    The problem remains to write U-boot on the NAND. During this writing I have only bad block:

            ........................................................................................................

         Block number 22 is a BAD BLOCKBlock 22 is a bad block
    Block number 23 is a BAD BLOCKBlock 23 is a bad block
    Block number 24 is a BAD BLOCKBlock 24 is a bad block
    Block number 25 is a BAD BLOCKBlock 25 is a bad block
    Block number 26 is a BAD BLOCKBlock 26 is a bad block
    .........................................................................................................



    Then, which would raise problem according to you? Should the function  "DEVICE_NAND_BB_checkSpareBytes()" or "DEVICE_NAND_BB_markSpareBytes()" and the structures "NAND_ECC_InfoObj DEVICE_NAND_ECC_info{}" or "NAND_BB_InfoObj DEVICE_NAND_BB_info{}" not be adapted to our NAND?

    U-boot, would it proceed in a different way to detect Bad block?  Have you an idea for the origin of this problem?

    Once again, thank you.

    Richard & Sakho

     

     

     

  • Richard and Sakho,

    Thanks for the information. The device that you have is Rev 1.1 (you can find this information on the Silicon Errata Sec 1.2)

    DEVICE_NAND_BB_checkSpareBytes()", "DEVICE_NAND_BB_markSpareBytes()" and the structures "NAND_ECC_InfoObj DEVICE_NAND_ECC_info{}" or "NAND_BB_InfoObj DEVICE_NAND_BB_info{}" are generic function and structures and uses parameters for different NANDs.

    If the NAND doesn't have actual bad blocks, then the NAND geometry information that UBL has is not correct.

    The UBL uses atleast the following information about the NAND:
    1. Page size
    2. Pages per block
    3. Address cycles

    Can you please print this information from the UBL and see if this is matching the NAND information (from the NAND datasheet).

    As I mentioned in the previous post, for this NAND, if the device is is 0xD3 (please check from the NAND datasheet), then the entry in the table DEVICE_NAND_CHIP_infoTable should be updated from:

      { 0xD3,   4096,       64,             2048+64}

    to

      { 0xD3,   4096,       64,             4096+128}

    Let me know how it goes.

    Thanks,
    Gaurav

  •  

    Gaurav,

    Thank you for your answer and your help.

    About the silicon revision/part no , let us have to take ourselves specific arrangements?

    Indeed, when I applied the modifications that you recommended us, UBL and U-boot spells indeed on the NAND flash.

    The parameters of the NAND which UBL sends back to us are the following ones and they corespondent to those of the
    datasheet.
    MANUFACT ID: 0x0000002C ID: 0x000000D3 NB BLOCK: 0x00001000 NB PAGE/BLOCK: 0x00000040 NB BYTES/PAGE: 0x00001000
    NB SPARE-BYTES/PAGE: 0x000000DA DATA_BYTES/OP: 0x00001000 S_BYTES/OP: 0x00000080 CS OFFSET: 0x00000000 BUS WIDTH: 0x00000001
    FLASH BASE ADDR: 0x02000000 NB OPS/PAGE: 0x00000001 NUM COL ADDR: 0x00000002 NUM ROW ADDR: 0x00000003 !!!


    Now, it seems to me that we manage to flash the NAND with TI tools in UART mode (sfh and sft). But when we pass in NAND boot select (BITSEL [1:0] = 00), there is absolutely nothing. The purpose is to arrive at this boot mode (NAND boot) after flashing. would you have an idea on this problem?

    Here is a print of the parameters that we use for flashing:

    For UBL (ubl_DM35x_nand.bin):
    MAGIC NUMBER: 0xA1ACED00 ENTRY POINT: 0x00000100 LOAD ADDR: 0x00000020

    For U-Boot (u-boot.bin  that we compiled):
    MAGIC NUMBER: 0xA1ACED66 ENTRY POINT: 0x81080000 LOAD ADDR: 0x81080000 START BLOCK: 0x00000019 !!!

    With these parameters and by having selecting well the mode, the nand boot fails and we do not manage to understand  why.

    Thanks a lot

    Regard

    sakho



  • Sakho,

    The silicon version no of the device is required to figure out the features supported in RBL (ROM bootloader). This in turns determine if a particular NAND is compatible with that version of RBL.

    If the NAND is not compatible, RBL will not be able to load UBL.

    From the description given, the silicon revision is 1.1 and this RBL might not work with the NAND in question. In this case the NAND page size is 4K but the RBL will read 2K.
    One possible workaround is to flash multiple version of header descriptor. A similar issue is discussed at the forum post:

    http://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/100/p/48003/169881.aspx#169881

    There are later versions of the DM355. Can you please suggest is there is any specific reason why you are using an earlier version?

    Thanks,
    Gaurav

  • Dear Gaurav,

    Thank you for the reply.

    We bought the DM355 parts from DIGIKEY for our prototypes and unfortunatly the revision was not specified on it :(

    I just hope that the workaround you suggested works otherwise I will have to get new prototypes to have this fixed...

    If you have any other documentation regarding this workaround, can you please post it here ?

    Thanks a lot again for your help !

    Richard