Hi,
I've been doing some tests to measure the delay between encode and decode, with the following network connection schema:
dm6467t encoder(h264) -> pc -> dm6467t decoder(h264)
The connections are made over ethernet, and the pc has been configured to forward all ip traffic.
I've measured delays of about 6 seconds between the captured image and the decoded image.
Has anyone run such a test? Can that delay be improved?
I've used the default encoder configuration which is supplied with the dvsdk 3.10.00.12.
Thanks!