Hello, I'm working on a dm6446 board with only 128MB DDR2 on board. I have read the <http://wiki.davincidsp.com/index.php/Changing_the_DVEVM_memory_map> guide, but got an error on loading decodeCombo.x64P.
There's a section metioned about changing the memory address inside the encode.tcf/decode.tcf files, but how do I rebuild the codec servers to adopt my needs?
I'm on a linux host and installed everything under /opt/dvevm_1_20. and I installed C6000CGT6.1.11 for cl6x.
I'm having "cmem_1_02", "codec_engine_1_10_01", "codec_servers_1_23", "dsplink_1_30_08_02", "bios_5_20_05", "xdais_5_10", and "xdc_2_94" under /opt/dvevm_1_20.
What else the tool do I need? And what are the exact steps (exact commands I have to issue) I have to follow for rebuilding the x64P (or just relinking) the x64P packages?