Part Number: AM3351
Other Parts Discussed in Thread: TPS65910
My sysboot is [15:0] = 0100 0000 0111 0110
SPI0 ---> MMC0 ----> UART0 ----> EMAC1
In serial i can see 5x "C", and after this the AM3351 request a IP Address, after this my PC send a MLO firmware to the processor and the next file (barebox.bin) it do not sended.
So, i tried to pass the MLO firmware by serial (UART0). After the begining of the transfer, it stops and nothing happen.
I use a TPS65910 with the AM3351, i measured the power supplies, EXT_WAKEUP, PWRONRST, WARMRST, TRSTn and the behaviour was as expected.
What do i look out? DDR3?
I need help to boot the processor.
Thanks.