Hello, I am using evmdm6437 and we finally we got our first custom board, but when I tried to run the program that runs well on the evmdm6437, it doesn't it well on our board. I guess that maybe I need to adapt more things in the project. On the other hand, our custom board has a very similar configuration to EVM, so I don't know very well where I have to look for. For example, MEM (Mem Section Manager), in .tcf file should be the same than evdm6437.
The program seems to be able to run, but never start the main(). What could I check?
Thank you very much