Hi,
On CCS 3.2, I simply tried to run a demo C:\CCStudio_v3.2\examples\evm5510\csl\timer\timer1_useBios\, after *.pjt is opened, the messages are showing below:
Running "C:\CCStudio_v3.2\examples\evm5510\csl\timer\timer1_useBios\cdb2tcf.bat"
Please wait . . .
Conversion FAILED. This is the command execution log:
Application: C:\CCStudio_v3.2\examples\evm5510\csl\timer\timer1_useBios\timer1_u
seBios.cdb
Error: Seed file C:/CCStudio_v3.2/C5500/bios/include/c55xx.cdb cannot be found
Error code 20
cdb2tcf command FAILED.
Press any key to continue . . .
It looks that the seed file directory (C:/CCStudio_v3.2/C5500) is not correct. CCS 3.2 is loaded on a PC that doesn't have previous version installed presently or before. How to correct this ?
Thanks,
Yuhua